This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() |
Coming soon |
This article explain what is and how to use EXTI through examplesl
1. External interrupt/event controller (EXTI)
The external interrupt/event controller consists of up to 23 edge detectors for generating event/interrupt requests. Each input line can be independently configured to select the type (interrupt or event) and the corresponding trigger event (rising or falling or both).
2. Configure EXTI to turn on LED when user button is pressed
2.1. Objective
- Learn how to setup input pin with EXTI in STM32CubeMX
- How to Generate Code in STM32CubeMX and use HAL functions
2.2. Goal
- Configure GPIO and EXTI pin in STM32CubeMX and Generate Code
- Add into project Callback function and function which turn on led
- Verify the correct functionality by pressing button which turns on LED
2.3. Create project in STM32CubeMX
- Menu > File > New Project
- Select STM32F439ZITx
- Configure LED pin as GPIO_Output ( PG14 on NucleoF439ZI, for other board check User Manual)
File:LED UM.png File:LED PIN.png
- Configure Button pin as GPIO_EXTIX (PA0 on NucleoF439ZI, for other board check User Manual)
- GPIO Configuration check
- Enable the interrupt for EXTI
- Save your project and generate the code for your IDE
2.4. HAL Library workflow summary
2.5. Open you IDE
We create function which will handle the EXTI interrupts
- HAL callback function for EXTI : void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
- For LED turn on we need to use this functions : HAL_GPIO_WritePin
The functions we want to put into main.c
/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
if(GPIO_Pin == GPIO_PIN_0) {
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_14, GPIO_PIN_SET);
} else {
__NOP();
}
}
/* USER CODE END 4 */
2.6. Compile and flash
- When you press the blue button of you board the LED should switch on