Getting started with RTC

Revision as of 17:13, 18 November 2022 by Registered User (→‎Configure RTC and Alarm with interrupt)
Under construction.png Coming soon

This article explains how to use the RTC. It provides code examples to use RTC Alarm with interrupt.

1. RTC definition

A real-time clock (RTC) is an independent binary-coded decimal (BCD) timer/counter. For that, the RTC provides a time-of-day clock/calendar with programmable alarm interrupt. Also, the RTC can provide an automatic wakeup to manage all low-power modes. The STM32L476 integrated RTC peripheral can be used for different main features are the following:

  • Calendar with subseconds, seconds, minutes, hours, day, date of day in month, month and year.
  • Daylight saving compensation programmable by software.
  • Programmable alarm with interrupt function.
  • Automatic wakeup unit generating a periodic flag that triggers an automatic wakeup interrupt.
  • Reference clock detection: a more precise second source clock (50 or 60 Hz) can be used to enhance the calendar precision.
  • Accurate synchronization with an external clock using the subsecond shift feature.
  • Digital calibration circuit (periodic counter correction).
  • Time-stamp function for event saving.
  • Tamper detection event with configurable filter and internal pull-up.
  • 32 backup registers.
  • Maskable interrupts/events:

- Alarm A
- Alarm B
- Wakeup interrupt
- Time-stamp
- Tamper detection

2. Configure RTC and Alarm with interrupt

2.1. Objectives

The objectives of this wiki article are to know how to setup RTC with interrupt in STM32CubeIDE and how to create a simple RTC project with periodic alarm interrupt.

2.2. How

Configure the LED pin and the RTC alarm interrupts in STM32CubeIDE and generate code.
Verify the correct functionality by periodic RTC alarm interrupts and by toggle the LED.

2.3. Create the project in STM32CubeIDE

  • File>New>STM32 Project in main panel.

create STM32CubeIDE project.png
In this example the NUCLEO-L476RG board is used to test RTC Alarm with interrupt.

  • For that, Select NUCLEO-L476RG board using Board Selector as shown in the below figure.

Select NUCLEO-L476RG board.png
In case you haven't downloaded the STM32L476 Cube library, it will be downloaded automatically, it may take some time.
Once the download is done, you can select NUCLEO-L476RG in board Selector.

  • Enter a name for the project, for example “RTC_And_Alarm_With_Interrupt”.

create project name.png

  • Initialize all peripherals with their default settings.

Answer “Yes” to initialize all peripherals with their default mode? Popup as below:
Popup.png

2.4. RTC Configuration

  • Set Internal Alarm on Alarm A.
  • Modify the seconds Alarm value to 1 in the parameter settings to set first Alarm to 1s.

RTC configuration.png

  • Enable alarm interrupt.

To enable the alarm interrupt, it is necessary to refer to the reference manual and precisely vectors table to choose the correct interrupt RTC alarm.
For the STM32L476 the RTC alarm interrupt is connected to EXTI line as shown below.
NVIC interruption.png

2.5. GPIO configuration

Green Led of NUCLEO-L476RG board is connected to PA5. Configure it in output push-pull to toggle as alarm indication.
GPIO configuration1.png
File:GPIO configuration2.png

2.6. Generate source code

  • Click "Ctrl+S" to generate the project.

Generate project.png

2.7. Edit main.c

  • Add these lines of code to toggle the LED to indicate the RTC alarm is done between USER CODE BEGIN 4 and USER CODE END 4.



[[category:Getting_started_with_STM32_system_peripherals | 15]]