STM32StepByStep:Step3 Introduction to the UART: Difference between revisions


Latest revision as of 15:21, 27 May 2024

UART and new board introductionClock.png 34min

Target description
Following this tutorial, you will:

  • get familiar with the L475 IoT Node Discovery board,
  • learn how to program and use a RS232 serial link on:
    • the previously used NUCLEO-L476RG board
    • the L475 IoT Node Discovery board (B-L475E-IOT01A ).

Prerequisites


Hardware
The hardware requirements to start the application are the following:

  • NUCLEO-L476RG[1] board (64-pin)
  • STM32L4 Discovery kit IoT node[2] (B-L475E-IOT01A )
  • USB cables Type-A to Mini-B and Type-A to Micro-B


1. Introduction to the UART I/F on NUCLEO-L476RG

Clock.png 12min
Create NUCLEO-L476RG UART project using STM32CubeMX

  • Create a new project using STM32CubeMX.
  • Select NUCLEO-L476RG board using Board Selector.
  • Answer Yes to Initialize all peripherals with their default mode ? popup.
  • In Pinout view tab, check that USART2 mode is configured to Asynchronous, PA2 is connected to USART2_TX and PA3 is connected to USART2_RX.

UART setup.png

  • Click on USART2 button in Configuration tab and set Word Length to 8 Bits.
  • Make sure that the settings are as in the screenshot below:

UART setup2.png

  • Disable all other USARTs.
  • Switch to the Project Manager tab and select STM32CubeIDE as Toolchain / IDE and give a name to your project.
  • Click on Generate Code and accept to open your project in STM32CubeIDE.

Edit and compile the NUCLEO-L476RG UART project using STM32CubeIDE

  • Open main.c in Project Explorer / myproject / Src / main.c.
  • Insert the following lines between /* USER CODE BEGIN 3 */ and /* USER CODE END 3 */:
uint8_t Test[] = "Hello World !!!\r\n"; //Data to send
HAL_UART_Transmit(&huart2,Test,sizeof(Test),10);// Sending in normal mode
HAL_Delay(1000);
  • Click on Build button Built Button.png to compile the project.
  • Click in Debug button Debug Button.png to run the software.
  • Open a console emulator such as TeraTerm[3]. Configure the console baud rate and data bits length. the COM Port name may differ on your PC.
  • STM32CubeIDE opens Debug perspective. Click on Resume button Resume Button.png to execute your code.
  • TeraTerm[3] displays Hello World !!! string confirming you were able to program and use RS232.

TeraTerm Setup.png

2. Introduction to the UART I/F on B-L475E-IOT01A (IoT Node)

Clock.png 22min
Quick view
The B-L475E-IOT01A Discovery kit[2] for IoT node allows the users to develop applications with direct connection to cloud servers.
Key features
The Discovery kit enables a wide diversity of applications by exploiting low-power communication, multiway sensing and Arm® Cortex®-M4 core-based STM32L4 Series features.

Create B-L475E-IOT01A UART project using STM32CubeMX

  • Create a new project using STM32CubeMX.
  • Select B-L475E-IOT01A board using Board selector.
  • Answer Yes to Initialize all peripherals with their default Mode ? popup.
  • Verify in Pinout tab that USART1 mode is configured to Asynchronous.
  • USART1 conflicts can be solved by (1) disabling all unnecessary features (I2C, LCD, SAI, SPI, UART, USART2) and (2) setting the pins PA9 and PB7 to reset state.

UART issue.png

  • Click on USART1 button in Configuration tab and set Word Length to 8 Bits, baud rate to 115200 Bits/s, Parity to None and Stop Bits to 1 as shown below.

UART setup2.png

  • Switch to the Project Manager tab and select STM32CubeIDE as Toolchain / IDE and give a name to your project.
  • Click on Generate Code and accept to open the project in STM32CubeIDE.

Edit and compile B-L475E-IOT01A UART project using STM32CubeIDE

  • Open main.c in Project Explorer / myproject / Src / main.com.
  • Insert the following lines between /* USER CODE BEGIN 3 */ and /* USER CODE END 3 */:
uint8_t Test[] = "Hello World !!!\r\n"; //Data to send
HAL_UART_Transmit(&huart1,Test,sizeof(Test),10);// Sending in normal mode
HAL_Delay(1000);
  • Click on Build button Built Button.png to compile the project.
  • Click on Debug button Debug Button.pngto run the software.
  • Open a console emulator such as TeraTerm[3]. Configure the console baud rate and data bits length. The COM Port name may differ on your PC.
  • STM32CubeIDE opens Debug perspective. Click on Resume Resume Button.png button to execute your code.
  • TeraTerm[3] displays Hello World !!! string confirming you were able to program and use RS232.

TeraTerm Setup.png

Now you are able to:

  • use the UART I/F on NUCLEO-L476RG
  • use the L475 IoT Node Discovery board
  • use the UART I/F on L475 IoT Node Discovery board

3. References