This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The following pages link to Template:Warning:
Displayed 100 items.
- How to record audio (transclusion) (← links)
- How to debug OP-TEE (transclusion) (← links)
- SPI device tree configuration (transclusion) (← links)
- ST-LINK (transclusion) (← links)
- How to configure OP-TEE (transclusion) (← links)
- Modify, rebuild and reload a firmware (transclusion) (← links)
- How to compile the device tree with the Distribution Package (transclusion) (← links)
- I2S device tree configuration (transclusion) (← links)
- IKS01Ax MEMS expansion board (transclusion) (← links)
- Android application frameworks overview (transclusion) (← links)
- STM32CubeIDE (transclusion) (← links)
- BSEC device tree configuration (transclusion) (← links)
- DDRCTRL and DDRPHYC device tree configuration (transclusion) (← links)
- STM32MP15 distribution for Android release note (transclusion) (← links)
- How to define your low-power strategy (transclusion) (← links)
- Package repository for OpenSTLinux distribution (transclusion) (← links)
- How to configure flash memory for TF-A BL2 (transclusion) (← links)
- Wrapper for FSBL images (transclusion) (← links)
- How to update OTP with U-Boot (transclusion) (← links)
- How to configure U-Boot for your board (transclusion) (← links)
- TFLite Cpp image classification (transclusion) (← links)
- TFLite Cpp object detection (transclusion) (← links)
- TFLite Python image classification (transclusion) (← links)
- TFLite Python object detection (transclusion) (← links)
- Coral Cpp image classification (transclusion) (← links)
- Coral Python image classification (transclusion) (← links)
- Coral Cpp object detection (transclusion) (← links)
- STPM4RasPI expansion board (transclusion) (← links)
- Coral Python object detection (transclusion) (← links)
- How to compile model and run inference on Coral Edge TPU using STM32MP1 (transclusion) (← links)
- How to run Coral Edge TPU inference using Python TensorFlow Lite API (transclusion) (← links)
- How to install the Yocto Project SDK in STM32CubeIDE (transclusion) (← links)
- How to manage OpenSTLinux projects in STM32CubeIDE (transclusion) (← links)
- How to read or write peripheral registers (transclusion) (← links)
- TAMP device tree configuration (transclusion) (← links)
- How to install Node-RED (transclusion) (← links)
- TFLite Cpp face recognition (transclusion) (← links)
- How to configure TF-A FIP (transclusion) (← links)
- IKS01A3 MEMS expansion board (transclusion) (← links)
- IKS01A2 MEMS expansion board (transclusion) (← links)
- HSEM device tree configuration (transclusion) (← links)
- DCMIPP device tree configuration (transclusion) (← links)
- STM32 MPU ROM code overview (transclusion) (← links)
- STM32MP13 V4L2 camera overview (transclusion) (← links)
- How to develop an X-Linux Expansion Package (transclusion) (← links)
- IPCC device tree configuration (transclusion) (← links)
- STM32MP15 OTP mapping (transclusion) (← links)
- STM32MP13 Discovery kits - Starter Package (transclusion) (← links)
- STM32MP13 Discovery kits - required material (transclusion) (← links)
- STM32MP135x-DK - board assembly (transclusion) (← links)
- STM32MP135x-DK - board connections (transclusion) (← links)
- STM32MP13 Discovery kits - starting for the first time (transclusion) (← links)
- How to measure performance of your NN models using the Coral Edge TPU (transclusion) (← links)
- How to measure performance of your NN models using TensorFlow Lite runtime (transclusion) (← links)
- STM32MP13 OTP mapping (transclusion) (← links)
- How to install OPC UA (transclusion) (← links)
- STM32MP13 backup registers (transclusion) (← links)
- How to use U-Boot stm32key command (transclusion) (← links)
- Secure Firmware Update (transclusion) (← links)
- OP-TEE OTP overview (transclusion) (← links)
- PKA device tree configuration (transclusion) (← links)
- SAES device tree configuration (transclusion) (← links)
- How to perform Secure Boot from Distribution package (transclusion) (← links)
- STM32MP1 Developer Package - OpenSTLinux BSP (transclusion) (← links)
- How to secure STM32 MPU (transclusion) (← links)
- TF-A BL2 Trusted Board Boot (transclusion) (← links)
- Calibration device tree configuration (transclusion) (← links)
- STM32MP135x-DK - hardware description (transclusion) (← links)
- How to build an example using libcoral API (transclusion) (← links)
- How to reproduce an example using PyCoral API (transclusion) (← links)
- How to create Signed FIT image from Distribution package (transclusion) (← links)
- STM32DDRFW-UTIL (transclusion) (← links)
- STM32DDRFW-UTIL release note (transclusion) (← links)
- STM32PRGFW-UTIL (transclusion) (← links)
- STM32PRGFW-UTIL release note (transclusion) (← links)
- How to measure the performance of your models using ONNX Runtime (transclusion) (← links)
- Secure Secret Provisioning (SSP) (transclusion) (← links)
- How to deploy SSP: a step-by-step approach (transclusion) (← links)
- ONNX Python image classification (transclusion) (← links)
- X-LINUX-AI OpenSTLinux Expansion Package (transclusion) (← links)
- ONNX Python object detection (transclusion) (← links)
- ONNX Cpp object detection (transclusion) (← links)
- Hardware Unique Key overview (transclusion) (← links)
- X-LINUX-AI Starter package (transclusion) (← links)
- X-LINUX-AI Developer package (transclusion) (← links)
- X-LINUX-AI Distribution package (transclusion) (← links)
- X-LINUX-AI OpenSTLinux Expansion Package - v5.0.0 (transclusion) (← links)
- STM32 MPU ecosystem release note - v5.0.0 (transclusion) (← links)
- How to measure performance of your NN models using TVM runtime (transclusion) (← links)
- TVM Python image classification (transclusion) (← links)
- TVM Cpp image classification (transclusion) (← links)
- X-LINUX-AWS Distribution package (transclusion) (← links)
- X-LINUX-AWS Starter package (transclusion) (← links)
- X-LINUX-AWS Expansion Package (transclusion) (← links)
- STM32CubeMP15 Package - Getting started (transclusion) (← links)
- STM32CubeMP13 Package - Getting started (transclusion) (← links)
- How to load and start STM32CubeMP13 applications via microSD card (transclusion) (← links)
- How to load and start STM32CubeMP13 applications via SNOR flash (transclusion) (← links)
- Introduction to THREADX (transclusion) (← links)
- X-LINUX-AZURE expansion package (transclusion) (← links)