STM32CubeIDE

Revision as of 14:47, 22 April 2020 by Registered User


This article will explain some of the basic things about STM32CubeIDE is an all-in-one multi-OS development tool, which is part of the STM32Cube software ecosystem. STM32CubeIDE is an advanced C/C++ development platform with peripheral configuration, code generation, code compilation, and debug features for STM32 microcontrollers and microprocessors. It is based on the ECLIPSE™/CDT framework and GCC toolchain for the development, and GDB for the debugging. It allows the integration of the hundreds of existing plugins that complete the features of the ECLIPSE™ IDE. STM32CubeIDE integrates all STM32CubeMX functionalities to offer all-in-one tool experience and save installation and development time.

1. Prerequisites[edit source]

The following tools are prerequisites for understanding the tutorial on this wiki page and developing an application based on the STM32MP1 Series:

  • STM32CubeIDE 1.1.0 or newer
  • STM32Cube_FW_MP 1.1.0 or newer
  • STM32CubeMX 5.4.0 or newer


2. Target status[edit source]

See the how to use the STM32CubeIDE target status.


3. Project structure[edit source]

When an MPU project is created, its structure is automatically made hierarchical. The project structure for single-core projects is flat. On the contrary, in a multi-core project, the hierarchical project structure is used. When the user creates or imports an MPU project, it consists of one root project together with sub-projects, referred to as MCU projects, for each core. A hierarchical structure example is shown below.

Hierarchical project structure


4. How to get started with STM32CubeIDE[edit source]

This section links to two different how to articles depending on if you are moving from SW4STM32 to STM32CubeIDE or if you are starting a new project with STM32CubeIDE.

4.1. How to get started with STM32CubeIDE from scratch[edit source]

How to get started with STM32CubeIDE from scratch.

4.2. How to move from SW4STM32 to STM32CubeIDE[edit source]

How to move from SW4STM32 to STM32CubeIDE.

5. FAQ[edit source]

How to copy/paste in the STM32CubeIDE console








6. STM32CubeIDE[edit source]

6.1. Overview[edit source]

From its release 1.1.0 available on www.st.com, STM32CubeIDE provides support for STM32 MPU family.

The features previously proposed in STM32-CoPro-MPU plugin for SW4STM32 IDE are now integrated within STM32Cube ecosystem meaning that now launching STM32CubeIDE, you can:

  • select an STM32 MPU or an STM32 MPU board,
  • configure it, thanks to embedded STM32CubeMX features
  • generate your project
  • compile it
  • debug it

This release addresses the Cortex®-M located inside the STM32MP1 Series.

It provides:

  • target status widget, useful to be aware of the target device when debugging in production mode
  • console management, for automatic port detection
  • Cortex®-M project creation, compilation and debug in two modes:
    • engineering mode, with Cortex®-M firmware download via JTAG/SWD
    • production mode, with Cortex®-M firmware download :
      • via Ethernet link to the LAN or point-to-point
      • via Ethernet-over-USB for point-to-point connection
  • remote target path project property (for production mode)
  • remote system explorer configuration


It is available on Linux® and Windows® platforms.

Info white.png Information
Note:

6.2. Eclipse perspectives[edit source]

6.2.1. Device configuration tool[edit source]

MX perspective provides STM32CubeMX feature for STM32 MPU family.

6.2.2. C/C++[edit source]

C/C++ perspective allows to build a cortex-M project for STM32MP1 boards.

6.2.3. Debug[edit source]

Debug configurations menu allows to select production or engineering mode.

6.3. Documentation[edit source]

Additional information about the STM32CubeIDE is available on www.st.com.