This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The OpenSTLinux BSP encompasses the following components:
- The boot chain based on TF-A and U-Boot
- The OP-TEE secure OS running on the Cortex-A in secure mode
- The Linux kernel running on the Cortex-A in non-secure mode
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.

OpenSTLinux BSP architecture overview