This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Starting, stopping and restarting Weston
Weston has its own systemd service (/lib/systemd/system/weston.service) to easily start, stop and restart Weston.
The following command stops the Weston service:
systemctl stop weston
The following command starts the Weston service:
systemctl start weston
The following command stops and then restarts the Weston service:
systemctl restart weston
2. Preventing Weston from automatically starting on boot
The Weston service is automatically started on boot as specified in /lib/systemd/system/weston.service.
The following command disables the automatic start of the Weston service:
systemctl disable weston
Note: The following command enables the automatic start of the Weston service:
systemctl enable weston