This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. How to setup Bluetooth[edit source]
1.1. Setup[edit source]
- Check that the driver has been probed correctly in the kernel log message
USART driver initialized [ 0.928711] 4000e000.serial: ttyS1 at MMIO 0x4000e000 (irq = 42, base_baud = 6046875) is a stm32-usart[ 0.923697] STM32
- Check the Bluetooth interface
UART BD Address: 43:43:A1:12:1F:AC ACL MTU: 1021:8 SCO MTU: 64:1 DOWN RX bytes:619 acl:0 sco:0 events:31 errors:0 TX bytes:410 acl:0 sco:0 commands:31 errors:0 Features: 0xbf 0xfe 0xcf 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: SLAVE ACCEPThciconfig -a hci0: Type: Primary Bus:
1.2. Initialize the Bluetooth interface[edit source]
UART BD Address: AA:AA:AA:AA:AA:AA ACL MTU: 1021:8 SCO MTU: 64:1 UP RUNNING RX bytes:1378 acl:0 sco:0 events:74 errors:0 TX bytes:1186 acl:0 sco:0 commands:74 errors:0 Features: 0xbf 0xfe 0xcf 0xfe 0xdb 0xff 0x7b 0x87 Packet type: DM1 DM3 DM5 DH1 DH3 DH5 HV1 HV2 HV3 Link policy: RSWITCH SNIFF Link mode: SLAVE ACCEPT Name: 'BlueZ 5.46' Class: 0x000000 Service Classes: Unspecified Device Class: Miscellaneous, HCI Version: 4.1 (0x7) Revision: 0x0 LMP Version: 4.1 (0x7) Subversion: 0x2209 Manufacturer: Broadcom Corporation (15)hciconfig hci0 up hciconfig -a hci0: Type: Primary Bus: