Last edited 4 years ago

Wayland Weston troubleshooting grid


Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


Some typical issues related to the Wayland / Weston framework are listed below. Solutions or debugging methods are proposed for these issues.

If your issue is not listed, try also looking in the articles in the Wayland/Weston or troubleshooting grids categories.


Symptom Resolution
 glmark2-es2-wayland 
[11380.091100] reserved_mem_unmap_user: vm_munmap failed
eglCreateWindowSurface failed with error: 0x3003
Error: eglCreateWindowSurface failed with error: 0x3003
Error: CanvasGeneric: Invalid EGL state
Error: main: Could not initialize canvas
 weston-simple-egl
[11380.091100] reserved_mem_unmap_user: vm_munmap failed
has EGL_EXT_buffer_age and EGL_EXT_swap_buffers_with_damage
weston-simple-egl: ../git/clients/simple-egl.c:440: create_surface: 
  Assertion `ret == EGL_TRUE' failed.
Aborted (core dumped)
 weston-simple-egl
has EGL_EXT_buffer_age and EGL_EXT_swap_buffers_with_damage
Segmentation fault (core dumped) 

Weston is using pixman software composition instead of GPU hardware composition. This may be because you have not accepted the EULA at the beginning of the build...

 cat /etc/default/weston
#Autogenerated
OPTARGS=--use-pixman

Please comment the content of the file /etc/default/weston or delete it.

 systemctl stop Weston
Failed to stop Weston.service: Unit Weston.service not loaded.

Please remove the capital letter in the word Weston. The correct command is

 systemctl restart weston