Registered User No edit summary |
Registered User mNo edit summary |
||
(40 intermediate revisions by 8 users not shown) | |||
Line 1: | Line 1: | ||
This article aims to describe the content of the release '''''STM32MP15-Ecosystem-v1.0.0''''' for ''STM32MPU Embedded Software distribution'' and its associated ecosystem. | This article aims to describe the content of the release '''''STM32MP15-Ecosystem-v1.0.0''''' for ''STM32MPU Embedded Software distribution'' and its associated ecosystem. | ||
Line 38: | Line 31: | ||
==Licensing== | ==Licensing== | ||
'''This software package is licensed under SOFTWARE LICENSE AGREEMENT, the "SLA". Customer may not use this package except in compliance with the [[OpenSTLinux licenses#Top Software license agreement (SLA) and third-party licences|software license agreement (SLA)]].''' | '''This software package is licensed under SOFTWARE LICENSE AGREEMENT, the "SLA". Customer may not use this package except in compliance with the [[LegalInformation:OpenSTLinux licenses - v1.0.0#Top Software license agreement (SLA) and third-party licences|software license agreement (SLA)]].''' | ||
==Main features / main highlights== | ==Main features / main highlights== | ||
=== Boards === | === Boards === | ||
{| | |||
{|class="st_table" | |||
!Boards !! PCBs list !! Content !! Availability !! Distribution Package !! Starter Package !! Developper Package | !Boards !! PCBs list !! Content !! Availability !! Distribution Package !! Starter Package !! Developper Package | ||
|- | |- | ||
Line 70: | Line 64: | ||
==== Boot configurations ==== | ==== Boot configurations ==== | ||
* At boot, you can select two kernel configurations: | * At boot, you can select two kernel configurations: | ||
** Configuration 1: All internal peripherals assigned to Cortex-A7 for Linux drivers, Cortex-M4 | ** Configuration 1: All internal peripherals assigned to Cortex-A7 for Linux drivers, Cortex-M4 coprocessing firmware TTY executed by default | ||
** Configuration 2: Some internal peripherals assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see ([[STM32CubeMP1 Package#How to run the Examples|How to run Cortex-M4 examples]]). | ** Configuration 2: Some internal peripherals assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see ([[STM32CubeMP1 Package#How to run the Examples|How to run Cortex-M4 examples]]). | ||
Line 115: | Line 109: | ||
* Application can activate Low power modes (STOP and STANBY) | * Application can activate Low power modes (STOP and STANBY) | ||
* Develop Linux application, libraries, kernel modules based on OpenSTLinux delivery | * Develop Linux application, libraries, kernel modules based on OpenSTLinux delivery | ||
* Develop Cube application with | * Develop Cube application with coprocessing link based on Cube delivery | ||
* Prototype some applications based on ST boards | * Prototype some applications based on ST boards | ||
* Stress available features | * Stress available features | ||
Line 141: | Line 135: | ||
* Exhaustive restriction lists are available in the release notes of each delivery. | * Exhaustive restriction lists are available in the release notes of each delivery. | ||
* See sections [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]] and [[#Referenced tools release notes |Referenced tools release notes ]]. | * See sections [[#STM32MPU Embedded Software distribution detailed release notes|STM32MPU Embedded Software distribution detailed release notes]] and [[#Referenced tools release notes |Referenced tools release notes ]]. | ||
* Implemented SW workarounds information in STM32MP15-Ecosystem-v1.0.0 release based on workarounds proposed in STM32MP15xx device errata. See [[ | * Implemented SW workarounds information in STM32MP15-Ecosystem-v1.0.0 release based on workarounds proposed in STM32MP15xx device errata. See [[STM32MP15_ecosystem_errata_sheet]] | ||
==Minor release updates== | |||
STMicroelectronics regularly delivers corrections through github<sup>®</sup> components which are [https://github.com/STMicroelectronics/u-boot/ u-boot], [https://github.com/STMicroelectronics/optee_os optee-os], [https://github.com/STMicroelectronics/arm-trusted-firmware tf-a], [https://github.com/STMicroelectronics/linux Linux kernel]. <br> | |||
You can decide to incorporate them into your developer package (please refer to [[STM32MP1 Developer Package]]) or Distribution package.<br/> | |||
For updating Distribution package please proceed as follow: | |||
:# [[OpenSTLinux_distribution#Reference_source_code| Switch to github<sup>®</sup> mode]] your Distribution package | |||
:# Use the command ''' [[OpenEmbedded_-_devtool#devtool_modify|devtool modify]] <recipe name>''' to have direct access to source code git used by build process | |||
:# In source code just extracted, use git command as '''git checkout -b WORK <github<sup>®</sup> TAG>''' to points on new revision of component | |||
More rarely and independently, STMicroelectronics also delivers fixes on layers through github<sup>®</sup>. These changes can be integrated (via [[git]] commands) into your local [[STM32MP1 Distribution Package]] environment. Please find below the github<sup>®</sup> links of the quoted layers : | |||
* [https://github.com/STMicroelectronics/meta-st-stm32mp/ meta-st-stm32mp] | |||
* [https://github.com/STMicroelectronics/meta-st-openstlinux/ meta-st-openstlinux ] | |||
* [https://github.com/STMicroelectronics/meta-st-stm32mp-addons/ meta-st-stm32mp-addons] | |||
===v1.0.1=== | |||
[[STM32MP15_OpenSTLinux_release_note_-_v1.0.0#v1.0.1 |OpenSTLinux updates v1.0.1]]<br> | |||
[[STM32CubeMP1_Package_release_note_-_v1.0.0#STM32CubeMP1 Package v1.0.1|STM32CubeMP1 updates v1.0.1]]<br> | |||
===v1.0.2=== | |||
[[STM32MP15_OpenSTLinux_release_note_-_v1.0.0#v1.0.2 |OpenSTLinux updates v1.0.2]]<br> | |||
===v1.0.3=== | |||
[[STM32MP15_OpenSTLinux_release_note_-_v1.0.0#v1.0.3 |OpenSTLinux updates v1.0.3]]<br> | |||
===v1.0.4=== | |||
[[STM32MP15_OpenSTLinux_release_note_-_v1.0.0#v1.0.4 |OpenSTLinux updates v1.0.4]]<br> | |||
===v1.0.5=== | |||
[[STM32MP15_OpenSTLinux_release_note_-_v1.0.0#v1.0.5 |OpenSTLinux updates v1.0.5]]<br> | |||
==Reference documents== | ==Reference documents== | ||
{{:STM32MP15 resources - v1.0.0}} | {{:STM32MP15 resources - v1.0.0}} | ||
{{ReviewsComments | UM2534.pdf : dead link to .pdf}} | |||
== How to get the software and start with this release? == | == How to get the software and start with this release? == | ||
Line 161: | Line 185: | ||
*'''Build''' an embedded software | *'''Build''' an embedded software | ||
{| class="st-table" style="text-align: center;" | |||
{| class=" | |||
|- | |- | ||
! style="width: 50%; text-align: center;" | Board part number | ! style="width: 50%; text-align: center;" | Board part number | ||
! style=" width:50%" | Jump to | ! style=" width:50%; text-align: center;" | Jump to | ||
|- | |- | ||
| '''STM32MP157C-EV1'''<br>Evaluation board | | '''STM32MP157C-EV1'''<br>Evaluation board | ||
|| [[STM32MP15 Evaluation boards - getting started|STM32MP15 Evaluation boards - getting started, including software download]] | || [[STM32MP15 Evaluation boards - getting started|STM32MP15 Evaluation boards - getting started, including software download]] | ||
|- | |- | ||
| '''STM32MP157X-DKX'''<br>Discovery kit | | '''STM32MP157X-DKX'''<br>Discovery kit | ||
|| [[STM32MP15 Discovery kits - getting started|STM32MP15 Discovery kits - getting started, including software download]] | || [[STM32MP15 Discovery kits - getting started|STM32MP15 Discovery kits - getting started, including software download]] | ||
Line 179: | Line 202: | ||
The release notes does not explain how to get software. For that, refer chapter [[#How to get the software and start with this release?|How to get the software and start with this release ]] | The release notes does not explain how to get software. For that, refer chapter [[#How to get the software and start with this release?|How to get the software and start with this release ]] | ||
{|class="st-table" style="width: 98%;" | |||
{|class=" | |||
|- | |- | ||
! '''Firmware''' | |||
! '''Release note''' | |||
! '''Version''' | |||
|- | |- | ||
| OpenSTLinux Distribution | |||
| [[STM32MP15 OpenSTLinux release note - v1.0.0]] | |||
| openstlinux-4.19-thud-mp1-19-02-20 | |||
|- | |- | ||
| STM32Cube MPU Package | |||
| [[STM32CubeMP1 Package release note - v1.0.0]] | |||
| STM32CubeMP1-V1.0.0 | |||
|} | |} | ||
Line 202: | Line 224: | ||
The set of tools to be downloaded depends on the Package to be used (double check [[Which Package better suits your needs]] article to find more information on each Package). | The set of tools to be downloaded depends on the Package to be used (double check [[Which Package better suits your needs]] article to find more information on each Package). | ||
{|class=" | {|class="st-table" style="text-align:center; width:95%; cellspacing=0" | ||
|- | |- | ||
! style="text-align:center;" rowspan="2" | '''Tools''' | |||
! style="text-align:center;" rowspan="2" | '''Release notes''' | |||
! style="text-align:center;" colspan='2' | ''' Host PC''' | |||
! style="text-align:center;" colspan='3' | '''Which Package may need the tool ?''' | |||
|- | |- | ||
| | | '''Linux version''' | ||
| '''Windows version''' | |||
| ''' Starter Package''' | |||
| | | ''' Developer Package''' | ||
| | | ''' Distribution Package''' | ||
| | |||
| | |||
|- | |- | ||
| STM32CubeProgrammer | |||
| [[STM32CubeProgrammer release note]] | |||
| 2.0.0 | |||
| 2.0.0 | |||
| <span style="font-size:21px">☑</span> | |||
| <span style="font-size:21px">☐</span> | |||
| <span style="font-size:21px">☑</span> | |||
|- | |- | ||
| STM32-CoPro-MPU plug-in for SW4STM32 IDE | |||
| [[STM32-CoPro-MPU plugin release note]] | |||
| 1.0.0 | |||
| 1.0.0 | |||
| <span style="font-size:21px">☐</span> | |||
| <span style="font-size:21px">☑</span> | |||
| <span style="font-size:21px">☐</span> | |||
|- | |- | ||
| STM32CubeMX | |||
| [https://www.st.com/en/development-tools/stm32cubemx.html STM32CubeMX release note] | |||
| from 5.1 | |||
| from 5.1 | |||
| <span style="font-size:21px">☐</span> | |||
| <span style="font-size:21px">☑</span> | |||
| <span style="font-size:21px">☑</span> | |||
|- | |- | ||
| Keygen | |||
| [[KeyGen release note]] | |||
| 1.0.0 | |||
| 1.0.0 | |||
| <span style="font-size:21px">☑</span> | |||
| <span style="font-size:21px">☑</span> | |||
| <span style="font-size:21px">☑</span> | |||
|- | |- | ||
| Signing tool | |||
| [[Signing tool release note]] | |||
| 1.0.0 | |||
| 1.0.0 | |||
| <span style="font-size:21px">☑</span> | |||
| <span style="font-size:21px">☑</span> | |||
| <span style="font-size:21px">☑</span> | |||
|} | |} | ||
Line 264: | Line 283: | ||
==References== | ==References== | ||
<references/> | <references/> | ||
<noinclude> | |||
{{PublicationRequestId | Auto}} | |||
[[Category:Release notes archives]] | |||
</noinclude> |
Latest revision as of 11:49, 2 April 2020
This article aims to describe the content of the release STM32MP15-Ecosystem-v1.0.0 for STM32MPU Embedded Software distribution and its associated ecosystem.
1. Delivery purpose and scope[edit source]
The purpose of this delivery is the Mass Market release, aka STM32MP1-V1.0.0, provided to STMicroelectronics customers.
The scope of this ecosystem delivery, dedicated to STM32MP15 devices, is:
- The STM32MPU Embedded Software distribution:
- The OpenSTLinux distribution running on the Arm® Cortex®-A7 processor(s)
- The STM32Cube MPU Package running on the Arm® Cortex®-M4 processor
- The associated tools: : Referenced tools
- STM32-CoPro-MPU Eclipse plugin
- STM32CubeMX
- STM32CubeProgrammer
- Keygen
- Signing tool
- The documentation:
- This user guide (wiki format)
- Documentation package : Reference_documents
- The supported boards: Boards
- STM32MP15 Evaluation board
- STM32MP15 Discovery kit
Aim of this release:
- To provide a full ecosystem for STM32MP15x devices.
- To work efficiently with STM32MP15 boards, using one of the Packages developed by STMicroelectronics for STM32 MPU devices (Starter Package, Developer Package, Distribution Package). See Which Package better suits your needs for more information on these Packages.
2. Intended audience[edit source]
The targeted audience consists in STMicroelectronics customers.
3. Licensing[edit source]
This software package is licensed under SOFTWARE LICENSE AGREEMENT, the "SLA". Customer may not use this package except in compliance with the software license agreement (SLA).
4. Main features / main highlights[edit source]
4.1. Boards[edit source]
Boards | PCBs list | Content | Availability | Distribution Package | Starter Package | Developper Package |
---|---|---|---|---|---|---|
EVAL Rev.C | MB1263C (Daughter) + MB1262C (Mother) + MB1230C (Display) + MB1379A (Camera) |
STM32MP1 STM32MP157AAA3 Rev.B PMIC STPMIC1APQR cut1.2 external oscillator |
Jan'19 | Machine stm32mp1-boards-revc for all flashs Machine stm32mp1-eval-revc for SDCard |
EVAL Rev.C Starter Package | EVAL Rev.C Developer Package |
DISCO Rev.C | MB1272C (Mother) + MB1407B (Display) |
STM32MP1 STM32MP157CAC3 Rev.B PMIC STPMIC1APQR cut1.2 external oscillator |
Jan'19 | Machine stm32mp1-boards-revc for all flashs Machine stm32mp1-disco-revc for SDCard |
DISCO Rev.C Starter Package | DISCO Rev.C Developer Package |
- Warning STLINK in EVAL and DISCO Rev.C boards integrates the latest firmware STLINK (V2J32M22) which requires upgraded USB PC drivers - new Windows USB driver
4.2. Embedded software[edit source]
4.2.1. Cortex-A7 Linux software[edit source]
- STM32MP15 microprocessor support with following components:
- Kernel version LTS v4.19.9
- TF-A version v2.0
- U-Boot version v2018.11
- OP-TEE version v3.3.0
- openOCD version v0.10.0
- Build process
- OpenEmbedded Thud (v2.6)
- GCC version v8.2
- Applicative components
- Weston version v5.0.0
- GStreamer version v1.14.2
- GCnano version v6.2.4
4.2.2. Boot configurations[edit source]
- At boot, you can select two kernel configurations:
- Configuration 1: All internal peripherals assigned to Cortex-A7 for Linux drivers, Cortex-M4 coprocessing firmware TTY executed by default
- Configuration 2: Some internal peripherals assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see (How to run Cortex-M4 examples).
- Configuration 1 activated by default if you do not specify 2 in the console at boot.
4.2.3. Cortex-M4 Cube firmware[edit source]
- The STM32Cube HAL, STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
- Low-layer APIs (LL) offering a fast lightweight expert-oriented layer that is closer to the hardware than the HAL. LL APIs are available only for a set of peripherals.
- A consistent set of middleware components such as FreeRTOS, OpenAMP.
- All embedded software utilities, delivered with a full set of examples.
4.3. STM32CubeProgrammer, Signing tool, Key gen[edit source]
- Flashload SDCard, eMMC, NAND, NOR images through USB and UART for EV1, DK1, DK2 boards
- Private and public keys generation
- Images signature with hash public key
- Flashlayout file format change
- STM32MP1 fuses management (with console interface only)
- PMIC NVM management (with console interface only)
4.4. STM32CubeMX[edit source]
4.5. SW4STM32 IDE[edit source]
STM32-CoPro-MPU plug-in integrated in SW4STM32 IDE covers the Arm Cortex-M4 development and debug with:
- SW4STM32 plug-in to support Cortex-M4 STM32CubeMP1 in Production mode and Engineering mode
- Cortex-M4 Firmware compilation, Load, Debug
- PC Linux with Ethernet (recommended) or serial link
- PC Windows with Ethernet or Ethernet over USB link
- Cortex-M4 Firmware installation directory configurable
This plug-in is delivered with SW4STM32 from version 2.8.0 SW4STM32 release note
Note: To use delivered Cortex-M4 examples per ST board, the user needs to enable Cortex-M4 examples device tree configuration using U-Boot
4.6. Miscellaneous[edit source]
- Detailed features are available in the release notes of the different items constituting this delivery.
- See sections STM32MPU Embedded Software distribution detailed release notes , Referenced tools release notes and Reference documents
5. Recommendations of use[edit source]
5.1. Safe[edit source]
- Develop board based on STM32MP1
- Flashload and boot from all flashes SDCard, eMMC, NAND ONFI, NOR
- Application can activate Low power modes (STOP and STANBY)
- Develop Linux application, libraries, kernel modules based on OpenSTLinux delivery
- Develop Cube application with coprocessing link based on Cube delivery
- Prototype some applications based on ST boards
- Stress available features
5.2. Not recommended[edit source]
6. Main restriction list[edit source]
6.1. Boards[edit source]
- None
6.2. Embedded software[edit source]
- Some modes proposed in CubeMX for Cortex-A7 non secure context not supported in Cortex-A7 secure context. See details in STM32MP15_OpenSTLinux_release_note_-_v1.0.0#Main_restrictions_list
6.3. STM32CubeProgrammer, signing tool, key generator[edit source]
- None
6.4. STM32CubeMX[edit source]
6.5. SW4STM32 IDE[edit source]
- None
6.6. Miscelleanous[edit source]
- Exhaustive restriction lists are available in the release notes of each delivery.
- See sections STM32MPU Embedded Software distribution detailed release notes and Referenced tools release notes .
- Implemented SW workarounds information in STM32MP15-Ecosystem-v1.0.0 release based on workarounds proposed in STM32MP15xx device errata. See STM32MP15_ecosystem_errata_sheet
7. Minor release updates[edit source]
STMicroelectronics regularly delivers corrections through github® components which are u-boot, optee-os, tf-a, Linux kernel.
You can decide to incorporate them into your developer package (please refer to STM32MP1 Developer Package) or Distribution package.
For updating Distribution package please proceed as follow:
- Switch to github® mode your Distribution package
- Use the command devtool modify <recipe name> to have direct access to source code git used by build process
- In source code just extracted, use git command as git checkout -b WORK <github® TAG> to points on new revision of component
More rarely and independently, STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands) into your local STM32MP1 Distribution Package environment. Please find below the github® links of the quoted layers :
7.1. v1.0.1[edit source]
OpenSTLinux updates v1.0.1
STM32CubeMP1 updates v1.0.1
7.2. v1.0.2[edit source]
7.3. v1.0.3[edit source]
7.4. v1.0.4[edit source]
7.5. v1.0.5[edit source]
8. Reference documents[edit source]
All the resources for the STM32MP1 Series are in the Resources area of the STM32MP1 Series web page.
The resources below are referenced in some of the articles in this user guide for the STM32MP1 Series.
Reference | Name | Link | Version |
---|---|---|---|
Application notes | |||
AN5031 | Getting started with STM32MP15 Series hardware development | AN5031.pdf | v1.0 |
AN5109 | STM32MP1 Series using low-power modes | AN5109.pdf | v1.0 |
AN5253 | Migration of microcontroller applications from STM32F4x9 lines to STM32MP15x lines microprocessor | AN5253.pdf | v1.0 |
AN5122 | STM32MP1 Series DDR memory routing guidelines | AN5122.pdf | v1.0 |
AN5168 | STM32MP1 series DDR configuration | AN5168.pdf | v1.0 |
Datasheets[1] | |||
DS12505 | STM32MP157Cxx datasheet (secure) |
DS12505.pdf | v1.0 |
DS12504 | STM32MP157Axx datasheet (basic) |
DS12504.pdf | v1.0 |
DS12503 | STM32MP153Cxx datasheet (secure) |
DS12503.pdf | v1.0 |
DS12502 | STM32MP153Axx datasheet (basic) |
DS12502.pdf | v1.0 |
DS12501 | STM32MP151Cxx datasheet (secure) |
DS12501.pdf | v1.0 |
DS12500 | STM32MP151Axx datasheet (basic) |
DS12500.pdf | v1.0 |
Errata sheets | |||
ES0438 | STM32MP15xx device errata | ES0438.pdf | v1.0 |
Reference manuals[1] | |||
RM0436 | STM32MP157xxx reference manual (STM32MP157xxx advanced Arm®-based 32-bit MPUs) |
RM0436.pdf | v2.0 |
RM0442 | STM32MP153xxx reference manual (STM32MP153xxx advanced Arm®-based 32-bit MPUs) |
RM0442.pdf | v2.0 |
RM0441 | STM32MP151xxx reference manual (STM32MP151xxx advanced Arm®-based 32-bit MPUs) |
RM0441.pdf | v2.0 |
Boards schematics | |||
MB1262 schematics | STM32MP157C-EV1 motherboard schematics (Evaluation board) |
MB1262C-01.pdf | vC-0.1 |
MB1263 schematics | STM32MP157C-EV1 daughterboard schematics (Evaluation board) |
MB1263C-01.pdf | vC-0.1 |
MB1230 schematics | DSI 720p LCD display daughterboard schematics (Evaluation board) |
MB1230B-02.pdf | vB-0.2 |
MB1379 schematics | Camera daughterboard schematics (Evaluation board) |
MB1379A-01.pdf | vA-0.1 |
MB1272 schematics | STM32MP157x-DKx motherboard schematics (Discovery kit) |
MB1272C-01.pdf | vC-0.1 |
MB1407 schematics | STM32MP157x-DKx daughterboard schematics (Discovery kit) |
MB1407C-01.pdf | vB-0.1 |
Boards user manuals | |||
UM2535 | STM32MP157x-EV1 evaluation board user manual | UM2535.pdf | V1.0 |
UM2534 | STM32MP157x-DKx discovery board user manual | UM2534.pdf | V1.0 |
9. How to get the software and start with this release?[edit source]
The list of embedded software packages available for downloaded depends on the Package to be used.
More information can be found on STM32MPU Embedded Software distribution and the supported Packages, at:
The table below provides the available board part numbers and the source of information in order to:
- Get started with one of the three available Packages (Starter, Developer or Distribution Packages)
- Get started with the board
- Find the associated embedded software distributions
- Download source code
- Build an embedded software
Board part number | Jump to |
---|---|
STM32MP157C-EV1 Evaluation board |
STM32MP15 Evaluation boards - getting started, including software download |
STM32MP157X-DKX Discovery kit |
STM32MP15 Discovery kits - getting started, including software download |
10. STM32MPU Embedded Software distribution detailed release notes[edit source]
The table below lists the software packages available in the STM32MPU Embedded Software distribution, and provides the corresponding release notes.
The release notes provide more information and details about the features and content of each package.
The release notes does not explain how to get software. For that, refer chapter How to get the software and start with this release
Firmware | Release note | Version |
---|---|---|
OpenSTLinux Distribution | STM32MP15 OpenSTLinux release note - v1.0.0 | openstlinux-4.19-thud-mp1-19-02-20 |
STM32Cube MPU Package | STM32CubeMP1 Package release note - v1.0.0 | STM32CubeMP1-V1.0.0 |
11. Referenced tools release notes[edit source]
The table below lists the available tools, and provides links to the respective release notes.
Each release note provides information on how to install and use the corresponding tool.
The set of tools to be downloaded depends on the Package to be used (double check Which Package better suits your needs article to find more information on each Package).
Tools | Release notes | Host PC | Which Package may need the tool ? | |||
---|---|---|---|---|---|---|
Linux version | Windows version | Starter Package | Developer Package | Distribution Package | ||
STM32CubeProgrammer | STM32CubeProgrammer release note | 2.0.0 | 2.0.0 | ☑ | ☐ | ☑ |
STM32-CoPro-MPU plug-in for SW4STM32 IDE | STM32-CoPro-MPU plugin release note | 1.0.0 | 1.0.0 | ☐ | ☑ | ☐ |
STM32CubeMX | STM32CubeMX release note | from 5.1 | from 5.1 | ☐ | ☑ | ☑ |
Keygen | KeyGen release note | 1.0.0 | 1.0.0 | ☑ | ☑ | ☑ |
Signing tool | Signing tool release note | 1.0.0 | 1.0.0 | ☑ | ☑ | ☑ |
12. Change log[edit source]
See detailed release notes for more information STM32MPU Embedded Software distribution detailed release notes and Referenced tools release notes .
13. References[edit source]
- ↑ Jump up to: 1.0 1.1 The part numbers are specified in STM32MP15 microprocessor part numbers