TTY tools

Revision as of 12:43, 21 February 2020 by Registered User
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

1. Article Purpose[edit source]

This article aims at giving some first information useful to start with the Linux® TTY tools. These tools are useful for interacting with TTY terminals.

2. Introduction[edit source]

These tools use TTY sysfs and character device directly (See TTY user space interface for further details).

3. Tools list[edit source]

Please find below a list of useful TTY tools provided by Linux® community:

  • fuser [1] - to identify processes using files or sockets.
  • inputattach [2] (based on termios API) - to attach a serial line to an input-layer device.
    Inputattach attaches a serial line to an input-layer device via a line discipline. Exactly one of the available modes must be specified on the command line.
  • kermit [3] - transport and platform independent interactive and scriptable communications software.
    C-Kermit is a modem program, a Telnet client, an Rlogin client, an FTP client, an HTTP client, and on selected platforms, also an X.25 client. It can make its own secure internet connections using IETF-approved security methods including Kerberos IV, Kerberos V, SSL/TLS, and SRP and it can also make SSH connections through an external SSH client application. It can be the far-end file-transfer or client/server partner of a desktop Kermit client. It can also accept incoming dialed and network connections. It can even be installed as an internet service on its own standard TCP socket, 1649 [RFC2839, RFC2840].
  • ldattach [4] (based on termios API) - to attach a line discipline to a serial line.
    The ldattach daemon opens the specified device file (which should refer to a serial device) and attaches the line discipline ldisc to it for processing of the sent and/or received data. It then goes into the background keeping the device open so that the line discipline stays loaded. The line discipline ldisc may be specified either by name or by number. In order to detach the line discipline, kill the ldattach process. With no arguments, ldattach prints usage information.
  • minicom [5] - friendly serial communication program.
    Minicom is a communication program which somewhat resembles the shareware program TELIX but is free with source code and runs under most Unices. Features include dialing directory with auto-redial, support for UUCP-style lock files on serial devices, a separate script language interpreter, capture to file, multiple users with individual configurations, and more.
  • setserial [6] - To get/set Linux serial port information.
    Setserial is a program designed to set and/or report the configuration information associated with a serial port. This information includes the I/O port and the IRQ used by a particular serial port, and whether or not the break key should be interpreted as the Secure Attention Key, and so on.
  • stty [7] (based on termios API) - to change and print terminal line settings.
  • tty [8] - to print the file name of the terminal connected to standard input
Info white.png Information
The descriptions above are provided by the manual pages of the tools.

4. Getting started[edit source]

Examples of TTY tools usage are handled in the following articles :

5. Installation on your target[edit source]

Some of the TTY tools aren't embedded by default in OpenSTLinux distribution. They can be compiled independently and then installed on the target (see Adding Linux user space applications).

6. References[edit source]