ADB

Revision as of 10:34, 12 September 2019 by Registered User

The Android Debug Bridge (ADB) is a versatile command-line tool that lets you communicate with a device (an emulator or a connected Android device).

This article is intended to a Developer Package or a Distribution Package user (see Which Package better suits your needs for more information).

ADB.png

  • The ADB client is an executable with a subcommand such as adb shell, adb logcat, etc.
  • The ADB server acts as a proxy between adb clients and adbd
  • The ADBD daemon is started by init on the target device

The target device can be connected using different solutions:


As soon as connected, it is possible to start testing your application with Android Studio.


It is also possible to execute all ADB commands (see ADB commands for more details).

For that purpose, you have to find the ADB tool within your environment: Host computer installation

1. Host computer installation[edit source]

ADB is available by default within Android Studio IDE (part of the Android SDK). It is available for Linux, Windows and OS X.


When required, it is possible to execute directly ADB commands within Android Studio Terminal.

It is required to go to the correct directory (<SDK path>/platform-tools)

cd <SDK path>
cd platform-tools

The <SDK path> can be determined by opening the SDK Manager (from Android Studio: "Tools/Android/SDK Manager" menu):

Android SDK Path

Info white.png Information
If you are using a Distribution Package, please refer to ADB for Distribution Package

2. Commands[edit source]

The ADB commands enable the execution of a variety of actions on the target device, such as installing and debugging apps. They also provide access to a Unix shell that you can use to run a variety of commands on a device.

See ADB commands summary for more information.

3. Device Connection[edit source]

3.1. How to connect over USB[edit source]

Several steps are required to connect your device:

3.1.1. Host computer configuration[edit source]

The required installation and configuration depends on the host computer OS used:

3.1.1.1. Linux Host (Ubuntu)[edit source]

In Linux environments, the Android USB drivers are built-in. The only action needed is to set the target device's information.

Info white.png Information
You need administration rights for this, you may need to add sudo in front of each executed command

For that purpose, you have to open a terminal and:

  • create (or update if already exists) the 51-android.rules file in /etc/udev/rules.d/ with the following information
    • idVendor = 0483 (STMicroelectronics vendor)
    • idProduct = 0adb (ADB on STMicroelectronics device)
    • Mode = 0666 (read/write permissions)
    • Group = plugdev (Unix group which owns the device node)
Info white.png Information
You can check if you are in the plugdev group executing the following command:
$ groups

Example:

# ADB on STMicroelectronics devices
SUBSYSTEM=="usb", ATTR{idVendor}=="0483", ATTR{idProduct}=="0adb", MODE="0660", GROUP="plugdev"
  • Ensure that the file created has the correct access rights:
 chmod a+r /etc/udev/rules.d/51-android.rules

At this stage, you have an USB driver correctly installed and configured.

3.1.1.2. Windows Host[edit source]

In Windows environments, it is required to install the USB driver and to set the target device's information.

Warning white.png Warning
Please, execute all the following instruction before installing the driver

Follow the instructions from the Android Studio website to get the USB driver: Get the Google USB Driver

Then, you have to:

  • edit the file android_winusb.inf available in the usb_driver directory and add under each section (ex: under [Google.NTx86] and under [Google.NTamd64]) the following data:
%SingleAdbInterface%        = USB_Install, USB\VID_0483&PID_0ADB
%CompositeAdbInterface%     = USB_Install, USB\VID_0483&PID_0ADB&MI_00
%SingleAdbInterface%        = USB_Install, USB\VID_0483&PID_0ADB&REV_0409
%CompositeAdbInterface%     = USB_Install, USB\VID_0483&PID_0ADB&REV_0409&MI_00

Depending on your Windows OS version, the driver installation procedure can differ: Installing a USB Driver

At this stage, you have an USB driver correctly installed and configured.

3.1.1.3. OS X Host[edit source]

In OS X environments, the Android USB drivers are built-in and it is not required to do any manual configuration.

At this stage, you have an USB driver correctly installed and configured.

3.1.2. Target device configuration[edit source]

Prerequisite: the target device is started with the ST Android distribution and you can access the Android user interface.


On the target device, you have to:

  • disconnect the USB cable between the target device and the host computer (if already connected)
  • find the Settings > Developer options configuration screen on your target device (If it is not visible, you must select Settings > About device and tap the Build number menu entry seven times).
  • enable the USB Debugging option from Settings > Developer options.
  • re-connect the USB cable between the target device and the host computer
  • if you see an alert on your target device requesting permission to "Allow USB debugging," click OK. It is recommended to check "Always allow from this computer" to avoid this step each time the target device is connected on the same host computer.

3.1.3. Check device connection[edit source]

First, ensure that the device is connected on the host computer using an USB cable and that the device is started.

Android Studio integrates a tool named Device Monitor (from Android studio: "Tools/Android/Android Device Monitor" menu). You can launch it and check that you can see the target device in the list (name of the device starting by stmicroelectronics).

Android Device Monitor


3.2. How to connect over Ethernet[edit source]

To use ADB over an Ethernet connection, you have to connect the host computer and the target device on the same network.

First, you have to follow instruction in How to connect over USB.

Then, you have to:

  • connect the USB cable between the target device and the host computer
  • open a terminal on your host computer
    • go to the <SDK path>/platform-tools/ directory (see Host computer installation to know how to get the <SDK path>)
    • execute adb shell ifconfig to get the target's IP address <device_ip_address>
    • execute adb tcpip 5555 to set the TCP/IP connection over port 5555
  • disconnect the USB cable between the target device and the host computer
  • execute adb connect <device_ip_address> to reconnect on the device through Ethernet

3.3. How to connect over Wi-Fi[edit source]

Follow the instructions from the Android Studio website: Connect to a device over Wi-Fi

4. ADB for Distribution Package[edit source]

4.1. Host computer installation[edit source]

By default, ADB is built when you compile the ST Android distribution. It is automatically added to your environment's $PATH.

Another possibility is to install ADB: apt-get install android-tools-adb, although this may be a hindrance to development if the ST Android distribution's and the OS's adb versions mismatch (the server is restarted every time it is used with a mismatched version of an adb client).


The device is not necessarily seen in the terminal when executing adb devices. You have to:

  • create a file within ~/.android/ directory named adb_usb.ini
  • add one line with the STMicrolectronics idVendor
0x0483

4.2. ADB implementation[edit source]

ADB's source code is stored in system/core/adb (common files between host and target device are differentiated by ADB_HOST tag).


Three properties are available for ADB (set within the device/stm/<BoardId>/device.mk):

  • persist.adb.trace_mask → used to enable or disable ADBD traces on target device (0x7FF for full trace, 0 to disable).
  • ro.adb.secure → used to enable or disable authentication mechanism (1 to enable authentication, 0 to disable), this property can not be modified dynamically. This property is considered only in case of eng or userdebug image builds. Otherwise, it is ignored (the authentication mechanism is enabled by default for user build).
  • service.adb.tcp.port → used to set TCP/IP port if a wireless connection is used (this property is not set by default as not required in case of USB)


ADB is an Android specific gadget device available in user space. It is required to mount functionfs as it is used to create this gadget device and register it to the USB Device Controller (UDC). Three endpoints are used (one for control, one for data input, one for data output).


It is also possible to create a composite device between ADB and other protocols using the configfs mechanism.

You can open the device/stm/<STM32Series>/<BoardId>/init.stm.usb.rc file to understand how the USB is configured for ADB and the file system/core/rootdir/init.usb.configfs.rc to understand what are the USB composite devices available (by default).


ADB over USB is the default configuration within the Android baseline with following properties set:

  • persist.adb.trace_mask: [0] → no ADB trace by default
  • ro.adb.secure: [1] → authentication mechanism enabled by default (need to accept connection through popup on target device)
  • persist.sys.usb.config: [adb] → USB ADB gadget device
  • sys.usb.config: [adb] → USB ADB gadget device
  • sys.usb.state: [adb] → USB ADB gadget device

It is possible to set the ADB over wireless connection within your distribution (Ethernet or Wi-Fi) by adding the following property in /device/stm/<STM32Series>/<BoardId>/device.mk:

PRODUCT_PROPERTY_OVERRIDES += service.adb.tcp.port=5555