This article describes how to populate completely or partially a board with a built STM32MPU distribution for Android™.
It is intended for Distribution Package users.
1. Prerequisites[edit source]
The environment must be installed using the Distribution Package adapted to your selected microprocessor device. See the list of Android Distribution Package.
You should also follow the PC prerequisites dedicated to Android to ensure all necessary packages to use the environment are present.
It is assumed that STM32CubeProgrammer tool has been installed (refer to STM32CubeProgrammer).
You have to build the STM32MPU distribution for Android™ adapted to your board (refer to How to build STM32MPU distribution for Android).
2. Populate a board[edit source]
The out/target/product/<BoardId>
directory contains all images built for board selected during the setup (lunch step).
out/target/product/<BoardId>
:
├── boot.img Binary forboot
partition(s) ├── dt.img Linux kernel device tree image fordt
partition(s) ├── fsbl-optee.img TF-A binary forfsbl
partition(s) (case optee boot mode) ├── fsbl-trusted.img TF-A binary forfsbl
partition(s) (case trusted boot mode) ├── fsbl-programmer.img TF-A binary used directly by the STM32CubeProgrammer ├── misc.img Binary formisc
partition ├── splash.img Binary forsplash
partition (splashscreen) ├── ssbl-optee-fbsd.img U-Boot binary forssbl
partition (case optee boot mode) ├── ssbl-trusted-fbsd.img U-Boot binary forssbl
partition (case trusted boot mode) ├── ssbl-programmer.img U-Boot binary used directly by the STM32CubeProgrammer ├── system.img Binary forsystem
partition(s) ├── teed.img Binary forteed
partition (OP-TEE OS paged data) ├── teeh.img Binary forteeh
partition (OP-TEE OS header image) ├── teex.img Binary forteex
partition (OP-TEE OS resident core) ├── userdata.img Binary foruserdata
partition ├── vendor.img Binary forvendor
partition(s) └── [...]
The STM32CubeProgrammer tool is used to flash the first stages of images to the board. Then fastboot is used to flash the remaining images.
The board shall be started in "Forced USB boot for flashing" mode (named also DFU), selecting it through boot switches as explained in the document <you board reference - hardware description, chapter Boot related switches (for example, Boot switches on the STM32MP157x-EV1 board for the STM32MP157C-EV1 board).
The board shall be connected through USB to your computer.
Depending on the board, several flash devices (microSD, eMMC and so on) might be available. The microSD card is considered as the Flash device in the rest of this article.
- Go to the distribution root directory, and run flash-device:
flash-device
- Select the flashlayout you want to use (ex: FlashLayout_sd_optee.tsv to flash OP-TEE build for microSD card)
1) FlashLayout_emmc_optee.tsv 3) FlashLayout_sd_optee.tsv 2) FlashLayout_sd_trusted.tsv 4) FlashLayout_emmc_trusted.tsv Which layout do you want to flash ?
Once the DFU flashing is terminated, the boot switches must be configured so that the Flash device (e.g. microSD card), on which the image has been flashed, is selected as the boot source.
- Press the reset button, and a long press on the button associated with fastboot (refer to LEDs and buttons on STM32 MPU boards). The device provisioning continue until the end.
- This operation takes several minutes.
- When the download is finished, press the reset button to reset the board. The Android software then starts.
3. Populate a SD card[edit source]
You can flash images directly to a SD card connected to your machine.
Before starting, you need to be sure that SD card settings match yours. Please refer to the Memory settings page.
3.1. Format the SD card[edit source]
The first time you use your SD card or if the partition layout changes, you need to format it. The goal is to prepare it with appropriate partition size to accept images.
format-device <device_path>
With:
- <device_path>: the device identify in your system to access your SD card. For example
/dev/sdb
for an USB connected SD card reader.
This command will automatically use the partition configuration from device/stm/<STM32Series>/layout/android_layout.config
.
For more information please see the usage option:
Usage: format-device [Options] <device_path> This script allows formatting memory device to create required partition before provisioning Options: -h/--help: print this message -v/--version: get script version -s/--size <disk-size>: set requested disk size [4GiB or 8GiB] (default: PART_MEMORY_SIZE value set in <path_to>/android_layout.config) -c/--config <config-file-path>: set used partition configuration file (default: <path_to>/android_layout.config) <device_path>: /dev/sdX (sd connected through usb), /dev/mmcblkX (sd connected through reader)
3.2. Provision the SD card[edit source]
To push the built images, you need to execute:
provision-device <device_path>
With:
- <device_path>: the device identify in your system to access your SD card. For example
/dev/sdb
for an USB connected SD card reader.
This will push all images to the SD card.
From this stage, you can plug your SD card on your board and reboot it.
4. Flash a dedicated image[edit source]
If you already have an Android distribution installed and booted on your board, it's possible to update partitions one by one depending on your needs. For example, if you rebuild the kernel you can just flash the boot (kernel), the dt (device tree) and the vendor images (modules).
First you need to restart your device in fastboot mode:
- Press the reset button, and a long press on the button associated with fastboot (USER PA13 for Evaluation board, USER2 for Discovery kits).
or
- Run the command
adb reboot-bootloader
Then execute the flashing command:
provision-device -i reboot
- -i option means that you will have to confirm the flash partition per partition (select the partitions you want to update)
- reboot option means that the device will reboot automatically at the end
5. Update an Android distribution[edit source]
If you want to update only partitions dedicated to Android (vendor
,system
or userdata
) after a rebuild, it's possible to use ADB tool.
You have first to switch read-only partitions to read-write:
adb root adb remount
You can then update the Android partitions.
adb sync
Finally, you have to reboot your device to take these changes into account
adb reboot