ADEB

Revision as of 12:59, 8 August 2019 by Registered User

This article shows how to install adeb for Distribution Package user.

It gives the step-by-step process to set up adeb for your system.

1. Article purpose[edit source]

This article is intended to a Distribution Package user (see Which Package better suits your needs for more information).

The adeb project installs a chroot environment on your Android device to help debugging. This article will show you how to install it on the board and how to use it to have BCC tools

2. Prerequisites[edit source]

Warning white.png Warning
You need to use a 8Gb SD card in order to be able to use adeb

The environment must be installed using the Distribution Package adapted to your selected microprocessor device, STM32MP1 Distribution Package for Android.

The kernel sources must have been dowload following How to build kernel for Android.

The following pacakge need to be install to generate adeb:

sudo apt-get install debootstrap qemu-user-static schroot

The following instructions should be launch from the distribution root directory STM32MP1 Distribution Package for Android, initialise your environment and then lunch:

source build/envsetup.sh

lunch aosp-eval-userdebug

3. Kernel preparation[edit source]

On first step you need to get the kernel source and compile it, like explain in more details How to build kernel for Android.

load_kernel

build_kernel

The compilation output will be in out-bsp/<SocId>/KERNEL_OBJ

3.1. Kernel customisation for BCC[edit source]

To be able to use tracepoint for BCC some change need to be done in the kernel. Apply the patch 0001-add-selinux-tracepoint.patch.

Warning white.png Warning
Fichier à télécharger !!!!!

cd device/stm/<SocId>-kernel/linux-<SocId>

git apply 0001-add-selinux-tracepoint.patch

Then rebuild the kernel and flash your board.

build_kernel

4. Adeb initialisation[edit source]

Retreive the adeb repository, and put it in the external folder from the distribution.

cd external

Clone the git.

git clone https://android.googlesource.com/platform/external/adeb

cd adeb

Have look at the adeb README.md[1] in case of trouble

Create a sym link to the adeb executable to make things easier

sudo ln -s $(pwd)/adeb /usr/bin/adeb

5. Adeb install[edit source]

Warning white.png Warning
You need to have a device power on with Android connected to the computer and accessible via ADB

adeb prepare --build --arch armhf --kernelsrc out-bsp/<SocId>/KERNEL_OBJ/

Info white.png Information
A sudo password may be requested

A chroot debian environment will be pushed on the board.

Once adeb installed, we can use it by running the following command:

adeb shell

6. Install BCC tools[edit source]

To install the BCC tools, some dependencies need to be install in the debian. Make sure your board has access to the internet to be able to retreive packages:

apt update

apt install git cmake clang-6.0 libclang-6.0-dev libelf-dev bison flex build-essential

Once all dependencies are installed, we can clone the BCC repository with the following command:

git clone https://github.com/iovisor/bcc

6.1. Adapt BCC[edit source]

By default, BCC is only working for 64-bits architecture and doesn't support arm 32-bits device.

cd bcc

git checkout 1a47a9a

Push the file 0001-arm-make-bcc-32-bits-compatible.patch

Warning white.png Warning
Fichier à télécharger !!!!!

adeb push 0001-arm-make-bcc-32-bits-compatible.patch

adeb shell

cd bcc

git apply 0001-arm-make-bcc-32-bits-compatible.patch

6.2. Compile BCC[edit source]

It is recommandes to create a swap to be able to compile BCC:

dd if=/dev/zero of=/data/swapfile bs=1M count=400

mkswap /data/swapfile

swapon /data/swapfile

Now, we can install the BCC's trace tool using CMake with the following command in the bcc repo root directory

mkdir build && cd build && CXX=/usr/bin/clang++-6.0 cmake .. -DCMAKE_INSTALL_PREFIX=/usr

make && make install

The BCC tools uses some kernel headers that needs to be provide in the androdeb environment.

To do so, push the kernel headers from the kernel source to the kernel-headers folder of the debian environment.

adeb push out-bsp/<SocId>/KERNEL_OBJ/usr/include/* /data/androdeb/debian/kernel-headers/include/

adeb push device/stm/<SocId>-kernel/linux-<SocId>/include/* /data/androdeb/debian/kernel-headers/include/


7. BCC's trace tool[edit source]

7.1. Install[edit source]

The BCC's trace tool auto-generates the code that will be compiled into eBPF.

This generated code uses kernel headers that are now incompatible with our patched BCC so we need to update the trace tool to use rewritten headers with our own types.

In the BCC repository, apply this patch '0001-trace-update-headers-to-make-trace-work-with-BCC-32-.patch' to fix the BCC's trace tool by running the following command:

Warning white.png Warning
Fichier à télécharger !!!!!

git apply 0001-trace-update-headers-to-make-trace-work-with-BCC-32-.patch

This patch simply replace the kernel header used in the generated eBPF code by our own rewritten headers with the define and struct needed by the generated code.

Then reinstall the trace tool by launching the following commands:

cd build

make && make install

7.2. Usage[edit source]

To launch the BCC's trace tool, simply run the following command:

trace -K -U 't:selinux:selinux_denied'

The BCC's trace tool should now print the user and kernel callstack every time a SELinux denied is raised.

8. Backup adeb[edit source]

It is possible to backup the adeb folder in order to deploy it faster next times.

8.1. Saving[edit source]

First you need to mount the userdata partition into your computer. Create the androdeb archive wherever you want:

tar -cpf androdeb.tar.bz2 <mount point>/data/androdeb

8.2. Setup[edit source]

Extract the previously created archive to the <mount point>/data/androdeb folder:

tar -xphf androdeb.tar.bz2

9. Limitation[edit source]

All the BCC tools that use kernel headers won't work without some modifications due to pointer size that need to be redefine. You need to apply the same kind of modifications like explain in #BCC's trace tool.