X-LINUX-AI-CV OpenSTLinux expansion package

Revision as of 15:59, 28 June 2019 by Registered User

Template:ArticleMainWriter Template:ArticleFirstDraftVersion


1. Description[edit source]

X-LINUX-AI-CV is a STM32 MPU OpenSTLinux expansion package that targets Artificial Intelligence for Computer Vision.
This package contains AI and Computer Vision Frameworks as well as application examples to start playing with some basic use cases.

File:STM32 MPU Embedded Software And X-LINUX-AI-CV Expansion Package.png.png
STM32MPU Embedded Software with the X-LINUX-AI-CV OpenSTLinux Expansion Package
OpenSTLinux OE legend.png

1.1. Current version[edit source]

X-LINUX-AI-CV v1.0.0

1.2. Contents[edit source]

  • Tensorflow Lite 2.0.0-alpha0
  • OpenCV 3.4.x
  • Python 3.5.x (enabling Pillow module)
  • Python Application examples
    • Image classification example based on MobileNet v1 model
    • Object detection example based on COCO SSD MobileNet v1 model

1.3. Software structure[edit source]

X-LINUX-AI-CV v1.0.0 Expansion Package Software structure

1.4. Supported hardware[edit source]

2. How to use it?[edit source]

2.1. Software installation[edit source]

2.2. needed material[edit source]

board, webCam


3. AI application examples[edit source]

3.1. Python TensorFlowLite applications[edit source]

This part provide python applications example based on TensorflowLite and OpenCV.
The applications integrate camera preview and test data picture that is then connected to the chosen TensorFlowLite model.

3.1.1. Image classification[edit source]

3.1.1.1. Description[edit source]

An image classification Neural Network model will allow you to identify what an image represents. It classify an image into various classes.

The label_tfl_multiprocessing.py python script is a multi-process python application for image classification.
The application enable OpenCV camera streaming (or test data pictures) and TensorFlowLite interpreter that run the NN inference based on the camera (or test data pictures) inputs.
The user interface is done thanks to python GTK.

3.1.1.2. How to use it[edit source]

The python scripts label_tfl_multiprocessing.py accepts different input parameters:

-i, --image          image directory with images to be classified
-v, --video_device   video device (default /dev/video0)
--frame_width        width of the camera frame (default is 640)
--frame_height"      height of the camera frame (default is 480)
--framerate          framerate of the camera (default is 30fps)
-m, --model_file     tflite model to be executed
-l, --label_file     name of file containing labels
--input_mean         input mean
--input_std          input standard deviation

To ease the launch of the python script, two shell scripts are available:

  • launch image classification based on camera frame inputs
 /usr/local/demo-ai/python/launch_python_label_tfl_mobilenet.sh
  • launch image classification based on the picture located in /usr/local/demo-ai/models/mobilenet/testdata directory
 /usr/local/demo-ai/python/launch_python_label_tfl_mobilenet_testdata.sh


3.1.1.3. Mobilenet V1[edit source]
3.1.1.3.1. Default model is Mobilenet V1 0.5 128 quant[edit source]

The default model use for tests is the mobilenet\_v1\_0.5\_128\_quant.tflite downloaded from https://www.tensorflow.org/lite/guide/hosted\_models.

3.1.1.3.2. Testing another Mobilenet V1 model[edit source]

You can test other models by downloading it directly on the STM32MP1 board. As example:

 curl http://download.tensorflow.org/models/mobilenet_v1_2018_02_22/mobilenet_v1_1.0_224_quant.tgz | tar xzv -C /usr/local/demo-ai/models/mobilenet/
 python3 /usr/local/demo-ai/python/label_tfl_multiprocessing.py -m /usr/local/demo-ai/models/mobilenet/mobilenet_v1_1.0_224_quant.tflite -l /usr/local/demo-ai/models/mobilenet/labels.txt -i /usr/local/demo-ai/models/mobilenet/testdata/

3.1.2. Object detection[edit source]

3.1.2.1. Description[edit source]

An object detection Neural Network model will allow you to identify and locate a known object within an image.