Template:ArticleMainWriter Template:ReviewersList
1. Article purpose[edit source]
The purpose of this article is to explain how to integrate the IKS01A expansion board with STM32MP157C-DK2. IKS01A expansion is a motion MEMS and environmental sensor expansion board.
This article will explain step by step how to support IKS01A expansion board on Linux part of software and describe how to use several motion MEMS like HTS221 and LSM6DX.
2. Pre-requisite[edit source]
2.1. Hardware[edit source]
- STM32MP157C-DK2
For more information about hardware and how to start it: link
- IKS01A2 expansion board
2.2. Software[edit source]
For the software, please follow all step described on [start for STM32MP157C-DK2]
3. Software customization for supporting IKS01A expansion board[edit source]
For using IKS01A expansion board you need to configure the kernel with some device tree add-ons and kernel configuration.
3.1. Kernel configuration[edit source]
By default the motions MEMS driver present on IKS01A expansion board are supported: hts221, pressure(lp22hb) and lsm6dsl
To verify if the kernel have this driver, at runtime on board , the configuration of kernel available:
$BOARD> cat /proc/config.gz | gunzip | grep HTS221 CONFIG_HTS221=y CONFIG_HTS221_I2C=y CONFIG_HTS221_SPI=y
$BOARD> cat /proc/config.gz | gunzip | grep ST_PRESS CONFIG_IIO_ST_PRESS=m CONFIG_IIO_ST_PRESS_I2C=m CONFIG_IIO_ST_PRESS_SPI=m
$BOARD> cat /proc/config.gz | gunzip | grep ST_LSM6DS CONFIG_IIO_ST_LSM6DSX=m CONFIG_IIO_ST_LSM6DSX_I2C=m CONFIG_IIO_ST_LSM6DSX_SPI=m
3.2. Kernel device tree[edit source]
The IKS01A expansion board are use via the IC2 bus and on STM32MP157C-DK2 this I2C bus associated are I2C5.
On device tree of STM32MP157C-DK2, the I2C5 must be activated and contains the entry for each hardware to support.
Content to add in stm32mp157c-dk2.dts:
&i2c5 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&i2c5_pins_a>; pinctrl-1 = <&i2c5_pins_sleep_a>; i2c-scl-rising-time-ns = <124>; i2c-scl-falling-time-ns = <3>; /delete-property/dmas; /delete-property/dma-names; status = "okay"; hts221@5f { compatible = "st,hts221"; reg = <0x5f>; }; lsm6dsl@6b { compatible = "st,lsm6dsl"; reg = <0x6b>; }; };
3.3. Activate new configuration on board[edit source]
- Pre-requisite: you need to have re-generated your device tree and your kernel.
- Please put the two file on file system of board, on bootfs partition (/boot directory)
$BOARD> ls -1 /boot/stm32*dk2* /boot/stm32mp157c-dk2-a7-examples.dtb /boot/stm32mp157c-dk2-iks01a2.dtb /boot/stm32mp157c-dk2-m4-examples.dtb /boot/stm32mp157c-dk2.dtb
- add an entry on extlinux.conf file, here on /boot/mmc0_stm32mp157c-dk2_extlinux/extlinux.conf or if there is no mmc0-<something> available on /boot/extlinux/extlinux.conf
# Generic Distro Configuration file generated by OpenEmbedded menu title Select the boot mode MENU BACKGROUND ../splash.bmp TIMEOUT 20 DEFAULT stm32mp157c-dk2-iks01a2 LABEL stm32mp157c-dk2-sdcard KERNEL /uImage FDT /stm32mp157c-dk2.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-dk2-a7-examples-sdcard KERNEL /uImage FDT /stm32mp157c-dk2-a7-examples.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-dk2-m4-examples-sdcard KERNEL /uImage FDT /stm32mp157c-dk2-m4-examples.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-dk2-iks01a2 KERNEL /uImage FDT /stm32mp157c-dk2-iks01a2.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
- Reboot the board
3.4. Verify new configuration on board[edit source]
- Verify if i2c5 are enable:
$BOARD> cat /proc/device-tree/soc/i2c\@40015000/status okay
- Verify if motions MEMS driver are declared on device tree node:
$BOARD> ls -l /proc/device-tree/soc/i2c\@40015000/ total 0 -r--r--r-- 1 root root 4 Dec 19 11:01 #address-cells -r--r--r-- 1 root root 4 Dec 19 11:01 #size-cells -r--r--r-- 1 root root 8 Dec 19 11:01 clocks -r--r--r-- 1 root root 15 Dec 19 11:01 compatible -r--r--r-- 1 root root 6 Dec 19 11:01 dma-names -r--r--r-- 1 root root 32 Dec 19 11:01 dmas drwxr-xr-x 2 root root 0 Dec 19 10:54 hts221@5f -r--r--r-- 1 root root 4 Dec 19 11:01 i2c-scl-falling-time-ns -r--r--r-- 1 root root 4 Dec 19 11:01 i2c-scl-rising-time-ns -r--r--r-- 1 root root 19 Dec 19 11:01 interrupt-names -r--r--r-- 1 root root 44 Dec 19 11:01 interrupts-extended drwxr-xr-x 2 root root 0 Dec 19 10:54 lsm6dsl@6b -r--r--r-- 1 root root 4 Dec 19 11:01 name -r--r--r-- 1 root root 4 Dec 19 11:01 pinctrl-0 -r--r--r-- 1 root root 4 Dec 19 11:01 pinctrl-1 -r--r--r-- 1 root root 14 Dec 19 11:01 pinctrl-names -r--r--r-- 1 root root 4 Dec 19 11:01 power-domains -r--r--r-- 1 root root 8 Dec 19 11:01 reg -r--r--r-- 1 root root 8 Dec 19 11:01 resets -r--r--r-- 1 root root 12 Dec 19 11:01 st,syscfg-fmp -r--r--r-- 1 root root 5 Dec 19 11:01 status
- Verify if the driver are probed correctly and see the hardware:
$BOARD> grep OF_NAME /sys/bus/iio/devices/iio\:device*/uevent /sys/bus/iio/devices/iio:device0/uevent:OF_NAME=adc /sys/bus/iio/devices/iio:device1/uevent:OF_NAME=adc /sys/bus/iio/devices/iio:device2/uevent:OF_NAME=hts221 /sys/bus/iio/devices/iio:device3/uevent:OF_NAME=temp /sys/bus/iio/devices/iio:device4/uevent:OF_NAME=lsm6dsl /sys/bus/iio/devices/iio:device5/uevent:OF_NAME=lsm6dsl