How to configure ethernet interface

Revision as of 10:58, 6 May 2019 by Registered User (→‎Purpose)

Template:ArticleMainWriter Template:ArticleApprovedVersion


1. Purpose[edit source]

This article describes how to configure the Ethernet interface.


2. With Ifconfig tools[edit source]

  • Connect an Ethernet cable and enjoy

At startup SSH daemon (sshd) and ifplugd daemon are automatically launched:

  • sshd (useful to perform ssh, scp)
  • ifplugd detect:
    • udhcpc is launched on cable detection to retrieve an IP address,

If a DHCP server is not available, one can set the Ethernet IP adress with :

  ifconfig eth0 uuu.xxx.yyy.zzz
Warning white.png Warning
If there is some service like systemd-networkd, NetworkManager, Connman the configuration of ethernet interface can change when the service see the change


To check if eth0 and the gateway are well configured, one can type:
 ifconfig
 route
In the console, a log similar to the one below should be displayed:
  ifconfig
 eth0      Link encap:Ethernet  HWaddr 00:80:E1:01:39:61  
           inet addr:10.48.1.172  Bcast:10.48.3.255  Mask:255.255.252.0
           UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
           RX packets:18 errors:0 dropped:0 overruns:0 frame:0
           TX packets:2 errors:0 dropped:0 overruns:0 carrier:0
           collisions:0 txqueuelen:1000 
           RX bytes:3038 (2.9 KiB)  TX bytes:684 (684.0 B)
           Interrupt:103 
 STM32MP1 # route
 Kernel IP routing table
 Destination     Gateway         Genmask         Flags Metric Ref    Use Iface
 default         lme-gw-vl802.lm 0.0.0.0         UG    10     0        0 eth0
 10.48.0.0       *               255.255.252.0   U     0      0        0 eth0

3. With systemd-networkd[edit source]

Systemd-networkd is a network service provided by systemd.

3.1. Ethernet interface[edit source]

Systemd-networkd provide a directory on which the ethernet interface must be configured via configuration file: /lib/systemd/network.

  ls /lib/systemd/network
50-wired.network            52-static.network.static    80-container-vz.network
50-wired.network.static     80-container-host0.network  99-default.link 
51-wireless.network.sample  80-container-ve.network

ST provide some configurations file:

  • 50-wired.network: basic dhcp configuration for each ethX ethernet interface
  • 50-wired.network.static: example of basic dhcp configuration on which eth0 are exclude of list
  • 52-static.network.static: example of static ip configuration for eth0

3.2. Configuration file[edit source]

Example of configuration:
DHCP configuration;

[Match]
Name=eth*

[Network]
DHCP=ipv4

Static ip configuration:

[Match]
Name=eth0

[Network]
DNS=192.168.72.254
Address=192.168.72.2/24
Gateway=192.168.72.254

[Match]

  • MACAddress= a whitespace-separated list of hardware addresses
  • Name= a white-space separated list of device names or expression (e.g. eth*).
  • Host= the machine hostname

[NETWORK]
[Network]

  • DHCP= enables the DHCP client, value can be: yes, no, ipv4, ipv6
  • DHCPServer= enables the DHCP server for this configuration
  • DNS= list DNS addresses in case of static configuration (you may specify several addresses)
  • IPForward= configures IP packet forwarding, value can be: ipv4 or ipv6
  • IPMasquerade= configures IP masquerading for the network interface. If enabled, packets forwarded from the network interface will be appear as coming from the local host. Takes a boolean argument. Implies IPForward=ipv4. Defaults to "no". Value can be yes or no.

The list of all parameters are described on official documenation of systemd-networkd: [1]

3.3. DHCP configuration[edit source]

DHCP configuration;

[Match]
Name=eth*

[Network]
DHCP=ipv4

All Ethernet interface are configured with dhcp client address.

3.4. STATIC configuration[edit source]

Static configuration;

[Match]
Name=eth0

[Network]
DNS=192.168.72.254
Address=192.168.72.2/24
Gateway=192.168.72.254

Eth0 Ethernet interface are configured with static ip address.

Info white.png Information
In case of static configuration or specific configuration, please take care to not configure two time your Ethernet interface
, with the static configuration example you need to exclude eth0 interface of default configuration (here 50-wired.network)


Exclude eth0 from default Ethernet configuration:

[Match]
Name=eth[1-9]

[Network]
DHCP=ipv4

3.5. DHCP Server configuration[edit source]

DHCP server example:

[Match]
Name=eth0

[Network]
Address=192.168.72.1/24
DHCPServer=yes
IPForward=ipv4
IPMasquerade=yes


4. References[edit source]