Template:ArticleApprovedVersion
1. Release information[edit source]
This article aims to describe the content of the software release included in the STM32CubeMP1 Package, version v1.0.0
2. Delivery scope and purpose[edit source]
The STM32CubeMP1 Package is a software package running on Arm® Cortex® M4 processors and is a fundamental part of the STM32MPU Embedded Software distribution.
This release includes:
- The STM32Cube HAL, STM32 abstraction layer embedded software ensuring maximized portability across the STM32 portfolio. HAL APIs are available for all peripherals.
- Low-layer APIs (LL) offering a fast lightweight expert-oriented layer that is closer to the hardware than the HAL. LL APIs are available only for a set of peripherals.
- A consistent set of middleware components such as FreeRTOS, OpenAMP.
- All embedded software utilities, delivered with a full set of examples.
It also includes:
- BSP for the STM32MP157C-EV1 Evaluation board and the STM32MP157C-DK2 Discovery kit (button and LEDs only)
- Multi-core components
- OpenAMP
- ResourceManager
- CoproSync
- IDE ready projects (examples, applications and demonstration firmware) with the System Workbench for STM32 toolchain (SW4STM32)
3. Supported devices[edit source]
The drivers provided within this package support the following devices :
- STM32MP157Cxx, STM32MP157Axx
- STM32MP153Cxx, STM32MP153Axx
- STM32MP151Cxx, STM32MP151Axx
4. Supported hardware[edit source]
This software delivery is applicable to the following boards:
- STM32MP157C-EV1 Evaluation board (RevC). For information about this board, read the article STM32MP157C-EV1 - hardware description.
- STM32MP157C-DK2 Discovery board (RevC). For information about this board, read the article STM32MP157X-DKX - hardware description.
5. Known issues and limitations[edit source]
- Compilation issue with STM32MP151Cxx, STM32MP151Axx, STM32MP153Cxx, STM32MP15ACxx as :
- CRYP1 and CRYP2 not declared in stm32MP153cxx_cm4.h and stm32MP151cxx_cm4.h files - see patch upper V1.0.0 in github [1]
- CRYP1 & CRYP2 supported only for STM32MP157Cxx, STM32MP153Cxx, STM32MP151Cxx in resmngr.c
- FDCAN supported only for STM32MP157Cxx, STM32MP157Axx, STM32MP153Cxx, STM32MP153Axx in resmngr.c
- DSI, GPU supported only for STM32MP157Cxx, STM32MP157Axx in resmngr.c
- For Patch, please contact us
6. Contents[edit source]
6.1. Released projects[edit source]
The STM32CubeMP1 Firmware Package comes with a rich set of examples running on STMicroelectronics boards, organized by board and provided with preconfigured projects for the main supported toolchain (System Workbench for STM32). The exhaustive list of projects is provided in the table List of Projects.
- IDE ready projects
Projects | STM32MP157C-DK2 | STM32MP157C-EV1 |
---|---|---|
Availables Firmware | 24 | 25 |
6.2. Released components[edit source]
- Drivers
Component | Version | Notes |
---|---|---|
Cortex-M CMSIS V5.2.0 | V5.2.0 | |
STM32MP1xx CMSIS | V1.0.0 | |
STM32MP1xx HAL | V1.0.0 | |
BSP STM32MP15xx_EVAL | V1.0.0 | |
BSP STM32MP15xx_DISCO | V1.0.0 |
- Middleware
Component | Version | Notes |
---|---|---|
FreeRTOS | V10.0.1 ST modified 20180813 | |
OpenAMP | v2018.10 ST modified 20190125 |
- Utilities
Component | Version | Notes |
---|---|---|
Resourcemanager | V1.5.0 |
6.3. Available drivers[edit source]
Please find below the list of HAL and LL drivers available:
6.3.1. HAL drivers[edit source]
STM32CubeMP1 HAL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the Analog to Digital Convertor (ADC) * peripheral: * + Initialization and de-initialization functions * ++ Initialization and Configuration of ADC * + Operation functions * ++ Start, stop, get result of conversions of regular * group, using 3 possible modes: polling, interruption or DMA. * + Control functions * ++ Channels configuration on regular group * ++ Analog Watchdog configuration * + State functions * ++ ADC state machine management * ++ Interrupts and flags management * + Operation functions * ++ Start, stop, get result of conversions of ADC group injected, * using 2 possible modes: polling, interruption. * ++ Calibration * +++ ADC automatic self-calibration * +++ Calibration factors get or set * ++ Multimode feature when available * + Control functions * ++ Channels configuration on ADC group injected * + State functions * ++ ADC group injected contexts queue management |
CEC |
* This driver provides firmware functions to manage the following * functionalities of the High Definition Multimedia Interface * Consumer Electronics Control Peripheral (CEC). * + Initialization and de-initialization function * + IO operation function * + Peripheral Control function |
CRC |
* This driver provides firmware functions to manage the following
* functionalities of the Cyclic Redundancy Check (CRC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Peripheral State functions
* + Extended features functions
|
CORTEX |
* This driver provides firmware functions to manage the following
* functionalities of the CORTEX (MPU, Cache, …):
* + Initialization and de-initialization functions
* + Peripheral Control functions
|
CRYP |
* This driver provides firmware functions to manage the following * functionalities of the Cryptography (CRYP) peripheral: * + Initialization and de-initialization functions * + AES processing functions * + DES processing functions * + TDES processing functions * + DMA callback functions * + CRYP IRQ handler management * + Peripheral State functions * + Extended AES processing functions |
DAC |
* This driver provides firmware functions to manage the following * functionalities of the Digital to Analog Converter (DAC) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Errors functions * + Extended features functions |
DCMI |
* This driver provides firmware functions to manage the following * functionalities of the Digital Camera Interface (DCMI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions |
DFSDM |
* This driver provides firmware functions to manage the following * functionalities of the Digital Filter for Sigma-Delta Modulators * (DFSDM) peripherals: * + Initialization and configuration of channels and filters * + Regular channels configuration * + Injected channels configuration * + Regular/Injected Channels DMA Configuration * + Interrupts and flags management * + Analog watchdog feature * + Short-circuit detector feature * + Extremes detector feature * + Clock absence detector feature * + Break generation on analog watchdog or short-circuit event * + Set and get pulses skipping on channel. |
DMA |
* This driver provides firmware functions to manage the following * functionalities of the Direct Memory Access (DMA) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and errors functions * + Extended features functions |
EXTI |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (EXTI) peripheral: * + Initialization and de-initialization functions * + IO operation functions |
FDCAN |
* This driver provides firmware functions to manage the following
* functionalities of the Flexible DataRate Controller Area Network
* (FDCAN) peripheral:
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Configuration and Control functions
* + Peripheral State and Error functions
|
GPIO |
* This driver provides firmware functions to manage the following * functionalities of the General Purpose Input/Output (GPIO) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Extended Peripheral Control functions |
HAL |
* This driver provides firmware functions to manage the following * functionalities of HAL, Tick, SYSCFG, DBGMCU: * + Initialization and de-initialization functions * + HAL Initialization and de-initialization functions * + Configure the source of the time base * + HAL Control functions * + Tick management (get/set/inc/priority/suspend/resume) * + Get HAL revision, the device revision identifier, the device identifier * + Enable/Disable DBG wake up on AIEC * + Enable/Disable the Debug Module during Domain1 SLEEP mode * + Enable/Disable the Debug Module during Domain1 STOP mode * + Enable/Disable the Debug Module during Domain1 STANDBY mode * + Configure the internal voltage reference buffer voltage scale * + Configure the internal voltage reference buffer high impedance mode * + Tune the Internal Voltage Reference buffer (VREFBUF) * + Enable/Disable the Internal Voltage Reference buffer (VREFBUF) * + Ethernet PHY Interface Selection either MII or RMII * + Analog Switch control for dual analog pads * + Enable/Disable the booster to reduce the total harmonic distortion of the analog * + Enable/Power-down the I/O Compensation Cell * + To Enable/Disable optimize the I/O speed when the product voltage is low * + Code selection for the I/O Compensation cell |
HASH |
* This driver provides firmware functions to manage the following * functionalities of the HASH peripheral: * + Initialization and de-initialization methods * + HASH or HMAC processing in polling mode * + HASH or HMAC processing in interrupt mode * + HASH or HMAC processing in DMA mode * + Peripheral State methods * + HASH or HMAC processing suspension/resumption * Additionally, this driver provides functions to manage HMAC * multi-buffer DMA-based processing for MD-5, SHA-1, SHA-224 * and SHA-256. |
HSEM |
* This driver provides firmware functions to manage the following * functionalities of the semaphore peripheral: * + Semaphore Take function (2-Step Procedure) , non blocking * + Semaphore FastTake function (1-Step Procedure) , non blocking * + Semaphore Status check * + Semaphore Clear Key Set and Get * + Release and release all functions * + Semaphore notification enabling and disabling and callnack functions * + IRQ handler management |
I2C |
* This driver provides firmware functions to manage the following * functionalities of the Inter Integrated Circuit (I2C) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions * + Extended features functions |
IPCC |
* This driver provides firmware functions to manage the following
* functionalities of the Inter-Processor communication controller
* peripherals (IPCC).
* + Initialization and de-initialization functions
* + Configuration, notification and interrupts handling
* + Peripheral State and Error functions
|
LPTIM |
* This driver provides firmware functions to manage the following
* functionalities of the Low Power Timer (LPTIM) peripheral:
* + Initialization and de-initialization functions.
* + Start/Stop operation functions in polling mode.
* + Start/Stop operation functions in interrupt mode.
* + Reading operation functions.
* + Peripheral State functions.
|
MDIOS |
* This driver provides firmware functions to manage the following
* functionalities of the MDIOS Peripheral.
* + Initialization and de-initialization functions
* + IO operation functions
* + Peripheral Control functions
|
MDMA |
* This driver provides firmware functions to manage the following * functionalities of the Master Direct Memory Access (MDMA) peripheral: * + Initialization/de-initialization functions * + I/O operation functions * + Peripheral State and errors functions |
PWR |
* This driver provides firmware functions to manage the following * functionalities of the Power Controller (PWR) peripheral: * + Initialization and de-initialization functions * + Peripheral Control functions * + Peripheral Extended features functions |
QUADSPI |
* This driver provides firmware functions to manage the following * functionalities of the QuadSPI interface (QSPI). * + Initialization and de-initialization functions * + Indirect functional mode management * + Memory-mapped functional mode management * + Auto-polling functional mode management * + Interrupts and flags management * + MDMA channel configuration for indirect functional mode * + Errors management and abort functionality |
RCC |
* This driver provides firmware functions to manage the following
* functionalities of the Reset and Clock Control (RCC) peripheral:
* + Initialization and de-initialization functions
* + Peripheral Control functions
* + Extended Peripheral Control functions
|
RNG |
* This driver provides firmware functions to manage the following
* functionalities of the Random Number Generator (RNG) peripheral:
* + Initialization and configuration functions
* + Peripheral Control functions
* + Peripheral State functions
|
SAI |
* This driver provides firmware functions to manage the following
* functionalities of the Serial Audio Interface (SAI) peripheral:
* + Initialization/de-initialization functions
* + I/O operation functions
* + Peripheral Control functions
* + Peripheral State functions
* + Modify PDM microphone delays.
|
SD |
* This driver provides firmware functions to manage the following * functionalities of the Secure Digital (SD) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + Extended features functions |
SMBUS |
* This driver provides firmware functions to manage the following * functionalities of the System Management Bus (SMBus) peripheral, * based on I2C principles of operation : * + Initialization and de-initialization functions * + IO operation functions * + Peripheral State and Errors functions |
SPDIFRX |
* This driver provides firmware functions to manage the following
* functionalities of the SPDIFRX audio interface:
* + Initialization and Configuration
* + Data transfers functions
* + DMA transfers management
* + Interrupts and flags management
|
SPI |
* This driver provides firmware functions to manage the following * functionalities of the Serial Peripheral Interface (SPI) peripheral: * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State functions * + IO operation functions * + Peripheral Control functions |
TIMER |
* This driver provides firmware functions to manage the following * functionalities of the Timer (TIM) peripheral: * + Time Base Initialization * + Time Base Start * + Time Base Start Interruption * + Time Base Start DMA * + Time Output Compare/PWM Initialization * + Time Output Compare/PWM Channel Configuration * + Time Output Compare/PWM Start * + Time Output Compare/PWM Start Interruption * + Time Output Compare/PWM Start DMA * + Time Input Capture Initialization * + Time Input Capture Channel Configuration * + Time Input Capture Start * + Time Input Capture Start Interruption * + Time Input Capture Start DMA * + Time One Pulse Initialization * + Time One Pulse Channel Configuration * + Time One Pulse Start * + Time Encoder Interface Initialization * + Time Encoder Interface Start * + Time Encoder Interface Start Interruption * + Time Encoder Interface Start DMA * + Commutation Event configuration with Interruption and DMA * + Time OCRef clear configuration * + Time External Clock configuration * + Time Hall Sensor Interface Initialization * + Time Hall Sensor Interface Start * + Time Complementary signal bread and dead time configuration * + Time Master and Slave synchronization configuration * + Time Output Compare/PWM Channel Configuration (for channels 5 and 6) * + Time OCRef clear configuration * + Timer remapping capabilities configuration |
U(S)ART |
* This driver provides firmware functions to manage the following * functionalities of the Universal (Synchronous) Asynchronous Receiver Transmitter * Peripheral (U(S)ART). * + Initialization and de-initialization functions * + IO operation functions * + Peripheral Control functions * + Peripheral State and Error functions * + Peripheral Control functions |
WWDG |
* This driver provides firmware functions to manage the following
* functionalities of the Window Watchdog (WWDG) peripheral:
* + Initialization and Configuration functions
* + IO operation functions
|
6.3.2. LL drivers[edit source]
STM32CubeMP1 LL Driver items | Description |
---|---|
ADC |
* This driver provides firmware functions to manage the following * functionalities of the ADC peripheral: * + Initialization/de-initialization functions * + Configuration functions (ADC instance, group regular, group injected, * channels, analog watchdog, oversampling, multimode) * + IT/FLAGS management functions |
BUS |
* This driver provides firmware functions to manage the following * functionalities of the BUS peripheral: * + Enable/disable/reset clocks for all system BUS (AHB2, AHB3, AHB4, AHB5, AHB6, * AXI, MLAHB, APB1, APB2, APB3, APB4, APB5) |
GPIO |
* This driver provides firmware functions to manage the following
* functionalities of the GPIO peripheral:
* + Initialization/de-initialization functions
* + Data access functions
* + Port configuration functions
|
IPCC |
* This driver provides firmware functions to manage the following
* functionalities of the IPCC peripheral:
* + IT/FLAGS management functions
* + Enable/disable transmit and receive channels functions
|
RCC |
* This driver provides firmware functions to manage the following * functionalities of the RCC peripheral: * + Clocks management functions (HSE/HSI/CSI/LSE/LSI/MCO/PLL) * + RTC/TIMERS functions * + IT/FLAGS management functions * + De-initialization functions * + Get system and peripherals clocks frequency functions |
SYSTEM |
* This driver provides firmware functions to manage the following
* functionalities of the SYSTEM peripheral:
* + SYSCFG and DBGMCU functions
|
USART |
* This driver provides firmware functions to manage the following * functionalities of the USART peripheral: * + Initialization/de-initialization functions * + Configuration functions (Irda, Smartcard, Half duplex, * SPI Slave, LIN, Driver enable) * + Advanced configurations services functions * + IT/FLAGS management functions * + DMA management functions * + Data management functions * + Execution functions |
UTILS |
* This driver provides firmware functions to manage the following * functionalities of the UTILS peripheral: * + Device Electronic Signature functions * + DELAY functions * + SYSTEM functions |
6.4. Available projects[edit source]
Please find below the list of projects available for STM32MP157C-EV1 and STM32MP157C-DK2 :
Level | Module Name | Project Name | Description | STM32MP157C-DK2 | STM32MP157C-EV1 | Mode | Core |
---|---|---|---|---|---|---|---|
Examples | |||||||
ADC | ADC_SingleConversion_TriggerTimer_DMA | Use ADC to convert a single channel at each trig from timer, conversion data are transferred by DMA into an array, indefinitely (circular mode). | x | x | Production & Engineering | Cortex-M4 | |
CRC | CRC_UserDefinedPolynomial | How to configure the CRC using the HAL API. The CRC (cyclic redundancy check) calculation unit computes the 8-bit CRC code for a given buffer of 32-bit data words, based on a user-defined generating polynomial. | x | x | Production & Engineering | Cortex-M4 | |
CRYP | CRYP_AES_DMA | This example provides a short description of how to use the CRYPTO peripheral to encrypt and decrypt data using AES-128 Algorithm with ECB chaining mode. | x | x | Production & Engineering | Cortex-M4 | |
CORTEX | CORTEXM_MPU | Presentation of the MPU feature. This example configures a memory area as privileged read-only, and attempts to perform read and write operations in different modes. | x | x | Production & Engineering | Cortex-M4 | |
DAC | DAC_SimpleConversion | How to use the DAC peripheral to do a simple conversion. | - | x | Production & Engineering | Cortex-M4 | |
DMA | DMA_FIFOMode | This example provides a description of how to use a DMA to transfer a word data buffer from Flash memory to embedded SRAM with FIFO mode enabled through the HAL API. | x | x | Production & Engineering | Cortex-M4 | |
FDCAN | FDCAN_Loopback | How to configure the FDCAN to operate in loopback mode. | x | x | Engineering Only | Cortex-M4 | |
GPIO | GPIO_EXTI | How to configure external interrupt lines. | x | x | Production & Engineering | Cortex-M4 | |
HASH | HASH_SHA224SHA256_DMA | This example provides a short description of how to use the HASH peripheral to hash data using SHA224 and SHA256 Algorithms. | x | x | Production & Engineering | Cortex-M4 | |
I2C | I2C_TwoBoards_ComDMA | How to handle I2C data buffer transmission/reception between two boards, via DMA. | - | x | Production & Engineering | Cortex-M4 | |
I2C_TwoBoards_ComIT | How to handle I2C data buffer transmission/reception between two boards, using an interrupt. | x | x | Production & Engineering | Cortex-M4 | ||
LPTIM | LPTIM_PulseCounter | This example describes how to configure and use LPTIM to count pulses through the LPTIM HAL API. | x | x | Production (DK2) & Engineering (EV1 and DK2) | Cortex-M4 | |
QSPI | QSPI_ReadWrite_IT | This example describes how to erase part of the QSPI memory, write data in IT mode, read data in IT mode and compare the result in a forever loop. | - | x | Production & Engineering | Cortex-M4 | |
SPI | SPI_FullDuplex_ComDMA_Master | Data buffer transmission/reception between two boards via SPI in Polling. | x | x | Production & Engineering | Cortex-M4 | |
SPI_FullDuplex_ComDMA_Slave | Data buffer transmission/reception between two boards via SPI using DMA. | x | x | Production & Engineering | Cortex-M4 | ||
SPI_FullDuplex_ComIT_Master | Data buffer transmission/reception between two boards via SPI using Interrupt mode. | x | - | Production & Engineering | Cortex-M4 | ||
SPI_FullDuplex_ComIT_Slave | Data buffer transmission/reception between two boards via SPI using Interrupt mode. | x | - | Production & Engineering | Cortex-M4 | ||
TIM | TIM_DMABurst | This example shows how to update the TIMER TIM2_CH4 period and the duty cycle using the TIMER DMA burst feature. | x | x | Production & Engineering | Cortex-M4 | |
UART | UART_TwoBoards_ComDMA | UART transmission (transmit/receive) in DMA mode between two boards. | x | - | Production & Engineering | Cortex-M4 | |
UART_TwoBoards_ComIT | UART transmission (transmit/receive) in Interrupt mode between two boards. | x | x | Production & Engineering | Cortex-M4 | ||
WWDG | WWDG_Example | Configuration of the HAL API to periodically update the WWDG counter and simulate a software fault that generates an MCU WWDG reset when a predefined time period has elapsed. | x | x | Production & Engineering | Cortex-M4 | |
Total number of examples: 36 | 18 | 18 | |||||
Applications | |||||||
CoproSync | CoproSync_ShutDown | Send of shutdown information to Cortex-M4 so that it is able to take necessary actions before going to reset state. | - | x | Production | Cortex-M4 | |
FreeRTOS | FreeRTOS_ThreadCreation | How to implement thread creation using CMSIS RTOS API. | x | x | Production & Engineering | Cortex-M4 | |
OpenAMP | OpenAMP_TTY_echo | How to use OpenAMP MW + Virtual UART to create an Inter-Processor Communication channel seen as TTY device in Linux OS | x | x | Production | Cortex-M4 | |
OpenAMP_TTY_echo_wakeup | How to use OpenAMP MW to enter in different power system operating mode (Run, Stop and Standby). | x | x | Production | Cortex-M4 | ||
OpenAMP_raw | How to use OpenAMP MW to create an Inter-Processor Communication channel | x | x | Production | Cortex-M4 | ||
Total number of applications: 9 | 4 | 5 | |||||
Demonstrations | |||||||
AI | AI_Character_Recognition | This project demonstrate a complex application that is running on both CPU1(CA7) and CPU2(CM4) | x | x | Production | Cortex-M4 | |
Total number of demonstrations: 2 | 1 | 1 | |||||
Templates | |||||||
- | Starter project | This projects provides a reference template that can be used to build any firmware application in mode on Cortex-M4 | x | x | Engineering | Cortex-M4 | |
Total number of templates: 2 | 1 | 1 | |||||
Total number of projects: 49 | 24 | 25 |
7. How to get started with STM32CubeMP1 Package[edit source]
- Please refer to How to get software and start with this release
8. Associated tools[edit source]
- Please refer to Referenced tools release notes to obtain more information on all available tools.