Last edited 4 years ago

How to play audio

Template:ArticleMainWriter Template:ArticleApprovedVersion


1. Article purpose[edit source]

This article explains how to play audio through the ALSA audio framework in Linux® OS context. The examples below, show how to play audio on the different audio hardware interfaces of the STM32MPU boards.

2. Audio playback overview[edit source]

The ALSA framework exposes audio devices associated to the board audio hardware interfaces.

The application audio streams are routed by default through the PulseAudio sound server. PulseAudio exposes audio profiles which are mapped on the ALSA sound card audio devices. The PulseAudio server provides a command line interface which allows to list audio profiles and to select a profile, to play on a specific audio interface.

The audio playback examples in following sections are given for ALSA utilities. However, the audio playbacks can be launched by other applications, such as gstreamer multimedia framework.

3. Examples[edit source]

3.1. Audio playback on headset output[edit source]

  • Playback on ALSA device

Run audio playback on 'playback_codec' ALSA device: Template:Info

Template:Board$ aplay -D playback_codec /usr/share/sounds/alsa/Front_Left.wav
  • Playback via PulseAudio

Change the Pulseaudio active profile of the sound card, to 'analog-stereo' profile: Template:Info Template:Info

Template:Board$ pacmd set-card-profile 0 output:analog-stereo+input:analog-stereo

Run audio playback:

Template:Board$ aplay /usr/share/sounds/alsa/Front_Left.wav

3.2. Audio playback on HDMI output[edit source]

Template:Warning

  • Playback on ALSA device

Run audio playback on 'playback_hdmi' ALSA device: Template:Info

Template:Board$ aplay -D playback_hdmi /usr/share/sounds/alsa/Front_Left.wav
  • Playback via PulseAudio

Change the Pulseaudio active profile of the sound card, to 'hdmi-stereo' profile: Template:Info

Template:Board$ pacmd set-card-profile 0 output:hdmi-stereo

Run audio playback:

Template:Board$ aplay /usr/share/sounds/alsa/Front_Left.wav

3.3. Audio playback on S/PDIF output[edit source]

Template:Warning Template:Info

  • Playback on ALSA device

Run audio playback on 'playback_spdif' ALSA device: Template:Info

Template:Board$ speaker-test -D playback_spdif -c 2 -F S32_LE -f 440 -t sine -l 1
  • Playback via PulseAudio

Change the sound card active profile, to S/PDIF 'iec958-stereo' profile. Template:Info

Template:Board$ pacmd set-card-profile 0 output:iec958-stereo

Run audio playback:

Template:Board$ speaker-test -c 2 -F S32_LE -f 440 -t sine -l 1