Last edited 5 years ago

How to stream camera over network

Template:ArticleBasedOnModel Template:ArticleMainWriter Template:ArticleApprovedVersion


1. Overview

This article will explain how to stream camera content over network thanks to GStreamer application on top of V4L2 Linux® kernel framework.

Capturing compressed JPEG pictures is an efficient way to send camera images to any local or remote player; JPEG pictures require a limited bandwidth while being fully interoperable.

Find below some examples of command lines allowing to capture a continuous JPEG stream while playing it using various multimedia players, either local or remote.

2. Local streaming

Here is an example of a local preview involving V4l2-ctl for JPEG pictures capture and gst-play GStreamer player for JPEG decoding and display. JPEG pictures are sent over a standard Linux pipe.

Template:Board$ v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=-1 Template:Highlight Template:Highlight2 Template:Highlight gst-play-1.0 Template:Highlight

Template:Highlight tells V4l2-ctl to output binary captured content to standard output, which is then sent to pipe Template:Highlight.

Special URI Template:Highlight tells gst-play GStreamer player to read data from the pipe.

Note the Template:Highlight2 right after the V4l2-ctl command to remove the logs from console output.

3. UDP streaming

Template:InfoTemplate:UpdateNeededForNewBoard Get first the IP address Template:Highlight of the host PC using ifconfig command:

Template:PC$ ifconfig | grep "inet addr"
   inet addr:Template:Highlight  Bcast:10.201.23.255  Mask:255.255.252.0
   inet addr:127.0.0.1  Mask:255.0.0.0

Then fill the Template:Highlight2 udpsink property with this IP address on the remote side:

Template:Board$ v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=-1 --stream-to=- 2>/dev/null | gst-launch-1.0 fdsrc ! jpegparse ! rtpjpegpay ! udpsink Template:Highlight2Template:Highlight port=5000

Then play the UDP stream on host PC:

Template:PC$ gst-launch-1.0 udpsrc port=5000 ! application/x-rtp, encoding-name=JPEG ! rtpjpegdepay ! jpegparse ! decodebin ! autovideosink

A new window will popup on host PC displaying the camera content. Template:Info