1. Article purpose[edit source]
Linux® SPI framework offers several ways to access SPI peripherals. Among them, the spidev framework enables to easily control an SPI peripheral straight from Linux® userspace.
Before going further in this document, the reader might be interested in having a look at the
SPI overview article that describes how to use an SPI when the peripheral is assigned to Linux®:
- How to configure an SPI device through the board device tree (example using "spidev")
- How to perform data transfers in userland
2. SPI hardware testing - loopback MOSI / MISO[edit source]
Short-circuit the MISO and MOSI lines of SPI bus to create a loopback allows the bus to receive the same data it is sending. This is interesting to execute quickly basic tests and to execute performance tests.
On the STM32MP157X-DKX discovery board, MOSI and MISO signals are accessible via the D12 and D11 pins of the STM32MP157X-DKX_-_hardware_description#Arduino_Uno_connector.
3. Configuration (DT, kernel)[edit source]
In order to be able to control the SPI device from user-space, the "User mode SPI device driver support" must be enabled. Its configuration is explained in the SPI_overview#Kernel_configuration.
In addition to that, the device tree must be customized in order to expose the SPI peripheral via the spidev framework. Overall device tree configuration is explained in SPI_device_tree_configuration.
In our example of performing MOSI/MISO loopback on the STM32MP157X-DKX discovery board, the device tree stm32mp157a-dk1.dts[1] which already include the board skeleton for spi4 must be customized as followed:
- Activate SPI controller by setting status "okay"
- Add a spidev child node
- Enable spidev by adding compatible "spidev";
- Add a reg property, mandated by the SPI framework but not meaningfull in this case since chip select is not defined and we are in loopback.
- Configure bus speed when talking to the SPI peripheral by setting the spi-max-frequency property
&spi4 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&spi4_pins_a>; pinctrl-1 = <&spi4_sleep_pins_a>; status = "okay"; spidev@0{ compatible = "spidev"; reg = <0>; spi-max-frequency = <4000000>; }; };
4. SPI unitary tests using spidev_test[edit source]
The spidev_test tool, from the Linux® kernel, provides a test tool for performing tests via the spidev interface.
4.1. Source code[edit source]
The Linux® kernel spidev_test tool source code can be found under tools/spi[2] directory:
4.2. Installation on your target[edit source]
The Linux® kernel SPI tools aren't embedded by default in OpenSTLinux distribution. They can be compiled independently and then installed on the target. See How to build Linux kernel user space tools.
4.3. List the spidev options[edit source]
The spidev_test tool options can be listed:
spidev_test -h Usage: spidev_test [-DsbdlHOLC3vpNR24SItx] -D --device device to use (default /dev/spidev1.1) -s --speed max speed (Hz) -d --delay delay (usec) -b --bpw bits per word -i --input input data from a file (e.g. "test.bin") -o --output output data to a file (e.g. "results.bin") -l --loop loopback -H --cpha clock phase -O --cpol clock polarity -L --lsb least significant bit first -C --cs-high chip select active high -3 --3wire SI/SO signals shared -v --verbose Verbose (show tx buffer) -p Send data (e.g. "1234\xde\xad") -N --no-cs no chip select -R --ready slave pulls low to pause -2 --dual dual transfer -4 --quad quad transfer -S --size transfer size -I --iter iterations -t --txonly simplex tx transfer -r --rxonly simplex rx transfer
4.4. Example to transfer 32 bytes in full-duplex with loopback[edit source]
spidev_test -D /dev/spidev0.0 -v spi mode: 0x0 bits per word: 8 max speed: 500000 Hz (500 KHz) TX | FF FF FF FF FF FF 40 00 00 00 00 95 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF F0 0D | ......@.... .................. . RX | FF FF FF FF FF FF 40 00 00 00 00 95 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF F0 0D | ......@.... .................. .
5. References[edit source]
- ↑ arch/arm/boot/dts/stm32mp157a-dk1.dts
- ↑ tools/spi , Linux® SPI tools source code