STM32CubeIDE

Revision as of 10:37, 14 August 2020 by Registered User

This article explains some of the basics of STM32CubeIDE. It is an all-in-one multi-OS development tool, which is part of the STM32Cube software ecosystem.


For more information about STM32CubeIDE please refer to its User Manual

1. STM32CubeIDE purpose[edit source]

STM32CubeIDE is an advanced C/C++ development platform with peripheral configuration, code generation, code compilation, and debug features for STM32 microcontrollers and microprocessors. It is based on the ECLIPSE™/CDT framework, GCC toolchain for the development and GDB for the debugging.

It allows the integration of the hundreds of existing plugins that complete the features of the ECLIPSE™ IDE. STM32CubeIDE integrates all STM32CubeMX functionalities to offer all-in-one tool experience and to save installation and development time.

With STM32CubeIDE, you can

  • select the appropriate STM32 device corresponding to your needs,
  • configure the device using STM32CubeMX,
  • develop and debug applications on top on Arm® Cortex®-M


2. Prerequisites[edit source]

To take all advantages of explanations given in the wiki page and to develop some application based on the STM32 MP1 Series, following packages must constitute the development environment :

  • STM32CubeIDE v1.1.0 or newer
  • STM32CubeMP1 Package v1.1.0 or newer
  • STM32CubeMX v5.4.0 or newer

3. How to install STM32CubeIDE[edit source]

STM32CubeIDE for Linux® host PC STM32CubeIDE for Windows® host PC
Download

Version 1.3.0

  • Download the preferred all-in-one Linux installer from my.st.com
    • Generic Linux Installer - STM32CubeIDE-Lnx
    • RPM Linux Installer - STM32CubeIDE-RPM
    • Debian Linux Installer - STM32CubeIDE-DEB

Version 1.3.0

  • Download the all-in-one Windows installer from my.st.com
    • Windows Installer - STM32CubeIDE-Win
Installation guide
  • Please refer to STM32CubeIDE installation guide (UM2563) available on my.st.com.
User manual
  • When the installation is over, please see additional information about the STM32CubeIDE in my.st.com:
    • STM32CubeIDE quick start guide (UM2553)
    • Getting started with projects based on the STM32MP1 Series in STM32CubeIDE (UM5360)
Detailed release note
  • Details about the content of this tool version are available in Release Notes STM32CubeIDE release v1.3.0 from my.st.com:


4. How to get started with STM32CubeIDE[edit source]

This section links to two different how to articles depending on if you are moving from SW4STM32 to STM32CubeIDE or if you are starting a new project with STM32CubeIDE.

4.1. How to get started with STM32CubeIDE from scratch[edit source]

How to get started with STM32CubeIDE from scratch.

4.2. How to move from SW4STM32 to STM32CubeIDE[edit source]

How to move from SW4STM32 to STM32CubeIDE.

5. Project structure[edit source]

A hierarchical project structure is created in same time as the creation of an STM32 MPU project.

The project structure for single-core projects is flat. On the contrary, in a multi-core project, the hierarchical project structure is used. When the user creates or imports an STM32 MPU project, it consists of one root project together with sub-projects, referred to STM32 MCU projects, for each core. A hierarchical structure example is shown below.

Hierarchical project structure

6. Arm® Cortex®-M debug on STM32 MPU device[edit source]

Two modes are used to debug Arm® Cortex®-M firmware on STM32 MPU device.

6.1. Engineering mode[edit source]

Very powerful to debug preliminary Arm® Cortex®-M, the engineering mode implies a specific boot mode: the Engineering Boot Mode where only Cortex-M is started. Firmware is loaded via JTAG/SWD into its dedicated RAM.

This mode is not the default one, it has to be set via the "Debug Configuration" menu, in "Debugger" tab , "thru JTGA/SWD link (Engineering mode)" option selected.

Warning white.png Warning
initialization normally done in Cortex-A like (clock tree set-up, ...) have to be handled by Arm Cortex-M.

Debugging in Engineering Mode in STM32 MPU device is very similar to a standard STM32 MCU debug in term of functionality, expect that here Arm Cortex-M has only a dedicated memory, no flash memory type.

6.2. Production mode[edit source]

Production mode targets a debug close to final product. It means to have an STM32 MPU board up and running on the Cortex-A (Linux) and a Cortex-M firmware to debug (usually an STM32CubeIDE project).

Board, aka named as "target", is booted in Production mode from flash memory (e.g. SD card) ; it is network and JTAG/SWD connected.

ST-Link automatically brings support for Cortex-A Linux console via VCP (Virtual COM Port). This enables Target Status widget, from the bottom-right of STM32CubeIDE, allowing target IP address discovery.



Network connection can be set up by 2 ways:

  • Ethernet
    • managed network: IP address attributed by DHCP server
    • unmanaged network: IP address to be manually configured
  • USB
    • using the dedicated USB OTG connection for Ethernet point to point.




Debug is performed thanks to the following workflow:

1. The firmware built binary is transferred to the target using the network (ssh protocol), more precisely to the Cortex-A Linux file system.

2. The firmware is loaded to Cortex-M core thanks to the “remoteproc” framework.

3. Finally the Debug session is started via JTAG/SWD connection

The production mode is the default one when you create a new debug configuration. It is automatically set via the "Debug Configuration" menu.

File:MPU wiki show production mode.png
Debug configuration, production mode activated.
thumb



At debug launch, some specific pop-up appear:

  • The SSH Password has to be completed: the default one is root.
DebugCfg-Launch-PM-EnterPwd.png
  • The RSA key has to be approved.
DebugCfg-Launch-PM-RSA.png


6.2.1. Update STM32 MPU target for Arm Cortex-M[edit source]

Defining an Arm Cortex-M project in a STM32 MPU context also means to define where are downloaded on Arm Cortex-A Linux file system:

  • the Cortex-M Firmware: <ProjectName>.elf
  • the load/unload script fw_cortex_m4.sh used by the STM32CubeIDE if present it can be customized
  • and a README, informing a user having a direct connection onto the target.

This is the purpose of "Remote Path Setting" property which is linked to the project. Its default value at creation is /usr/local/project/<ProjectName>, but can also be changed thanks to the Remote Settings properties item.

CubeIDE-Dbg-RemotePath.png

Inside project structure,directory "<ProjectName>_CM4/Core/RemoteProc/" defines the tree downloaded when debugging in Production Mode.

6.3. ST-Link Server support[edit source]

From STM32CubeIDE v1.2.0, it is possible to connect to ST-Link via 'ST-Link Server' just like on standard STM32 MCU. This is enable by checking "Shared ST-Link inside Debug Configuration > Debugger > ST-Link Client Setup".

7. FAQ[edit source]

Under construction.png Coming soon