How to read or write peripheral registers

Revision as of 17:12, 2 June 2020 by Registered User


1. Article purpose[edit source]

This article provides the basic information needed to start using Devmem tool, which allows reading and writing in peripheral registers.

2. Introduction[edit source]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
Devmem Tracing tools Used for reading and writing in peripheral registers Yes Yes Yes No No No

3. Installing Devmem on your target board[edit source]

You can install Devmem either with the Starter Package, the Developer Package or the Distribution Package. For the Starter Package, you will need an internet access on your board.

3.1. Using the STM32MPU Embedded Software distribution[edit source]

3.1.1. Starter Package[edit source]

Enter the following commands to install Devmem:

 sudo apt-get update
 sudo apt-get install devmem2

For more information about apt-get, see the Package_repository_for_OpenSTLinux_distribution article.

3.1.2. Developer Package[edit source]

Enter the following commands:

  • Download sources :
 wget http://free-electrons.com/pub/mirror/devmem2.c 
  • Compile the application :
 make devmem2
  • Push it on the board:
 scp devmem2 root@<board ip address>:/usr/bin

3.1.3. Distribution Package[edit source]

Enter the following commands:

  • Build the package with bitbake:
 bitbake devmem2
  • Add it to the targeted image:
 echo 'IMAGE_INSTALL_append += "devmem2"' >> meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappend
  • Rebuild the image:
 bitbake st-image-weston

Then you have to flash the generated image on your board with STM32CubeProgrammer.

4. Getting started[edit source]

To use Devmem, enter the following command:

 devmem2 [address] [type] [data]

Where:

  • [address] corresponds to the register address you want to read
  • [type] corresponds to the output value size you want (b, h, w or l, respectively byte, halfword, word or long). Assigning a type is not necessary if you only read the register and the default output will be a word.
  • [data] corresponds to the data value you want to set on the register, assigning a type is mandatory in this case . If you don't assign a data, it will only read the register.

5. To go further[edit source]

5.1. Checking UART4 baud rate[edit source]

The UART baud rate is generated from UART clock frequency, with USARTDIV parameter found in the USART_BRR register. By default in OpenSTLinux Starter Package delivery, UART4 baud rate is set to 115 000, the Clock frequency CLOCK_UART4_K value is 64 000 000 Hz and the USARTDIV is equal to 556. These results are known and thanks to Devmem we will retrieve the USARTDIV value by looking at STM32MP1 registers.

On the STM32MP157 Reference Manual, we find out that the base address of UART4 is 0x4001 0000 and the USARTDIV value is located at the offset 0x0C.

 devmem2 0x4001000C
/dev/mem opened.
Memory mapped at address 0xb6fc300c.
Read at address 0x4001000C (0xb6fc300c): 0x0000022C

Which is equal to 556 in decimal.

5.2. Driving LED with Devmem[edit source]

In this example, we will check the output value of GPIO port A pins 13 and 14 corresponding to leds 6 and 5 on the DK2. According to the Reference Manual, we find out that the base address for GPIOA is 0x5000 2000 and the output value of leds is located at the offset 0x14.

However, GPIOs' clock have to be enabled at first if we want to see some results in registers. Else it will output 0 has you can see:

 devmem2 0x50002014
/dev/mem opened.
Memory mapped at address 0xb6f43014.
Read at address 0x50002014 (0xb6f43014): 0x00000000

The clock is called RCC_MP_AHB4ENSETR and is located at the address 0x5000 0A28.

 devmem2 0x50000A28
/dev/mem opened.
Memory mapped at address 0xb6fdca28.
Read at address 0x50000A28 (0xb6fdca28): 0x00000000

In this register, the first eleven bits (from LSB to MSB) allow enabling respectively from GPIOA to GPIOK (1 enable, 0 disable). In our case we only need the GPIO A to be enabled so we will write 0x1 in the register.

 devmem2 0x50000A28 w 0x1
/dev/mem opened.
Memory mapped at address 0xb6fdca28.
Read at address 0x50000A28 (0xb6fdca28): 0x00000000
Write at address 0x50000A28 (0xb6fdca28): 0x00000001, readback 0x00000001

Now let's check again in the GPIOA's register:

 devmem2 0x50002014
/dev/mem opened.
Memory mapped at address 0xb6f43014.
Read at address 0x50002014(0xb6f43014): 0x00002400

In my case only the led 5 is enabled, the following table shows the output value of the register in function of leds 5 and 6 states.

Led 5 Enabled Led 5 Disabled
Led 6 Enabled 0x400 0x4400
Led 6 Disabled 0x2400 0x6400

For example to enable both leds, set the value of the register to 0x400:

 devmem2 0x50002014 w 0x400
/dev/mem opened.
Memory mapped at address 0xb6f43014.
Read at address 0x50002014 (0xb6f43014): 0x00002400
Write at address 0x50002014 (0xb6f43014): 0x00000400, readback 0x00000400

You can see the change on your board

6. Restricted Access[edit source]

Keep in mind Devmem tool can only allow you to access peripheral registers, indeed all the registers in M4 and A7 cores are secured and will make the board rebooting if you try to read it.

Besides when trying to access a register, make sure the related peripheral has not been isolated on the MCU side. Else you would not be able to access it due to access rights.