This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.![]() |
Coming soon |
1. Introduction
This article will explain how to set up a proxy connection using STM32CubeIDE and what a user would need to keep in mind while using such a connection.
2. Setting up proxy
To set up the connection go to Windows -> Preferences -> General -> Network Connections.
Select "manual" in the Active Provider field.
Click on Add Host... and then add the board ip address in the Proxy bypass window.