How to use the STM32CubeIDE target status

Revision as of 15:33, 22 April 2020 by Registered User


1. Target status[edit source]

{{

In the production mode, a status light in the bottom right of the STM32CubeIDE window provides information regarding the current status of the connection between the computer and the embedded Linux® system.

Info white.png Information
The serial console is a shared resource and the target widget status has the lowest priority. If there is an active console view for the serial port, this prevents further target status updates until the serial port is disconnected from the view.
Status light Icon Description
Black
Black widget status
The light completely off meants that the widget is disabled.
Red
Red widget status
STM32CubeIDE cannot establish contact and cannot detect any target
Yellow
Yellow widget target status
Indicates a dysfunction such as:
  1. No network connection between the computer and the MPU.
  2. The console is opened.
Green The connection is up and running.