This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Installation
For reading and writing STM32MP1 registers, we will use Devmem tool. There are two ways for install it on your board:
- If you have an internet access on your board through apt-get
- Else through bitbake
1.1. With apt-get
Just enter the following commands:
sudo apt-get update sudo apt-get install devmem2
1.2. With bitbake
Enter the following commands:
bitbake devmem2\n echo 'IMAGE_INSTALL_append += "devmem2"' >> meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappend\n bitbake st-image-Weston
Then you just have to flash the generated image on your board with CubeProgrammer.
==Use of Devmem==
To use Devmem, enter the following command:
devmem2 [address] [type] [data]
Where:
- [address] corresponds to the register address you want to read
- [type] corresponds to the output value size you want (b, h, w or l, respectively byte, halfword, word or long). Assigning a type is not necessary if you only read the register and the default output will be a word. f you want to write a data
- [data] corresponds to the data value you want to set on the register. If you don't assign a data, it will only read the register.