STM32-CoPro-MPU plugin release note

Revision as of 16:12, 5 June 2019 by Registered User

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion



More information can be found in the detailed release notes referenced later in this article.

1. SW4TM32 - System Workbench for STM32 2.8.0 - STM32-CoPro-MPU plugin version 1.0.0[edit source]

The STM32-CoPro-MPU plugin, based onto the System Workbench for STM32 (SW4STM32), targets the support of Cortex®-M core contained in the STM32MP1 Family.
It is included in System Workbench for STM32 from version 2.8.0.
It provides:

  • the target status widget,
  • the console management,
  • the project creation, compilation and debug in two modes:
    • Engineering Mode,
    • Production Mode, with Cortex®-M firmware download :
      • via Ethernet Network (LAN or Point-to-Point)
      • via Ethernet over USB
  • the remote system explorer configuration


It is available on Linux® and Windows® platforms.

Upgrading your System Workbench, STM32-CoPro-MPU plugin can be installed using the System Workbench for STM32 - Updates in menu Windows > Preferences > Install/Update > Available Software Site.
The installation is then the standard Eclipse one: Help > Install New Software...

In order to access to the Ac6 site, take care to configure proxy at Eclipse level: in Windows > Preferences > General > Network Connections; Active Provider set to Manual.
Then after selecting HTTP proxy entry, click Edit... and enter your proxy setup.


IDE for Linux® host PC IDE for Windows® host PC
Download

Version 1.0.0 in SW4STM32 2.8.0

  • Download the all-in-one Linux installer 2.8 install_sw4stm32_linux_64bits-v2.8.run from openstm32.org

Version 1.0.0 in SW4STM32 2.8.0

  • Download the all-in-one Windows installer 2.8 install_sw4stm32_win_64bits-v2.8.exe from openstm32.org
Installation
  • Run the installation script
$ chmod +x install_sw4stm32_linux_64bits-v2.8.run
$ ./install_sw4stm32_linux_64bits-v2.8.run
  • Run the installation exe
$ install_sw4stm32_win_64bits-v2.8.exe
Detailed release notes Details about the content of this tool version are available on openstm32.org

Details about the content of this tool version are available on openstm32.org