STM32MP15 clock tree

Revision as of 13:58, 27 September 2019 by Registered User

Template:ArticleMainWriter Template:ArticleApprovedVersion


SUMMARY
All the peripherals receive one or several clocks that are generated via RCC internal peripheral. RCC relies on several clocks sources (LSI, LSE, HSI, HSE, CSI) and four PLL in order to provide adequate input frequencies to all the peripherals. The clock tree covers all the system clock distribution aspects, from the clock sources to the consumer peripherals (internal and external), except clock gating management that is locally controlled by each peripheral driver.

1. Overview[edit source]

The clock tree is managed via RCC internal peripheral hardware block and it is configured at different steps from the Cortex-A7:


Notice that STM32Cube (running on the Cortex-M4) does not control the clock tree setup so the configuration applied by the Cortex-A7 must provide suitable clocks to Cortex-M4, like it is explained in resource manager description. One exception to this rule is the engineering boot, allowing to directly load (and debug) the Cortex-M4 whereas the Cortex-A7 execution is stalled in the ROM code.

2. How to build a clock tree?[edit source]

Building a clock tree is quite complex as it needs to take into account the constraints set by each internal and external peripheral, including external clock sources.

We encourage the use of STM32CubeMX to build the clock tree, and avoid having to know all internal peripherals details: the tool allows to select the peripherals that will be present on the board, fix the clock sources frequencies and automatically find an optimized clock tree. It is then able to generate the device tree that is directly consumed by the boot chain and Linux.

3. ST boards clock tree[edit source]

For ecosystem release v1.1.0 More info.png[edit source]

3.1. STM32MP157C-EV1 case[edit source]

This chapter shows the boot time clock tree set by the FSBL on STM32MP157C-EV1 evaluation board. Linux eventual runtime modifications are not covered here.

3.1.1. Clock tree[edit source]

The following table shows what STM32MP157C-EV1 clock tree looks like, as a result of the boot chain execution with the device tree built with STM32CubeMX.

Component              | Parent  |   Frequency     | Used?  | Comment                           |
-----------------------|---------|-----------------|--------|-----------------------------------|
LSI                    |N.A.     |    0.032000 MHz |  yes   | Mandatory for IWDG, DAC
  DAC                  |LSI      |    0.032000 MHz |  yes   | 
  RNG1                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  RNG2                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  IWDG1                |LSI      |    0.032000 MHz |  yes   | 
  IWDG2                |LSI      |    0.032000 MHz |  yes   | 
LSE                    |N.A.     |    0.032768 MHz |  yes   | Mandatory for DTS
  RTC                  |LSE      |    0.032768 MHz |  yes   | 
  TAMP                 |LSE      |    0.032768 MHz |  yes   | 
  CEC                  |LSE      |    0.032768 MHz |  yes   | 
  LPTIM4               |LSE      |    0.032768 MHz |  yes   | 
  LPTIM5               |LSE      |    0.032768 MHz |  yes   | 
HSI                    |N.A.     |   64.000000 MHz |  yes   | 
  SPI4                 |HSI      |   64.000000 MHz |  no    | 
  SPI5                 |HSI      |   64.000000 MHz |  no    | 
  SPI6                 |HSI      |   64.000000 MHz |  yes   | 
  I2C4                 |HSI      |   64.000000 MHz |  yes   | PMIC
  I2C6                 |HSI      |   64.000000 MHz |  no    | 
  I2C1                 |HSI      |   64.000000 MHz |  no    | 
  I2C2                 |HSI      |   64.000000 MHz |  yes   | Rpi and peripherals
  I2C3                 |HSI      |   64.000000 MHz |  no    | 
  I2C5                 |HSI      |   64.000000 MHz |  yes   | Rpi
  USART1               |HSI      |   64.000000 MHz |  yes   | 
  USART2               |HSI      |   64.000000 MHz |  no    | 
  USART3               |HSI      |   64.000000 MHz |  yes   | Rpi
  UART4                |HSI      |   64.000000 MHz |  yes   | Linux console
  UART5                |HSI      |   64.000000 MHz |  no    | 
  USART6               |HSI      |   64.000000 MHz |  no    | 
  UART7                |HSI      |   64.000000 MHz |  no    | 
  UART8                |HSI      |   64.000000 MHz |  no    | 
  MCO1                 |HSI      |   64.000000 MHz |  no    | Available so can be used
HSE                    |N.A.     |   24.000000 MHz |  yes   | 
  DSIPLL               |HSE      |  125.000000 MHz |  no    | DSI DPHY PLL
    DSIBL              |DSIPLL   |  125.000000 MHz |  no    | DSI lanebyte clock
  RTCDIV               |HSE      |    1.000000 MHz |  yes   | Only used when RTC source is HSE
  ck_per               |HSE      |   24.000000 MHz |  yes   | 
    ADC                |ck_per   |   24.000000 MHz |  yes   | Can use internal divider to be < 40MHz
  PLL1                 |HSE      | 1300.000000 MHz |  yes   | 
    PLL1P              |PLL1     |  650.000000 MHz |  yes   | 
      MPUDIV           |PLL1P    |  325.000000 MHz |  yes   | 
      Cortex-A7        |PLL1P    |  650.000000 MHz |  yes   | 
        MCO2           |Cortex-A7|  650.000000 MHz |  no    | Available so can be used
  PLL2                 |HSE      | 1066.000000 MHz |  yes   | 
    PLL2P              |PLL2     |  266.500000 MHz |  yes   | 
      AXI              |PLL2P    |  266.500000 MHz |  yes   | < 266MHz
        FMC            |AXI      |  266.500000 MHz |  yes   | NAND flash
        QSPI           |AXI      |  266.500000 MHz |  yes   | NOR flash
        SYSRAM         |AXI      |  266.500000 MHz |  yes   | 
        ROM            |AXI      |  266.500000 MHz |  yes   | 
        AHB5           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRYP1        |AHB5     |  266.500000 MHz |  yes   | 
          HASH1        |AHB5     |  266.500000 MHz |  yes   | 
          GPIOZ        |AHB5     |  266.500000 MHz |  yes   | 
          BKPSRAM      |AHB5     |  266.500000 MHz |  yes   | 
        AHB6           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRC1         |AHB6     |  266.500000 MHz |  yes   | 
          MDMA         |AHB6     |  266.500000 MHz |  yes   | 
          USBH         |AHB6     |  266.500000 MHz |  yes   | USB Host
          APB4         |AHB6     |  133.250000 MHz |  yes   | 
          APB5         |AHB6     |   66.625000 MHz |  yes   | 
            BSEC       |APB5     |   66.625000 MHz |  yes   | < 67MHz
            ETZPC      |APB5     |   66.625000 MHz |  yes   | 
            TZC        |APB5     |   66.625000 MHz |  yes   | 
        DBGAPB         |AXI      |  133.250000 MHz |  yes   | JTAG & Coresight
          DBGMCU       |DBGAPB   |   66.625000 MHz |  yes   | 
          STM          |DBGAPB   |   66.625000 MHz |  yes   | 
    PLL2Q              |PLL2     |  533.000000 MHz |  yes   | 
      GPU              |PLL2Q    |  533.000000 MHz |  yes   | < 533MHz
    PLL2R              |PLL2     |  533.000000 MHz |  yes   | 
      DDR              |PLL2R    |  533.000000 MHz |  yes   | < 533MHz
  PLL3                 |HSE      |  417.755859 MHz |  yes   | 
    PLL3P              |PLL3     |  208.877930 MHz |  yes   | 
      MLAHB            |PLL3P    |  208.877930 MHz |  yes   | < 209MHz
        Cortex-M4      |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM1          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM2          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM3          |MLAHB    |  208.877930 MHz |  yes   | 
        RETRAM         |MLAHB    |  208.877930 MHz |  yes   | 
        AHB1           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
        AHB2           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          DMA1         |AHB2     |  208.877930 MHz |  yes   | 
          DMA2         |AHB2     |  208.877930 MHz |  yes   | 
          DMAMUX       |AHB2     |  208.877930 MHz |  yes   | 
        APB1           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM1       |APB1     |  104.438965 MHz |  yes   | 
          WWDG         |APB1     |  104.438965 MHz |  yes   | 
        APB2           |MLAHB    |  104.438965 MHz |  yes   | 
        TIM2           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM3           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM4           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM5           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM6           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM7           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM12          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM13          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM14          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM1           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM8           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM15          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM16          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM17          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        APB3           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM2       |APB3     |  104.438965 MHz |  yes   | 
          LPTIM3       |APB3     |  104.438965 MHz |  yes   | 
          SYSCFG       |APB3     |  104.438965 MHz |  yes   | 
          VREFBUF      |APB3     |  104.438965 MHz |  yes   | 
          DTS          |APB3     |  104.438965 MHz |  yes   | 
          HDP          |APB3     |  104.438965 MHz |  yes   | 
        AHB3           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          CRC2         |AHB3     |  208.877930 MHz |  yes   | 
          CRYP2        |AHB3     |  208.877930 MHz |  yes   | 
          HASH2        |AHB3     |  208.877930 MHz |  yes   | 
          DCMI         |AHB3     |  208.877930 MHz |  yes   | Camera
          IPCC         |AHB3     |  208.877930 MHz |  yes   | Mailbox
        AHB4           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          PWR          |AHB4     |  208.877930 MHz |  yes   | 
          RCC          |AHB4     |  208.877930 MHz |  yes   | 
          GPIOA-K      |AHB4     |  208.877930 MHz |  yes   | 
          EXTI         |AHB4     |  208.877930 MHz |  yes   | 
    PLL3Q              |PLL3     |   24.573874 MHz |  yes   | 
      SPI1             |PLL3Q    |   24.573874 MHz |  no    | 
      SPI2             |PLL3Q    |   24.573874 MHz |  no    | 
      SPI3             |PLL3Q    |   24.573874 MHz |  no    | 
      DFSDM            |PLL3Q    |   24.573874 MHz |  yes   | Digital micro
      SAI1             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI2             |PLL3Q    |   24.573874 MHz |  yes   | AudCodec 48kHz (use PLL3R for 44.1kHz)
      SAI3             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI4             |PLL3Q    |   24.573874 MHz |  yes   | SPDIF TX 48kHz (use PLL3R for 44.1kHz)
    PLL3R              |PLL3     |   11.290699 MHz |  yes   | 
  PLL4                 |HSE      |  594.000000 MHz |  yes   | 
    PLL4P              |PLL4     |   99.000000 MHz |  yes   | 
      SDMMC1           |PLL4P    |   99.000000 MHz |  yes   | µSD card
      SDMMC2           |PLL4P    |   99.000000 MHz |  yes   | eMMC
      SDMMC3           |PLL4P    |   99.000000 MHz |  yes   | 
      SPDIF            |PLL4P    |   99.000000 MHz |  yes   | SPDIF RX
    PLL4Q              |PLL4     |   74.250000 MHz |  yes   | 
      LCD              |PLL4Q    |   74.250000 MHz |  yes   | LTDC & DSI display pixel clock
    PLL4R              |PLL4     |   74.250000 MHz |  yes   | 
      FDCAN            |PLL4R    |   74.250000 MHz |  yes   | Should be as high as possible and < 100MHz
  STGEN                |HSE      |   24.000000 MHz |  yes   | 
  USBPHYC              |HSE      |   24.000000 MHz |  yes   | USB PHY Ctrl for USB Host and OTG
    USBPLL             |USBPHYC  |   48.000000 MHz |  yes   | 
      USBO             |USBPLL   |   48.000000 MHz |  yes   | USB OTG
CSI                    |N.A.     |    4.000000 MHz |  yes   | Mandatory for IO compensation
ETH                    |N.A.     |    0.000000 MHz |  no    | ETH clocked by RGMII PHY
-----------------------|---------|-----------------|--------|-----------------------------------|
3.1.2. Device tree[edit source]

Here are the corresponding device tree rcc_clk sub node properties consumed by the first stage boot loader (FSBL) to configure the clock tree above:

	st,clksrc = <
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_PLL12_HSE
		CLK_PLL3_HSE
		CLK_PLL4_HSE
		CLK_RTC_LSE
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
	>;

	st,clkdiv = <
		1 /*MPU*/
		0 /*AXI*/
		0 /*MCU*/
		1 /*APB1*/
		1 /*APB2*/
		1 /*APB3*/
		1 /*APB4*/
		2 /*APB5*/
		23 /*RTC*/
		0 /*MCO1*/
		0 /*MCO2*/
	>;

	st,pkcs = <
		CLK_CKPER_HSE
		CLK_FMC_ACLK
		CLK_QSPI_ACLK
		CLK_ETH_DISABLED
		CLK_SDMMC12_PLL4P
		CLK_DSI_DSIPLL
		CLK_STGEN_HSE
		CLK_USBPHY_HSE
		CLK_SPI2S1_PLL3Q
		CLK_SPI2S23_PLL3Q
		CLK_SPI45_HSI
		CLK_SPI6_HSI
		CLK_I2C46_HSI
		CLK_SDMMC3_PLL4P
		CLK_USBO_USBPHY
		CLK_ADC_CKPER
		CLK_CEC_LSE
		CLK_I2C12_HSI
		CLK_I2C35_HSI
		CLK_UART1_HSI
		CLK_UART24_HSI
		CLK_UART35_HSI
		CLK_UART6_HSI
		CLK_UART78_HSI
		CLK_SPDIF_PLL4P
		CLK_FDCAN_PLL4R
		CLK_SAI1_PLL3Q
		CLK_SAI2_PLL3Q
		CLK_SAI3_PLL3Q
		CLK_SAI4_PLL3Q
		CLK_RNG1_LSI
		CLK_RNG2_LSI
		CLK_LPTIM1_PCLK1
		CLK_LPTIM23_PCLK3
		CLK_LPTIM45_LSE
	>;

	/* VCO = 1300.0 MHz => P = 650 (CPU) */
	pll1: st,pll@0 {
		cfg = < 2 80 0 0 0 PQR(1,0,0) >;
		frac = < 0x800 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
	pll2: st,pll@1 {
		cfg = < 2 65 1 0 0 PQR(1,1,1) >;
		frac = < 0x1400 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 417.8 MHz => P = 209, Q = 25, R = 11 */
	pll3: st,pll@2 {
		cfg = < 1 33 1 16 36 PQR(1,1,1) >;
		frac = < 0x1a04 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 594.0 MHz => P = 99, Q = 74, R = 74 */
	pll4: st,pll@3 {
		cfg = < 3 98 5 7 7 PQR(1,1,1) >;
		u-boot,dm-pre-reloc;
	};

3.2. STM32MP157C-DK2 case[edit source]

This chapter shows the boot time clock tree set by the FSBL on STM32MP157C-DK2 DISCO board. Linux eventual runtime modifications are not covered here.

3.2.1. Clock tree[edit source]

The following table shows what STM32MP157C-DK2 clock tree looks like, as a result of the boot chain execution with the device tree built with STM32CubeMX.

Component              | Parent  |   Frequency     | Used?  | Comment                           |
-----------------------|---------|-----------------|--------|-----------------------------------|
LSI                    |N.A.     |    0.032000 MHz |  yes   | Mandatory for IWDG, DAC
  DAC                  |LSI      |    0.032000 MHz |  no    | 
  RNG1                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  RNG2                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  IWDG1                |LSI      |    0.032000 MHz |  yes   | 
  IWDG2                |LSI      |    0.032000 MHz |  yes   | 
LSE                    |N.A.     |    0.032768 MHz |  yes   | Mandatory for DTS
  RTC                  |LSE      |    0.032768 MHz |  yes   | 
  TAMP                 |LSE      |    0.032768 MHz |  yes   | 
  CEC                  |LSE      |    0.032768 MHz |  yes   | 
  LPTIM4               |LSE      |    0.032768 MHz |  yes   | 
  LPTIM5               |LSE      |    0.032768 MHz |  yes   | 
HSI                    |N.A.     |   64.000000 MHz |  yes   | 
  SPI4                 |HSI      |   64.000000 MHz |  yes   | Arduino
  SPI5                 |HSI      |   64.000000 MHz |  yes   | Rpi
  SPI6                 |HSI      |   64.000000 MHz |  no    | 
  I2C4                 |HSI      |   64.000000 MHz |  yes   | PMIC
  I2C6                 |HSI      |   64.000000 MHz |  no    | 
  I2C1                 |HSI      |   64.000000 MHz |  yes   | Rpi and peripherals
  I2C2                 |HSI      |   64.000000 MHz |  no    | 
  I2C3                 |HSI      |   64.000000 MHz |  no    | 
  I2C5                 |HSI      |   64.000000 MHz |  yes   | Rpi and Arduino
  USART1               |HSI      |   64.000000 MHz |  no    | 
  USART2               |HSI      |   64.000000 MHz |  yes   | Bluetooth
  USART3               |HSI      |   64.000000 MHz |  yes   | Rpi
  UART4                |HSI      |   64.000000 MHz |  yes   | Linux console
  UART5                |HSI      |   64.000000 MHz |  no    | 
  USART6               |HSI      |   64.000000 MHz |  no    | 
  UART7                |HSI      |   64.000000 MHz |  yes   | Arduino
  UART8                |HSI      |   64.000000 MHz |  no    | 
  MCO1                 |HSI      |   64.000000 MHz |  no    | Available so can be used
HSE                    |N.A.     |   24.000000 MHz |  yes   | 
  DSIPLL               |HSE      |  125.000000 MHz |  no    | DSI DPHY PLL
    DSIBL              |DSIPLL   |  125.000000 MHz |  no    | DSI lanebyte clock
  RTCDIV               |HSE      |    1.000000 MHz |  yes   | Only used when RTC source is HSE
  ck_per               |HSE      |   24.000000 MHz |  yes   | 
    ADC                |ck_per   |   24.000000 MHz |  yes   | Can use internal divider to be < 40MHz
  PLL1                 |HSE      | 1300.000000 MHz |  yes   | 
    PLL1P              |PLL1     |  650.000000 MHz |  yes   | 
      MPUDIV           |PLL1P    |  325.000000 MHz |  yes   | 
      Cortex-A7        |PLL1P    |  650.000000 MHz |  yes   | 
        MCO2           |Cortex-A7|  650.000000 MHz |  no    | Available so can be used
  PLL2                 |HSE      | 1066.000000 MHz |  yes   | 
    PLL2P              |PLL2     |  266.500000 MHz |  yes   | 
      AXI              |PLL2P    |  266.500000 MHz |  yes   | < 266MHz
        FMC            |AXI      |  266.500000 MHz |  no    | 
        QSPI           |AXI      |  266.500000 MHz |  no    | 
        SYSRAM         |AXI      |  266.500000 MHz |  yes   | 
        ROM            |AXI      |  266.500000 MHz |  yes   | 
        AHB5           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRYP1        |AHB5     |  266.500000 MHz |  yes   | 
          HASH1        |AHB5     |  266.500000 MHz |  yes   | 
          GPIOZ        |AHB5     |  266.500000 MHz |  yes   | 
          BKPSRAM      |AHB5     |  266.500000 MHz |  yes   | 
        AHB6           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRC1         |AHB6     |  266.500000 MHz |  yes   | 
          MDMA         |AHB6     |  266.500000 MHz |  yes   | 
          USBH         |AHB6     |  266.500000 MHz |  yes   | USB Host
          APB4         |AHB6     |  133.250000 MHz |  yes   | 
          APB5         |AHB6     |   66.625000 MHz |  yes   | 
            BSEC       |APB5     |   66.625000 MHz |  yes   | < 67MHz
            ETZPC      |APB5     |   66.625000 MHz |  yes   | 
            TZC        |APB5     |   66.625000 MHz |  yes   | 
        DBGAPB         |AXI      |  133.250000 MHz |  yes   | JTAG & Coresight
          DBGMCU       |DBGAPB   |   66.625000 MHz |  yes   | 
          STM          |DBGAPB   |   66.625000 MHz |  no    | 
    PLL2Q              |PLL2     |  533.000000 MHz |  yes   | 
      GPU              |PLL2Q    |  533.000000 MHz |  yes   | < 533MHz
    PLL2R              |PLL2     |  533.000000 MHz |  yes   | 
      DDR              |PLL2R    |  533.000000 MHz |  yes   | < 533MHz
  PLL3                 |HSE      |  417.755859 MHz |  yes   | 
    PLL3P              |PLL3     |  208.877930 MHz |  yes   | 
      MLAHB            |PLL3P    |  208.877930 MHz |  yes   | < 209MHz
        Cortex-M4      |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM1          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM2          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM3          |MLAHB    |  208.877930 MHz |  yes   | 
        RETRAM         |MLAHB    |  208.877930 MHz |  yes   | 
        AHB1           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
        AHB2           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          DMA1         |AHB2     |  208.877930 MHz |  yes   | 
          DMA2         |AHB2     |  208.877930 MHz |  yes   | 
          DMAMUX       |AHB2     |  208.877930 MHz |  yes   | 
        APB1           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM1       |APB1     |  104.438965 MHz |  yes   | 
          WWDG         |APB1     |  104.438965 MHz |  yes   | 
        APB2           |MLAHB    |  104.438965 MHz |  yes   | 
        TIM2           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM3           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM4           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM5           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM6           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM7           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM12          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM13          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM14          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM1           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM8           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM15          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM16          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM17          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        APB3           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM2       |APB3     |  104.438965 MHz |  yes   | 
          LPTIM3       |APB3     |  104.438965 MHz |  yes   | 
          SYSCFG       |APB3     |  104.438965 MHz |  yes   | 
          VREFBUF      |APB3     |  104.438965 MHz |  yes   | 
          DTS          |APB3     |  104.438965 MHz |  yes   | 
          HDP          |APB3     |  104.438965 MHz |  no    | 
        AHB3           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          CRC2         |AHB3     |  208.877930 MHz |  yes   | 
          CRYP2        |AHB3     |  208.877930 MHz |  yes   | 
          HASH2        |AHB3     |  208.877930 MHz |  yes   | 
          DCMI         |AHB3     |  208.877930 MHz |  no    | 
          IPCC         |AHB3     |  208.877930 MHz |  yes   | Mailbox
        AHB4           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          PWR          |AHB4     |  208.877930 MHz |  yes   | 
          RCC          |AHB4     |  208.877930 MHz |  yes   | 
          GPIOA-K      |AHB4     |  208.877930 MHz |  yes   | 
          EXTI         |AHB4     |  208.877930 MHz |  yes   | 
    PLL3Q              |PLL3     |   24.573874 MHz |  yes   | 
      SPI1             |PLL3Q    |   24.573874 MHz |  yes   | SPI2S1 for BT PCM
      SPI2             |PLL3Q    |   24.573874 MHz |  yes   | SPI2S2 for HDMI
      SPI3             |PLL3Q    |   24.573874 MHz |  no    | 
      DFSDM            |PLL3Q    |   24.573874 MHz |  no    | 
      SAI1             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI2             |PLL3Q    |   24.573874 MHz |  yes   | AudCodec 48kHz (use PLL3R for 44.1kHz)
      SAI3             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI4             |PLL3Q    |   24.573874 MHz |  no    | 
    PLL3R              |PLL3     |   11.290699 MHz |  yes   | 
  PLL4                 |HSE      |  594.000000 MHz |  yes   | 
    PLL4P              |PLL4     |   99.000000 MHz |  yes   | 
      SDMMC1           |PLL4P    |   99.000000 MHz |  yes   | µSD card
      SDMMC2           |PLL4P    |   99.000000 MHz |  yes   | Wifi
      SDMMC3           |PLL4P    |   99.000000 MHz |  yes   | Rpi
      SPDIF            |PLL4P    |   99.000000 MHz |  no    | 
    PLL4Q              |PLL4     |   74.250000 MHz |  yes   | 
      LCD              |PLL4Q    |   74.250000 MHz |  yes   | LTDC & DSI display pixel clock
    PLL4R              |PLL4     |   74.250000 MHz |  yes   | 
      FDCAN            |PLL4R    |   74.250000 MHz |  no    | 
  STGEN                |HSE      |   24.000000 MHz |  yes   | 
  USBPHYC              |HSE      |   24.000000 MHz |  yes   | USB PHY Ctrl for USB Host and OTG
    USBPLL             |USBPHYC  |   48.000000 MHz |  yes   | 
      USBO             |USBPLL   |   48.000000 MHz |  yes   | USB OTG
CSI                    |N.A.     |    4.000000 MHz |  yes   | Mandatory for IO compensation
ETH                    |N.A.     |    0.000000 MHz |  no    | ETH clocked by RGMII PHY
-----------------------|---------|-----------------|--------|-----------------------------------|
3.2.2. Device tree[edit source]

Here are the corresponding device tree rcc_clk sub node properties consumed by the first stage boot loader (FSBL) to configure the clock tree above:

	st,clksrc = <
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_PLL12_HSE
		CLK_PLL3_HSE
		CLK_PLL4_HSE
		CLK_RTC_LSE
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
	>;

	st,clkdiv = <
		1 /*MPU*/
		0 /*AXI*/
		0 /*MCU*/
		1 /*APB1*/
		1 /*APB2*/
		1 /*APB3*/
		1 /*APB4*/
		2 /*APB5*/
		23 /*RTC*/
		0 /*MCO1*/
		0 /*MCO2*/
	>;

	st,pkcs = <
		CLK_CKPER_HSE
		CLK_FMC_ACLK
		CLK_QSPI_ACLK
		CLK_ETH_DISABLED
		CLK_SDMMC12_PLL4P
		CLK_DSI_DSIPLL
		CLK_STGEN_HSE
		CLK_USBPHY_HSE
		CLK_SPI2S1_PLL3Q
		CLK_SPI2S23_PLL3Q
		CLK_SPI45_HSI
		CLK_SPI6_HSI
		CLK_I2C46_HSI
		CLK_SDMMC3_PLL4P
		CLK_USBO_USBPHY
		CLK_ADC_CKPER
		CLK_CEC_LSE
		CLK_I2C12_HSI
		CLK_I2C35_HSI
		CLK_UART1_HSI
		CLK_UART24_HSI
		CLK_UART35_HSI
		CLK_UART6_HSI
		CLK_UART78_HSI
		CLK_SPDIF_PLL4P
		CLK_FDCAN_PLL4R
		CLK_SAI1_PLL3Q
		CLK_SAI2_PLL3Q
		CLK_SAI3_PLL3Q
		CLK_SAI4_PLL3Q
		CLK_RNG1_LSI
		CLK_RNG2_LSI
		CLK_LPTIM1_PCLK1
		CLK_LPTIM23_PCLK3
		CLK_LPTIM45_LSE
	>;

	/* VCO = 1300.0 MHz => P = 650 (CPU) */
	pll1: st,pll@0 {
		cfg = < 2 80 0 0 0 PQR(1,0,0) >;
		frac = < 0x800 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
	pll2: st,pll@1 {
		cfg = < 2 65 1 0 0 PQR(1,1,1) >;
		frac = < 0x1400 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 417.8 MHz => P = 209, Q = 25, R = 11 */
	pll3: st,pll@2 {
		cfg = < 1 33 1 16 36 PQR(1,1,1) >;
		frac = < 0x1a04 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 594.0 MHz => P = 99, Q = 74, R = 74 */
	pll4: st,pll@3 {
		cfg = < 3 98 5 7 7 PQR(1,1,1) >;
		u-boot,dm-pre-reloc;
	};

For ecosystem release v1.0.0 More info.png[edit source]

3.3. STM32MP157C-EV1 case[edit source]

This chapter shows the boot time clock tree set by the FSBL on STM32MP157C-EV1 evaluation board. Linux eventual runtime modifications are not covered here.

3.3.1. Clock tree[edit source]

The following table shows what STM32MP157C-EV1 clock tree looks like, as a result of the boot chain execution with the device tree built with STM32CubeMX.

Component              | Parent  |   Frequency     | Used?  | Comment                           |
-----------------------|---------|-----------------|--------|-----------------------------------|
LSI                    |N.A.     |    0.032000 MHz |  yes   | Mandatory for IWDG, DAC
  DAC                  |LSI      |    0.032000 MHz |  yes   | 
  RNG1                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  RNG2                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  IWDG1                |LSI      |    0.032000 MHz |  yes   | 
  IWDG2                |LSI      |    0.032000 MHz |  yes   | 
LSE                    |N.A.     |    0.032768 MHz |  yes   | Mandatory for DTS
  RTC                  |LSE      |    0.032768 MHz |  yes   | 
  TAMP                 |LSE      |    0.032768 MHz |  yes   | 
  CEC                  |LSE      |    0.032768 MHz |  yes   | 
  LPTIM4               |LSE      |    0.032768 MHz |  yes   | 
  LPTIM5               |LSE      |    0.032768 MHz |  yes   | 
HSI                    |N.A.     |   64.000000 MHz |  yes   | 
  SPI4                 |HSI      |   64.000000 MHz |  no    | 
  SPI5                 |HSI      |   64.000000 MHz |  no    | 
  SPI6                 |HSI      |   64.000000 MHz |  yes   | 
  I2C4                 |HSI      |   64.000000 MHz |  yes   | PMIC
  I2C6                 |HSI      |   64.000000 MHz |  no    | 
  I2C1                 |HSI      |   64.000000 MHz |  no    | 
  I2C2                 |HSI      |   64.000000 MHz |  yes   | Rpi and peripherals
  I2C3                 |HSI      |   64.000000 MHz |  no    | 
  I2C5                 |HSI      |   64.000000 MHz |  yes   | Rpi
  USART1               |HSI      |   64.000000 MHz |  yes   | 
  USART2               |HSI      |   64.000000 MHz |  no    | 
  USART3               |HSI      |   64.000000 MHz |  yes   | Rpi
  UART4                |HSI      |   64.000000 MHz |  yes   | Linux console
  UART5                |HSI      |   64.000000 MHz |  no    | 
  USART6               |HSI      |   64.000000 MHz |  no    | 
  UART7                |HSI      |   64.000000 MHz |  no    | 
  UART8                |HSI      |   64.000000 MHz |  no    | 
  MCO1                 |HSI      |   64.000000 MHz |  no    | Available so can be used
HSE                    |N.A.     |   24.000000 MHz |  yes   | 
  DSIPLL               |HSE      |  125.000000 MHz |  no    | DSI DPHY PLL
    DSIBL              |DSIPLL   |  125.000000 MHz |  no    | DSI lanebyte clock
  RTCDIV               |HSE      |    1.000000 MHz |  yes   | Only used when RTC source is HSE
  ck_per               |HSE      |   24.000000 MHz |  yes   | 
    ADC                |ck_per   |   24.000000 MHz |  yes   | Can use internal divider to be < 40MHz
  PLL1                 |HSE      | 1300.000000 MHz |  yes   | 
    PLL1P              |PLL1     |  650.000000 MHz |  yes   | 
      MPUDIV           |PLL1P    |  325.000000 MHz |  yes   | 
      Cortex-A7        |PLL1P    |  650.000000 MHz |  yes   | 
        MCO2           |Cortex-A7|  650.000000 MHz |  no    | Available so can be used
  PLL2                 |HSE      | 1066.000000 MHz |  yes   | 
    PLL2P              |PLL2     |  266.500000 MHz |  yes   | 
      AXI              |PLL2P    |  266.500000 MHz |  yes   | < 266MHz
        FMC            |AXI      |  266.500000 MHz |  yes   | NAND flash
        QSPI           |AXI      |  266.500000 MHz |  yes   | NOR flash
        SYSRAM         |AXI      |  266.500000 MHz |  yes   | 
        ROM            |AXI      |  266.500000 MHz |  yes   | 
        AHB5           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRYP1        |AHB5     |  266.500000 MHz |  yes   | 
          HASH1        |AHB5     |  266.500000 MHz |  yes   | 
          GPIOZ        |AHB5     |  266.500000 MHz |  yes   | 
          BKPSRAM      |AHB5     |  266.500000 MHz |  yes   | 
        AHB6           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRC1         |AHB6     |  266.500000 MHz |  yes   | 
          MDMA         |AHB6     |  266.500000 MHz |  yes   | 
          USBH         |AHB6     |  266.500000 MHz |  yes   | USB Host
          APB4         |AHB6     |  133.250000 MHz |  yes   | 
          APB5         |AHB6     |   66.625000 MHz |  yes   | 
            BSEC       |APB5     |   66.625000 MHz |  yes   | < 67MHz
            ETZPC      |APB5     |   66.625000 MHz |  yes   | 
            TZC        |APB5     |   66.625000 MHz |  yes   | 
        DBGAPB         |AXI      |  133.250000 MHz |  yes   | JTAG & Coresight
          DBGMCU       |DBGAPB   |   66.625000 MHz |  yes   | 
          STM          |DBGAPB   |   66.625000 MHz |  yes   | 
    PLL2Q              |PLL2     |  533.000000 MHz |  yes   | 
      GPU              |PLL2Q    |  533.000000 MHz |  yes   | < 533MHz
    PLL2R              |PLL2     |  533.000000 MHz |  yes   | 
      DDR              |PLL2R    |  533.000000 MHz |  yes   | < 533MHz
  PLL3                 |HSE      |  417.755859 MHz |  yes   | 
    PLL3P              |PLL3     |  208.877930 MHz |  yes   | 
      MLAHB            |PLL3P    |  208.877930 MHz |  yes   | < 209MHz
        Cortex-M4      |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM1          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM2          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM3          |MLAHB    |  208.877930 MHz |  yes   | 
        RETRAM         |MLAHB    |  208.877930 MHz |  yes   | 
        AHB1           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
        AHB2           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          DMA1         |AHB2     |  208.877930 MHz |  yes   | 
          DMA2         |AHB2     |  208.877930 MHz |  yes   | 
          DMAMUX       |AHB2     |  208.877930 MHz |  yes   | 
        APB1           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM1       |APB1     |  104.438965 MHz |  yes   | 
          WWDG         |APB1     |  104.438965 MHz |  yes   | 
        APB2           |MLAHB    |  104.438965 MHz |  yes   | 
        TIM2           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM3           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM4           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM5           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM6           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM7           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM12          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM13          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM14          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM1           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM8           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM15          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM16          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM17          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        APB3           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM2       |APB3     |  104.438965 MHz |  yes   | 
          LPTIM3       |APB3     |  104.438965 MHz |  yes   | 
          SYSCFG       |APB3     |  104.438965 MHz |  yes   | 
          VREFBUF      |APB3     |  104.438965 MHz |  yes   | 
          DTS          |APB3     |  104.438965 MHz |  yes   | 
          HDP          |APB3     |  104.438965 MHz |  yes   | 
        AHB3           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          CRC2         |AHB3     |  208.877930 MHz |  yes   | 
          CRYP2        |AHB3     |  208.877930 MHz |  yes   | 
          HASH2        |AHB3     |  208.877930 MHz |  yes   | 
          DCMI         |AHB3     |  208.877930 MHz |  yes   | Camera
          IPCC         |AHB3     |  208.877930 MHz |  yes   | Mailbox
        AHB4           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          PWR          |AHB4     |  208.877930 MHz |  yes   | 
          RCC          |AHB4     |  208.877930 MHz |  yes   | 
          GPIOA-K      |AHB4     |  208.877930 MHz |  yes   | 
          EXTI         |AHB4     |  208.877930 MHz |  yes   | 
    PLL3Q              |PLL3     |   24.573874 MHz |  yes   | 
      SPI1             |PLL3Q    |   24.573874 MHz |  no    | 
      SPI2             |PLL3Q    |   24.573874 MHz |  no    | 
      SPI3             |PLL3Q    |   24.573874 MHz |  no    | 
      DFSDM            |PLL3Q    |   24.573874 MHz |  yes   | Digital micro
      SAI1             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI2             |PLL3Q    |   24.573874 MHz |  yes   | AudCodec 48kHz (use PLL3R for 44.1kHz)
      SAI3             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI4             |PLL3Q    |   24.573874 MHz |  yes   | SPDIF TX 48kHz (use PLL3R for 44.1kHz)
    PLL3R              |PLL3     |   11.290699 MHz |  yes   | 
  PLL4                 |HSE      |  594.000000 MHz |  yes   | 
    PLL4P              |PLL4     |   99.000000 MHz |  yes   | 
      SDMMC1           |PLL4P    |   99.000000 MHz |  yes   | µSD card
      SDMMC2           |PLL4P    |   99.000000 MHz |  yes   | eMMC
      SDMMC3           |PLL4P    |   99.000000 MHz |  yes   | 
      SPDIF            |PLL4P    |   99.000000 MHz |  yes   | SPDIF RX
    PLL4Q              |PLL4     |   74.250000 MHz |  yes   | 
      LCD              |PLL4Q    |   74.250000 MHz |  yes   | LTDC & DSI display pixel clock
    PLL4R              |PLL4     |   74.250000 MHz |  yes   | 
      FDCAN            |PLL4R    |   74.250000 MHz |  yes   | Should be as high as possible and < 100MHz
  STGEN                |HSE      |   24.000000 MHz |  yes   | 
  USBPHYC              |HSE      |   24.000000 MHz |  yes   | USB PHY Ctrl for USB Host and OTG
    USBPLL             |USBPHYC  |   48.000000 MHz |  yes   | 
      USBO             |USBPLL   |   48.000000 MHz |  yes   | USB OTG
CSI                    |N.A.     |    4.000000 MHz |  yes   | Mandatory for IO compensation
ETH                    |N.A.     |    0.000000 MHz |  no    | ETH clocked by RGMII PHY
-----------------------|---------|-----------------|--------|-----------------------------------|
3.3.2. Device tree[edit source]

Here are the corresponding device tree rcc_clk sub node properties consumed by the first stage boot loader (FSBL) to configure the clock tree above:

	st,clksrc = <
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_PLL12_HSE
		CLK_PLL3_HSE
		CLK_PLL4_HSE
		CLK_RTC_LSE
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
	>;

	st,clkdiv = <
		1 /*MPU*/
		0 /*AXI*/
		0 /*MCU*/
		1 /*APB1*/
		1 /*APB2*/
		1 /*APB3*/
		1 /*APB4*/
		2 /*APB5*/
		23 /*RTC*/
		0 /*MCO1*/
		0 /*MCO2*/
	>;

	st,pkcs = <
		CLK_CKPER_HSE
		CLK_FMC_ACLK
		CLK_QSPI_ACLK
		CLK_ETH_DISABLED
		CLK_SDMMC12_PLL4P
		CLK_DSI_DSIPLL
		CLK_STGEN_HSE
		CLK_USBPHY_HSE
		CLK_SPI2S1_PLL3Q
		CLK_SPI2S23_PLL3Q
		CLK_SPI45_HSI
		CLK_SPI6_HSI
		CLK_I2C46_HSI
		CLK_SDMMC3_PLL4P
		CLK_USBO_USBPHY
		CLK_ADC_CKPER
		CLK_CEC_LSE
		CLK_I2C12_HSI
		CLK_I2C35_HSI
		CLK_UART1_HSI
		CLK_UART24_HSI
		CLK_UART35_HSI
		CLK_UART6_HSI
		CLK_UART78_HSI
		CLK_SPDIF_PLL4P
		CLK_FDCAN_PLL4R
		CLK_SAI1_PLL3Q
		CLK_SAI2_PLL3Q
		CLK_SAI3_PLL3Q
		CLK_SAI4_PLL3Q
		CLK_RNG1_LSI
		CLK_RNG2_LSI
		CLK_LPTIM1_PCLK1
		CLK_LPTIM23_PCLK3
		CLK_LPTIM45_LSE
	>;

	/* VCO = 1300.0 MHz => P = 650 (CPU) */
	pll1: st,pll@0 {
		cfg = < 2 80 0 0 0 PQR(1,0,0) >;
		frac = < 0x800 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
	pll2: st,pll@1 {
		cfg = < 2 65 1 0 0 PQR(1,1,1) >;
		frac = < 0x1400 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 417.8 MHz => P = 209, Q = 25, R = 11 */
	pll3: st,pll@2 {
		cfg = < 1 33 1 16 36 PQR(1,1,1) >;
		frac = < 0x1a04 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 594.0 MHz => P = 99, Q = 74, R = 74 */
	pll4: st,pll@3 {
		cfg = < 3 98 5 7 7 PQR(1,1,1) >;
		u-boot,dm-pre-reloc;
	};

3.4. STM32MP157C-DK2 case[edit source]

This chapter shows the boot time clock tree set by the FSBL on STM32MP157C-DK2 DISCO board. Linux eventual runtime modifications are not covered here.

3.4.1. Clock tree[edit source]

The following table shows what STM32MP157C-DK2 clock tree looks like, as a result of the boot chain execution with the device tree built with STM32CubeMX.

Component              | Parent  |   Frequency     | Used?  | Comment                           |
-----------------------|---------|-----------------|--------|-----------------------------------|
LSI                    |N.A.     |    0.032000 MHz |  yes   | Mandatory for IWDG, DAC
  DAC                  |LSI      |    0.032000 MHz |  no    | 
  RNG1                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  RNG2                 |LSI      |    0.032000 MHz |  yes   | Input frequency should be as low as possible
  IWDG1                |LSI      |    0.032000 MHz |  yes   | 
  IWDG2                |LSI      |    0.032000 MHz |  yes   | 
LSE                    |N.A.     |    0.032768 MHz |  yes   | Mandatory for DTS
  RTC                  |LSE      |    0.032768 MHz |  yes   | 
  TAMP                 |LSE      |    0.032768 MHz |  yes   | 
  CEC                  |LSE      |    0.032768 MHz |  yes   | 
  LPTIM4               |LSE      |    0.032768 MHz |  yes   | 
  LPTIM5               |LSE      |    0.032768 MHz |  yes   | 
HSI                    |N.A.     |   64.000000 MHz |  yes   | 
  SPI4                 |HSI      |   64.000000 MHz |  yes   | Arduino
  SPI5                 |HSI      |   64.000000 MHz |  yes   | Rpi
  SPI6                 |HSI      |   64.000000 MHz |  no    | 
  I2C4                 |HSI      |   64.000000 MHz |  yes   | PMIC
  I2C6                 |HSI      |   64.000000 MHz |  no    | 
  I2C1                 |HSI      |   64.000000 MHz |  yes   | Rpi and peripherals
  I2C2                 |HSI      |   64.000000 MHz |  no    | 
  I2C3                 |HSI      |   64.000000 MHz |  no    | 
  I2C5                 |HSI      |   64.000000 MHz |  yes   | Rpi and Arduino
  USART1               |HSI      |   64.000000 MHz |  no    | 
  USART2               |HSI      |   64.000000 MHz |  yes   | Bluetooth
  USART3               |HSI      |   64.000000 MHz |  yes   | Rpi
  UART4                |HSI      |   64.000000 MHz |  yes   | Linux console
  UART5                |HSI      |   64.000000 MHz |  no    | 
  USART6               |HSI      |   64.000000 MHz |  no    | 
  UART7                |HSI      |   64.000000 MHz |  yes   | Arduino
  UART8                |HSI      |   64.000000 MHz |  no    | 
  MCO1                 |HSI      |   64.000000 MHz |  no    | Available so can be used
HSE                    |N.A.     |   24.000000 MHz |  yes   | 
  DSIPLL               |HSE      |  125.000000 MHz |  no    | DSI DPHY PLL
    DSIBL              |DSIPLL   |  125.000000 MHz |  no    | DSI lanebyte clock
  RTCDIV               |HSE      |    1.000000 MHz |  yes   | Only used when RTC source is HSE
  ck_per               |HSE      |   24.000000 MHz |  yes   | 
    ADC                |ck_per   |   24.000000 MHz |  yes   | Can use internal divider to be < 40MHz
  PLL1                 |HSE      | 1300.000000 MHz |  yes   | 
    PLL1P              |PLL1     |  650.000000 MHz |  yes   | 
      MPUDIV           |PLL1P    |  325.000000 MHz |  yes   | 
      Cortex-A7        |PLL1P    |  650.000000 MHz |  yes   | 
        MCO2           |Cortex-A7|  650.000000 MHz |  no    | Available so can be used
  PLL2                 |HSE      | 1066.000000 MHz |  yes   | 
    PLL2P              |PLL2     |  266.500000 MHz |  yes   | 
      AXI              |PLL2P    |  266.500000 MHz |  yes   | < 266MHz
        FMC            |AXI      |  266.500000 MHz |  no    | 
        QSPI           |AXI      |  266.500000 MHz |  no    | 
        SYSRAM         |AXI      |  266.500000 MHz |  yes   | 
        ROM            |AXI      |  266.500000 MHz |  yes   | 
        AHB5           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRYP1        |AHB5     |  266.500000 MHz |  yes   | 
          HASH1        |AHB5     |  266.500000 MHz |  yes   | 
          GPIOZ        |AHB5     |  266.500000 MHz |  yes   | 
          BKPSRAM      |AHB5     |  266.500000 MHz |  yes   | 
        AHB6           |AXI      |  266.500000 MHz |  yes   | < 266MHz
          CRC1         |AHB6     |  266.500000 MHz |  yes   | 
          MDMA         |AHB6     |  266.500000 MHz |  yes   | 
          USBH         |AHB6     |  266.500000 MHz |  yes   | USB Host
          APB4         |AHB6     |  133.250000 MHz |  yes   | 
          APB5         |AHB6     |   66.625000 MHz |  yes   | 
            BSEC       |APB5     |   66.625000 MHz |  yes   | < 67MHz
            ETZPC      |APB5     |   66.625000 MHz |  yes   | 
            TZC        |APB5     |   66.625000 MHz |  yes   | 
        DBGAPB         |AXI      |  133.250000 MHz |  yes   | JTAG & Coresight
          DBGMCU       |DBGAPB   |   66.625000 MHz |  yes   | 
          STM          |DBGAPB   |   66.625000 MHz |  no    | 
    PLL2Q              |PLL2     |  533.000000 MHz |  yes   | 
      GPU              |PLL2Q    |  533.000000 MHz |  yes   | < 533MHz
    PLL2R              |PLL2     |  533.000000 MHz |  yes   | 
      DDR              |PLL2R    |  533.000000 MHz |  yes   | < 533MHz
  PLL3                 |HSE      |  417.755859 MHz |  yes   | 
    PLL3P              |PLL3     |  208.877930 MHz |  yes   | 
      MLAHB            |PLL3P    |  208.877930 MHz |  yes   | < 209MHz
        Cortex-M4      |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM1          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM2          |MLAHB    |  208.877930 MHz |  yes   | 
        SRAM3          |MLAHB    |  208.877930 MHz |  yes   | 
        RETRAM         |MLAHB    |  208.877930 MHz |  yes   | 
        AHB1           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
        AHB2           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          DMA1         |AHB2     |  208.877930 MHz |  yes   | 
          DMA2         |AHB2     |  208.877930 MHz |  yes   | 
          DMAMUX       |AHB2     |  208.877930 MHz |  yes   | 
        APB1           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM1       |APB1     |  104.438965 MHz |  yes   | 
          WWDG         |APB1     |  104.438965 MHz |  yes   | 
        APB2           |MLAHB    |  104.438965 MHz |  yes   | 
        TIM2           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM3           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM4           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM5           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM6           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM7           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM12          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM13          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM14          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 1
        TIM1           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM8           |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM15          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM16          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        TIM17          |MLAHB    |  208.877930 MHz |  yes   | TIM Group 2
        APB3           |MLAHB    |  104.438965 MHz |  yes   | 
          LPTIM2       |APB3     |  104.438965 MHz |  yes   | 
          LPTIM3       |APB3     |  104.438965 MHz |  yes   | 
          SYSCFG       |APB3     |  104.438965 MHz |  yes   | 
          VREFBUF      |APB3     |  104.438965 MHz |  yes   | 
          DTS          |APB3     |  104.438965 MHz |  yes   | 
          HDP          |APB3     |  104.438965 MHz |  no    | 
        AHB3           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          CRC2         |AHB3     |  208.877930 MHz |  yes   | 
          CRYP2        |AHB3     |  208.877930 MHz |  yes   | 
          HASH2        |AHB3     |  208.877930 MHz |  yes   | 
          DCMI         |AHB3     |  208.877930 MHz |  no    | 
          IPCC         |AHB3     |  208.877930 MHz |  yes   | Mailbox
        AHB4           |MLAHB    |  208.877930 MHz |  yes   | < 209MHz
          PWR          |AHB4     |  208.877930 MHz |  yes   | 
          RCC          |AHB4     |  208.877930 MHz |  yes   | 
          GPIOA-K      |AHB4     |  208.877930 MHz |  yes   | 
          EXTI         |AHB4     |  208.877930 MHz |  yes   | 
    PLL3Q              |PLL3     |   24.573874 MHz |  yes   | 
      SPI1             |PLL3Q    |   24.573874 MHz |  yes   | SPI2S1 for BT PCM
      SPI2             |PLL3Q    |   24.573874 MHz |  yes   | SPI2S2 for HDMI
      SPI3             |PLL3Q    |   24.573874 MHz |  no    | 
      DFSDM            |PLL3Q    |   24.573874 MHz |  no    | 
      SAI1             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI2             |PLL3Q    |   24.573874 MHz |  yes   | AudCodec 48kHz (use PLL3R for 44.1kHz)
      SAI3             |PLL3Q    |   24.573874 MHz |  no    | 
      SAI4             |PLL3Q    |   24.573874 MHz |  no    | 
    PLL3R              |PLL3     |   11.290699 MHz |  yes   | 
  PLL4                 |HSE      |  594.000000 MHz |  yes   | 
    PLL4P              |PLL4     |   99.000000 MHz |  yes   | 
      SDMMC1           |PLL4P    |   99.000000 MHz |  yes   | µSD card
      SDMMC2           |PLL4P    |   99.000000 MHz |  yes   | Wifi
      SDMMC3           |PLL4P    |   99.000000 MHz |  yes   | Rpi
      SPDIF            |PLL4P    |   99.000000 MHz |  no    | 
    PLL4Q              |PLL4     |   74.250000 MHz |  yes   | 
      LCD              |PLL4Q    |   74.250000 MHz |  yes   | LTDC & DSI display pixel clock
    PLL4R              |PLL4     |   74.250000 MHz |  yes   | 
      FDCAN            |PLL4R    |   74.250000 MHz |  no    | 
  STGEN                |HSE      |   24.000000 MHz |  yes   | 
  USBPHYC              |HSE      |   24.000000 MHz |  yes   | USB PHY Ctrl for USB Host and OTG
    USBPLL             |USBPHYC  |   48.000000 MHz |  yes   | 
      USBO             |USBPLL   |   48.000000 MHz |  yes   | USB OTG
CSI                    |N.A.     |    4.000000 MHz |  yes   | Mandatory for IO compensation
ETH                    |N.A.     |    0.000000 MHz |  no    | ETH clocked by RGMII PHY
-----------------------|---------|-----------------|--------|-----------------------------------|
3.4.2. Device tree[edit source]

Here are the corresponding device tree rcc_clk sub node properties consumed by the first stage boot loader (FSBL) to configure the clock tree above:

	st,clksrc = <
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_PLL12_HSE
		CLK_PLL3_HSE
		CLK_PLL4_HSE
		CLK_RTC_LSE
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
	>;

	st,clkdiv = <
		1 /*MPU*/
		0 /*AXI*/
		0 /*MCU*/
		1 /*APB1*/
		1 /*APB2*/
		1 /*APB3*/
		1 /*APB4*/
		2 /*APB5*/
		23 /*RTC*/
		0 /*MCO1*/
		0 /*MCO2*/
	>;

	st,pkcs = <
		CLK_CKPER_HSE
		CLK_FMC_ACLK
		CLK_QSPI_ACLK
		CLK_ETH_DISABLED
		CLK_SDMMC12_PLL4P
		CLK_DSI_DSIPLL
		CLK_STGEN_HSE
		CLK_USBPHY_HSE
		CLK_SPI2S1_PLL3Q
		CLK_SPI2S23_PLL3Q
		CLK_SPI45_HSI
		CLK_SPI6_HSI
		CLK_I2C46_HSI
		CLK_SDMMC3_PLL4P
		CLK_USBO_USBPHY
		CLK_ADC_CKPER
		CLK_CEC_LSE
		CLK_I2C12_HSI
		CLK_I2C35_HSI
		CLK_UART1_HSI
		CLK_UART24_HSI
		CLK_UART35_HSI
		CLK_UART6_HSI
		CLK_UART78_HSI
		CLK_SPDIF_PLL4P
		CLK_FDCAN_PLL4R
		CLK_SAI1_PLL3Q
		CLK_SAI2_PLL3Q
		CLK_SAI3_PLL3Q
		CLK_SAI4_PLL3Q
		CLK_RNG1_LSI
		CLK_RNG2_LSI
		CLK_LPTIM1_PCLK1
		CLK_LPTIM23_PCLK3
		CLK_LPTIM45_LSE
	>;

	/* VCO = 1300.0 MHz => P = 650 (CPU) */
	pll1: st,pll@0 {
		cfg = < 2 80 0 0 0 PQR(1,0,0) >;
		frac = < 0x800 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
	pll2: st,pll@1 {
		cfg = < 2 65 1 0 0 PQR(1,1,1) >;
		frac = < 0x1400 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 417.8 MHz => P = 209, Q = 25, R = 11 */
	pll3: st,pll@2 {
		cfg = < 1 33 1 16 36 PQR(1,1,1) >;
		frac = < 0x1a04 >;
		u-boot,dm-pre-reloc;
	};

	/* VCO = 594.0 MHz => P = 99, Q = 74, R = 74 */
	pll4: st,pll@3 {
		cfg = < 3 98 5 7 7 PQR(1,1,1) >;
		u-boot,dm-pre-reloc;
	};