STM32MP15 distribution for Android release note - v1.0.0

Revision as of 10:53, 20 September 2019 by Registered User

This article describes the content of STM32MPU distribution for Android software release version Template:Highlight2, which is part of STM32MP15 ecosystem release note - v1.1.0.

1. Intended audience[edit source]

The targeted audience is STM32MP15 customers or partners.

2. Delivery scope and purpose[edit source]

The STM32MPU distribution for Android provides all necessary components for running, developing and/or making your own platform base don Android framework. It runs on the Arm® Cortex®-A7 processors, and is a fundamental part of the STM32MPU Embedded Software distribution for Android.

This delivery of STM32MPU distribution for Android is part of STM32MP15-Ecosystem-v1.0.0 (see the STM32MP15 ecosystem release note - v1.0.0).

3. Licensing[edit source]

This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).

All of the packages use the same source components. All components and their respective licenses are listed here.

4. Supported hardware[edit source]

This software delivery is compatible with the following boards:

5. Delivered features[edit source]

5.1. Main software components[edit source]

  • Android Common Kernel version v4.19.9
  • TF-A version v2.0
  • U-Boot version v2018.11-stm32mp-r2
  • OP-TEE version v3.3.0
  • STM32CubeMP1 FW v1.1.0
  • GStreamer version v1.14.2
  • GCC version arm-8.2-2019.01
  • openOCD version v0.10.0
  • GCnano version v6.2.4

5.2. Detailed features[edit source]

  • by components

5.2.1. Kernel part[edit source]

5.2.2. U-boot part[edit source]

5.2.3. TF-A part[edit source]

5.2.4. OP-TEE part[edit source]

  • or by main features
Domain Feature STM32MP15
Evaluation board
Comment
Boot Fastboot Yes Entering this mode through connect ST-Link console (uart) or by HW control
Verified boot No
A/B mechanism No A/B images available but boot on A by default
Recovery No
Multimedia Audio speaker Partially audio speaker output can be used only to connect heaset
Audio headset No
Audio USB No
Camera Yes
Camera USB No
Video SW decode Yes 480p30 max. without audio
Security SELinux Yes
Runtime verification No
Trust environment Yes OP-TEE
Keystore No Only default software solution available
Network and connectivity Ethernet Yes
Wifi Yes Using USB dongle (RTL8723AU)
Wifi hotspot No
BT / BLE Yes Using USB dongle (RTL8723AU)
USB Yes Mass storage / MTP / PTP
Systems Boot control Partially Available but not enable
Power control Partially Available but not enable
Thermal control Partially Available but not enable
Update engine No
Sensors Accelerometer No
Gyroscope No
Magnetometer No
Proximity No
Pressure No
Temperature No
Sensor Hub No
Debug ADB (USB) Yes
ADB (Ethernet) Yes
ADEB Yes
Perfetto Yes
SYSTRACE Yes
Metrics No
Storage USB Key Yes
microSD card Yes
eMMC Yes
Others Lights Yes
Touchscreen Yes

6. Recommendations for use[edit source]

7. Main restrictions list[edit source]

8. Minor release updates[edit source]

9. How to get started with st-android-9.0.0-2019-09-27[edit source]

Refer to How to get the software and start with this release.

10. Associated tools[edit source]

Refer to the Referenced tools release notes .

++ Android Studio?


11. Demo applications[edit source]

11.1. STCopro M4Echo application[edit source]

11.2. STCopro M4Example application[edit source]

12. Change log / Main changes[edit source]

Initial version.

13. Detailed delivery content[edit source]

13.1. Detailed description of STMicroelectronics modules[edit source]

13.1.1. BSP modules[edit source]

Module name Path of module Description
stm32mp1-bootloader device/stm/
stm32mp1-bootloader
Primary (Trusted Firmware-A) and secondary (Universal Boot Loader for embedded devices) bootloaders for STM32MP
STM32MPU distribution for Android licenses - v1.0.0
STM32MPU distribution for Android licenses - v1.0.0
stm32mp1-kernel device/stm/
stm32mp1-kernel
Linux STM32MP Kernel
STM32MPU distribution for Android licenses - v1.0.0
stm32mp1-tee device/stm/
stm32mp1-tee
OPTEE OS for STM32MP
STM32MPU distribution for Android licenses - v1.0.0
stm32mp1-openocd device/stm/
stm32mp1-openocd
Free and Open On-Chip Debugging, In-System Programming and Boundary-Scan Testing
Name Version License
stm32mp1-openocd 0.10.0 GPLv2

13.1.2. Common and peripherals modules[edit source]

Module name Path of module License Description
stm32mp1 device/stm/stm32mp1 TBD blabla
allocator device/stm/stm32mp1/peripheral/allocator TBD blabla
audio device/stm/stm32mp1/peripheral/audio TBD blabla
bootctrl device/stm/stm32mp1/peripheral/bootctrl TBD blabla
camera device/stm/stm32mp1/peripheral/camera TBD blabla
composer device/stm/stm32mp1/peripheral/composer TBD blabla
copro device/stm/stm32mp1/peripheral/copro TBD blabla
health device/stm/stm32mp1/peripheral/health TBD blabla
lights device/stm/stm32mp1/peripheral/lights TBD blabla
memtrack device/stm/stm32mp1/peripheral/memtrack TBD blabla
oemlock device/stm/stm32mp1/peripheral/oemlock TBD blabla
thermal device/stm/stm32mp1/peripheral/thermal TBD blabla
usb device/stm/stm32mp1/peripheral/usb TBD blabla
wifi device/stm/stm32mp1/peripheral/wifi TBD blabla

13.1.3. Board modules[edit source]

Module name Path of module License Description
eval device/stm/stm32mp1/eval TBD blabla

13.1.4. Coprocessor service module[edit source]

Module name Path of module License Description
CoproService packages/apps/CoproService TBD blabla

13.1.5. ST application modules[edit source]

Module name Path of module License Description
app vendor/stm/app TBD blabla