How to change audio device for Android

Revision as of 17:28, 22 August 2019 by Registered User (→‎Compile the Linux audio driver)

This article describes the integration steps required to connect your own audio device (inputs/outputs). It deals mainly with the Android impact of integrating the new audio solution. It is intended for Distribution Package users.

1. Prerequisites[edit source]

The environment must be installed using the Distribution Package adapted to your selected microprocessor device. See the list of Android Distribution Package.

The audio device (ex: Wolfson WM8994) must be already connected to the microprocessor device within your board.

2. Android audio overview[edit source]

Android Audio Overview

The Android audio software is structured in several layers:

  • Audio Drivers (hardware dependent) → interfaces providing a control and access to audio inputs or outputs
  • Audio Interface (audio@4-0, audio-effect@4.0) → hardware abstraction layers providing a standard way to configure the underlaying driver and audio-related functionality such as audio sources or sinks (as the Bluetooth stack for A2DP), based on the Android HIDL (Hardware Interface Definition Language) mechanism
  • Audio Server (audioserver) → native audio services managing routing, effects, mixing...
  • Audio JNI (Java Native Interface) → interfaces used to access the native audio services
  • Audio System service → several Android services useful for applications

3. Integrating[edit source]

The audio solution must be integrated in three main steps, explained in the next chapters:

  • Integrating within the Linux kernel
  • Integrating within Android
  • Validating

3.1. Integrating within the Linux kernel[edit source]

The audio integration in the Linux kernel is performed in two steps:

  • Add the audio driver within the compilation process
  • Update the device tree

3.1.1. Compile the Linux audio driver[edit source]

The audio subsystem is accessed through a dedicated driver (ALSA).

The Linux kernel audio driver documentation is available in the kernel sources, please refer to How to build kernel for Android for more information.

By default, audio is enabled within the kernel, adding the following lines within the android-soc.config available in kernel sources.

 CONFIG_SND=y
 CONFIG_SND_TIMER=y
 CONFIG_SND_PCM=y
 ...

Two options:

  • The audio driver is part of the Linux kernel source → select its config (e.g.: CONFIG_SND_SOC_WM8994=y for the Wolfson WM8994 audio codec). Refer to Updating the kernel configuration for more information.
  • The audio driver is provided separately → add it in the build_kernel.sh script

3.1.2. Update the Linux device tree[edit source]

The audio device tree documentation is available in the kernel sources.

Depending on the driver selected, it can be required to update the device tree (see Changing the Device Tree for more information).

3.2. Integrating within Android[edit source]

The audio device integration within Android is performed in several steps:

  • Add permissions to allow starting the required Android services
  • Add the audio interface (Hardware Abstraction Layer)
  • Configure the audio services (useful for audio policy)

3.2.1. Add Android permissions[edit source]

Three permissions can be added to ensure that the audio services are correctly started:

  • android.hardware.audio.output.xml for the audio track service
  • android.hardware.audio.low_latency.xml for the audio low latency service → ensure the use of a low latency audio card (not implemented by default)
  • android.hardware.audio.pro.xml for the audio pro service → ensure the use of a low latency audio card and audio high quality (not implemented by default)

For that purpose, it is required to add the following lines within the device.mk file:

PRODUCT_COPY_FILES += \
frameworks/native/data/etc/android.hardware.audio.output.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.audio.output.xml \
frameworks/native/data/etc/android.hardware.audio.low_latency.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.audio.low_latency.xml \
frameworks/native/data/etc/android.hardware.android.hardware.audio.pro.xml:$(TARGET_COPY_OUT_VENDOR)/etc/permissions/android.hardware.android.hardware.audio.pro.xml \

Note: the feature android.hardware.microphone, useful to start AudioRecord, is added by default within the different device core configurations (e.g.: wearable_core_hardware.xml for wearable devices)

3.2.2. Add the Android audio interface (Hardware Abstraction Layer)[edit source]

The audio interface is defined in hardware/interfaces/audio/

The default audio interface implementation is based on audio.<device>.so HAL libraries with the following devices:

  • Audio primary device (used to manage built-in audio inputs and outputs) → STMicroelectronics implementation available in device/stm/<STM32Series>/peripheral/audio
  • Audio usb device (used to manage USB audio inputs and outputs) → default implementation available in hardware/libhardware/modules/usbaudio/
  • Audio remote-submix device (used to loop audio signal between input and output) → default implementation available in hardware/libhardware/modules/audio_remote_submix
  • Audio a2dp device (used to manage Bluetooth A2DP audio inputs and outputs) → default implementation available in system/bt/audio_a2dp_hw

To select the required audio HAL (adapted to your requirements), first update the device.mk with the following information (STMicroelectronics implementation case):

 TARGET_USBAUDIO_HAL := default
 TARGET_PRIMARYAUDIO_HAL := stm
 TARGET_REMOTESUBMIX_AUDIO_HAL := default
 TARGET_A2DPAUDIO_HAL := default
 
 PRODUCT_PACKAGES += \
   libtinyalsa \
   tinyplay \
   tinycap \
   tinymix \
   tinypcminfo \
   libaudiohalcm \
 
 PRODUCT_PACKAGES += \
   audio.usb.$(TARGET_USBAUDIO_HAL) \
   audio.primary.$(TARGET_PRIMARYAUDIO_HAL)
   audio.r_submix.$(TARGET_REMOTESUBMIX_AUDIO_HAL)
   audio.a2dp.$(TARGET_A2DPAUDIO_HAL)
 
 PRODUCT_PROPERTY_OVERRIDES += \
   ro.hardware.audio.usb=$(TARGET_USBAUDIO_HAL) \
   ro.hardware.audio.primary=$(TARGET_PRIMARYAUDIO_HAL) \
   ro.hardware.audio.r_submix=$(TARGET_REMOTESUBMIX_AUDIO_HAL) \
   ro.hardware.audio.a2dp=$(TARGET_A2DPAUDIO_HAL)
 
 PRODUCT_PACKAGES += \
   android.hardware.audio@2.0-service \
   android.hardware.audio@4.0-impl \
   android.hardware.audio.effect@4.0-impl \
   android.hardware.soundtrigger@2.0-impl \
   libeffects

Then set the audio interfaces within the manifest.xml of the device (if not already performed):

 <manifest version="1.0" type="device">
   ...
   <hal format="hidl">
     <name>android.hardware.audio</name>
     <transport>hwbinder</transport>
     <version>4.0</version>
     <interface>
       <name>IDevicesFactory</name>
       <instance>default</instance>
     </interface>
   </hal>
   <hal format="hidl">
     <name>android.hardware.audio.effect</name>
     <transport>hwbinder</transport>
     <version>4.0</version>
     <interface>
       <name>IEffectsFactory</name>
       <instance>default</instance>
     </interface>
   </hal>
   ...
 </manifest>

It is possible to use the provided primary device implementation: configure it creating an xml file (example and directives are given within the file device/stm/<STM32Series>/peripheral/audio/audio.example.xml).

In this xml configuration file, you must set:

  • The mixer card number (e.g. /dev/snd/mixer0) and associated control settings executed at initialization
  • The list of devices (linked to Android audio devices) and the list of associated control setting (if any) to be executed in case of activation or deactivation
  • The list of stream card and device numbers (e.g. /dev/snd/pcmC1D0p) and the list of associated control setting (if any)

This file must be copied within the device in /vendor/etc/ directory adding these lines in the device.mk:

BOARD_USES_TINYHAL_AUDIO := true
PRODUCT_COPY_FILES += \
device/<STM32Series>/<BoardId>/media/audio/audio.stm.xml:$(TARGET_COPY_OUT_VENDOR)/etc/audio.<BoardId>.xml \

A basic implementation is available in the file device/stm/<STM32Series>/peripheral/audio/audio.stm.xml.

3.2.3. Configure the Android service[edit source]

The audio is potentially configured in two steps:

  • Create the audio policy configuration file giving information on audio capabilities of the platform (mandatory)
  • Customize the audio policy manager changing the decision rules concerning the audio

Additional information is available in the Android porting guide[1]

3.2.3.1. Audio policy configuration[edit source]

A file named audio_policy_configuration.xml must be created to give detailed configuration/capabilities of the integrated modules.

This file must contain the following information for each module (e.g for primary, usb, a2dp or remote_submix modules):

  • List of attached devices (ex: Speaker, HDMI...) and the default device (ex: Speaker) → include only the lists of built-in audio devices which are always present:
  • List of mixer ports and their possible configurations (ex: primary output and primary input with format PCM 16bits, 48kHz, stereo...)
  • List of device ports and their possible configurations (ex: speaker output with format PCM 16bits, 48kHz, mono...)
  • List of possible routings → links between possible sources (ex: primary output mixer port) and possible sinks (ex: Speaker device port)

In general, the default implementations of the modules are associated with the default configuration files available in frameworks/av/services/audiopolicy/config/ directory. You can then just include them.

These files must be copied within the device at /vendor/etc/ directory. For that purpose, you must add the following lines within the device.mk

USE_XML_AUDIO_POLICY_CONF := 1
PRODUCT_COPY_FILES += \
frameworks/av/services/audiopolicy/config/usb_audio_policy_configuration.xml:$(TARGET_COPY_OUT_VENDOR)/etc/usb_audio_policy_configuration.xml \
frameworks/av/services/audiopolicy/config/r_submix_audio_policy_configuration.xml:$(TARGET_COPY_OUT_VENDOR)/etc/r_submix_audio_policy_configuration.xml \
frameworks/av/services/audiopolicy/config/a2dp_audio_policy_configuration.xml:$(TARGET_COPY_OUT_VENDOR)/etc/a2dp_audio_policy_configuration.xml \
frameworks/av/services/audiopolicy/config/default_volume_tables.xml:$(TARGET_COPY_OUT_VENDOR)/etc/default_volume_tables.xml \
frameworks/av/services/audiopolicy/config/audio_policy_volumes.xml:$(TARGET_COPY_OUT_VENDOR)/etc/audio_policy_volumes.xml \
device/stm/<STM32Series>/<BoardId>/media/audio/audio_policy_configuration.xml:$(TARGET_COPY_OUT_VENDOR)/etc/audio_policy_configuration.xml

An example of implementation is available in device/stm/<STM32Series>/<BoardId>/media/audio/.

3.2.3.2. Audio policy customization[edit source]

The audio policy manager is required in Android, in charge of making all the audio related decisions (ex: audio output device selection, audio input device selection, audio routing, volume, mute...).

A default audio policy manager is implemented within framework/av/services/audiopolicy/managerdefault/.

It is possible to customize this policy (decision changes). For that purpose, there are two options:

  • Use the configurable audio policy implementation
  • Use your own implementation of the AudioPolicyManager (generating your own libaudiopolicymanager)
3.2.3.2.1. Configurable AudioPolicyManager[edit source]

To enable this option, you must add the following line within the device.mk

USE_CONFIGURABLE_AUDIO_POLICY := 1

This solution is based on the parameter-framework and an example of implementation is available for audio within framework/av/services/audiopolicy/engineconfigurable/parameter-framework/examples/.

3.2.3.2.2. Proprietary AudioPolicyManager[edit source]

To enable this option, you must add the following line within the device.mk file

USE_CUSTOM_AUDIO_POLICY:= 1

This solution requires to implement:

  • Your own AndroidPolicyManager class similar to the default one in framework/av/services/audiopolicy/managerdefault/ → generate for example a library libaudiopolicymanagerstm
  • Your own AndroidPolicyFactory similar to the default one in framework/av/services/audiopolicy/managerdefault/ → generate the required libaudiopolicymanager (statically linked with libaudiopolicymanagerstm)

3.3. Validating[edit source]

Audio validation can be performed in several steps:

  • Validate the Kernel integration
  • Check the audio Android compliance (CTS)

3.3.1. Validate the Kernel Integration[edit source]

Info white.png Information
It is required to build the Android distribution in eng or userdebug mode

Several tools are available to test audio at kernel level:

  • tinypcminfo → get capabilities of a stream input and output associated to a card/device pair
  • tinymix → used to control inputs and outputs (execute without parameter to get back list of controls)
  • tinycap → used to capture an audio stream input (card/device pair) within a .wav
  • tinyplay → used to play a .wav file on selected audio stream output (card/device pair)


If required, you can push a .wav file in the device storage:

 adb push file.wav /data

Open a device console executing:

 adb shell

Execute the following command to become root (needed to execute tiny tools):

 su


Some examples of commands:

  • Example on how to get information on the stream output:
 tinypcminfo -D 0 -d 0

Info for card 0, device 0:

PCM out:
      Access:	0x000009
   Format[0]:	0x000404
   Format[1]:	00000000
 Format Name:	S16_LE, S32_LE
   Subformat:	0x000001
        Rate:	min=32000Hz	max=48000Hz
    Channels:	min=2		max=2
 Sample bits:	min=16		max=32
 Period size:	min=32		max=16384
Period count:	min=2		max=4096

PCM in:
cannot open device '/dev/snd/pcmC0D0c'
Device does not exist.
  • Example on how to capture an audio frame in a file (mono signal at 16kHz/16bits format):
 tinycap test.wav -D 1 -d 0 -c 1 -r 16000 -b 16

Note: use Ctrl^C to stop capture


  • Example on how to play an audio file:
 tinyplay test.wav -D 0 -d 0
  • Example on how to control an audio card:
 tinymix -D 0 → used to get list of controls (with ctl IDs)
 tinymix -D 0 1 → used to get value of control with ctl ID = 1
 tinymix -D 0 1 0 → used to set value 0 to the control with ctl ID = 1

3.3.2. Execute the Audio CTS tests[edit source]

In the Android top directory, execute:

 make cts

Go in out/host/linux-x86/cts/android-cts/tools/ directory and execute:

 ./cts-tradefed

It is recommended to execute at least "CtsMediaTestCases" test suite:

 run cts --skip-preconditions --module CtsMediaTestCases

For more information on the CTS execution, see the Android compatibility guide[2]

4. References[edit source]