Template:ArticleMainWriter Template:ArticleFirstDraftVersion
1. Article purpose[edit source]
This article explains step by step how to create your own The Things Network LoRaWan gateway based on the STM32MP1.
2. Hardware needed[edit source]
The concentrator LoRaWan RAK831
The converter board
This bundle allows to start with all the hardware needed. (pick your geographic area)
3. Prerequisites[edit source]
The prerequisites from Installing the OpenSTLinux distribution must be executed.
4. How to create the LoRaWan gateway layer[edit source]
To start you need to add the LoRaWan gateway layer to your Distribution Package environment.
cd <working directory path of distribution>/openstlinux-4.19-thud-mp1-19-02-20/layers/meta-st git clone "https://gerrit.st.com/stm32mpuapp/meta/meta-st-stm32mpu-app-lorawan"
5. How to build the binaries[edit source]
The next step is to create the build for the LoRaWan gateway
cd <working directory path of distribution>/openstlinux-4.19-thud-mp1-19-02-20 source layers/meta-st/scripts/envsetup.sh
choose openstlinux-weston then stm32mp1-lorawan-a7 as machine.
bitbake st-image-lorawan
This may take some time.
6. How to create the SD card[edit source]
The final step is to 'populate the SD card with the binaries compiled previously:
cd <working directory path of distribution>/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxwestonextra-stm32mp1-lorawan-a7 cd tmp-glibc/deploy/images/stm32mp1-lorawan-a7/scripts/ ./create_sdcard_from_flashlayout.sh ../flashlayout_st-image-lorawan/FlashLayout_sdcard_stm32mp157c-lorawan-a7-mx-trusted.tsv sudo umount `lsblk --list | grep mmcblk0 | grep part | gawk '{ print $7 }' | tr '\n' ' '` sudo dd if=../flashlayout_st-image-lorawan/../flashlayout_st-image-lorawan_FlashLayout_sdcard_stm32mp157c-lorawan-a7-mx-trusted.raw of=/dev/mmcblk0 bs=8M conv=fdatasync status=progress
(more informations in the How to populate the SD card with dd command page)
You can now assemble the modules to the board.
This is how it should look:
7. Launching the binaries on the board[edit source]
This part explains how to launch the LoRaWan service on the board.
cd /usr/local/lorawan-gateway/ ./LoRaWan_gateway_launcher.sh
- During the launcher script, enter your prefered server, up and down ports when it is asked.
- Important: at the end of the script, copy your EUI before the restart of the gateway
In any case, all those informations can be found or changed manually in the global_conf.json and local_conf.json files in /usr/local/lorawan-gateway/ on the board.
8. How to proceed on The Things Network[edit source]
Login or create an account on https://www.thethingsnetwork.org
- Go into your Console.
- Clic on GATEWAYS.
- Clic on register gateway.
- Check I'm using the legacy packet forwarder and enter your EUI you previously copied.
- Enter a description of the gateway, this is the name you can see on the map of the site.
- Select your Frequency Plan.
- Select your Router (for europe choose ttn-router-eu).
- You can place your gateway on the map by clicking on it or by entering directly the precise coordinates.
- Tell if your antenna is indoor or outdoor.