STM32-CoPro-MPU plugin release note

Revision as of 18:04, 6 February 2019 by imported>Frq08554

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


More information can be found in the detailed release notes referenced later in this article.

1. System Workbench for STM32 2.8.0 - STM32-CoPro-MPU plugin version 1.0.0[edit source]

The STM32-CoPro-MPU plugin, based onto the System Workbench for STM32 (SW4STM32), targets the support of Cortex®-M core contained in the STM32MP1 Family.
It is included in System Workbench fro STM32 from version 2.8.0.
It provides:

  • the target status widget,
  • the console management,
  • the project creation, compilation and debug in two modes:
    • Engineering Mode,
    • Production Mode, with Cortex®-M firmware download :
      • via Ethernet
      • or serial link (on Linux® host only)
  • the remote system explorer configuration


It is available on Linux® and Windows® platforms.


If STM32-CoPro-MPU plugin is not already present, it can be installed onto your System Workbench using the System Workbench for STM32 - Updates defined in menu Windows > Preferences > Install/Update > Available Software Site.
The installation is then the standard Eclipse one: Help > Install New Software...

If already installed, it can be upgraded to version 1.0.0 using the same System Workbench for STM32 - Updates.
The update is the standard Eclipse one: Help > Check for Updates.

In order to access to the Ac6 site, take care to configure proxy at Eclipse level: in Windows > Preferences > General > Network Connections; Active Provider set to Manual.
Then after selecting HTTP proxy entry, click Edit... and enter your proxy setup.


IDE for Linux® host PC IDE for Windows® host PC
Download

Version 1.0.0 in SW4STM32 2.8.0

Template:STdotcomInfo

  • Download the all-in-one Linux installer 2.8 install_sw4stm32_linux_64bits-v2.8.run from openstm32.org

Version 1.0.0 in SW4STM32 2.8.0

Template:STdotcomInfo

  • Download the all-in-one Windows installer 2.8 install_sw4stm32_win_64bits-v2.8.exe from openstm32.org
Installation
  • Run the installation script
$ chmod +x install_sw4stm32_linux_64bits-v2.8.run
$ ./install_sw4stm32_linux_64bits-v2.8.run
  • Run the installation exe
$ install_sw4stm32_win_64bits-v2.8.exe
Detailed release notes Details about the content of this tool version are available on openstm32.org

Details about the content of this tool version are available on openstm32.org



2. Archives[edit source]

2.1. Eclipse IDE : STM32-CoPro-MPU plugin - version 0.4.9[edit source]

The STM32-CoPro-MPU plugin, based onto the System Workbench for STM32 (SW4STM32), targets the support of Cortex®-M core contained in the STM32MP1 Family.
It provides:

  • the target status widget,
  • the console management,
  • the project creation, compilation and debug in two modes:
    • Engineering Mode,
    • Production Mode, with Cortex®-M firmware download :
      • via Ethernet
      • or serial link (on Linux® host only)
  • the remote system explorer configuration


It is available on Linux® and Windows® platforms.

IDE for Linux® host PC IDE for Windows® host PC
Download

Version 0.4.9

Template:STdotcomInfo

Version 0.4.9

Template:STdotcomInfo

Installation
  • Uncompress the archive file to get IDE:
$ unzip STM32-CoPro-MPU_Full_Install_linux64_0.4.9.zip
  • Then follow instructions given in the detailed release note to finalize the installation
  • When the installation is over, to use the tool, you can follow instruction given in STM32-CoPro-MPU plugin for SW4STM32 or in the detailed release note.
  • Uncompress the archive file to get IDE:
$ unzip STM32-CoPro-MPU_Full_Install_win64_0.4.9.zip
  • Then follow instructions given in the detailed release note to finalize the installation
  • When the installation is over, to use the tool, you can follow instruction given in STM32-CoPro-MPU plugin for SW4STM32 or in the detailed release note.
Detailed release notes Details about the content of this tool version are available in the <System Workbench for STM32 installation directory>/README.htm file
  • If you are interested in former releases, please go through the archives

Details about the content of this tool version are available in the <System Workbench for STM32 installation directory>/README.htm file

2.2. Eclipse IDE : STM32-CoPro-MPU plugin - version 0.4.8[edit source]

The STM32-CoPro-MPU plugin, based onto the System Workbench for STM32 (SW4STM32), targets the support of Cortex®-M core contained in the STM32MP1 Family.
It provides:

  • the target status widget,
  • the console management,
  • the project creation, compilation and debug in two modes:
    • Engineering Mode,
    • Production Mode, with Cortex®-M firmware download :
      • via Ethernet
      • or serial link (on Linux® host only)
  • the remote system explorer configuration


It is available on Linux® and Windows® platforms.

IDE for Linux® host PC IDE for Windows® host PC
Download

Version 0.4.8

Template:STdotcomInfo

Version 0.4.8

Template:STdotcomInfo

Installation
  • Uncompress the archive file to get IDE:
$ unzip STM32-CoPro-MPU_Full_Install_linux64_0.4.8.zip
  • Then follow instructions given in the detailed release note to finalize the installation
  • When the installation is over, to use the tool, you can follow instruction given in STM32-CoPro-MPU plugin for SW4STM32 or in the detailed release note.
  • Uncompress the archive file to get IDE:
$ unzip STM32-CoPro-MPU_Full_Install_win64_0.4.8.zip
  • Then follow instructions given in the detailed release note to finalize the installation
  • When the installation is over, to use the tool, you can follow instruction given in STM32-CoPro-MPU plugin for SW4STM32 or in the detailed release note.
Detailed release notes Details about the content of this tool version are available in the <System Workbench for STM32 installation directory>/README.htm file
  • If you are interested in former releases, please go through the archives

Details about the content of this tool version are available in the <System Workbench for STM32 installation directory>/README.htm file


2.3. Eclipse IDE - version 0.4.1[edit source]

IDE for Linux host PC IDE for Windows host PC
Download

Version 0.4.1

Template:STdotcomInfo

No version available yet for Windows

Installation
  • Uncompress the archive file to get IDE:
$ unzip STM32-CoPro-MPU_Full_Install_linux64_0.4.1.zip
  • Then follow instructions given in the detailed release note to finalize the installation
  • When the installation is over, to use the tool, you can follow instruction given in STM32-CoPro-MPU plugin for SW4STM32 or in the detailed release note.

No version available yet for Windows

Detailed release notes Details about the content of this tool version are available in the <System Workbench for STM32 installation directory>/README.htm file
  • If you are interested in former releases, please go through the archives

No version available yet for Windows