This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article explains how to set up the RSE Perspective with STM32CubeIDE.
1. RSE Perspective set-up[edit source]
RSE is implemented in a dedicated Eclipse perspective that you have to open:
- Go to Window -> Perspective -> Open Perspective -> Other...
- Choose Remote System Explorer
2. Automatic RSE Connection[edit source]
After launching a first Debug Configuration in Production Mode via network, a ready-to-use RSE connection is created: MPU Target.
The Sftp Files directory gives access to the remote file system. The Ssh Shells provide an interface handling remote shell.
For more information about RSE in Eclipse, please see the RSE User Guide