This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Coming soon |
1. Introduction[edit source]
This article will explain how to set up a Point-to-Point connection to the MPU target, in case of a proxy is also setup on the PC for accessing the Internet.
2. Setting up proxy[edit source]
To set up the connection go to Windows -> Preferences -> General -> Network Connections.
Select "manual" in the Active Provider field.
Click on Add Host... and then add the board ip address in the Proxy bypass window.