STM32MP15 device tree

Revision as of 11:13, 14 February 2020 by Registered User (→‎First trial)

1. Purpose and scope[edit source]

This article shows the structure of the device tree files as it is implemented in STM32MP15 for the following software components: Linux® kernel, U-Boot and TF-A.

The purpose of this article is not to explain the device tree concept and the device tree configuration supported by STM32MP15. A good knowledge of the concept is a prerequisite before reading this article. The articles regarding the configuration can be read afterwards.

2. Device tree structure for Linux, U-Boot and TF-A[edit source]

2.1. Introduction[edit source]

The device tree files are used during boot time by the FSBL (TF-A / U-Boot SPL), the SSBL (U-Boot), and eventually by the Linux kernel.
These files are stored in different repositories, but source code reuse is maximized from one repository to another:

  • The initial device tree files supporting STM32MP15 are created in the Linux kernel.
  • In U-Boot, Linux files are copied and overloaded with U-Boot properties (including DDR configuration).
  • In TF-A, Linux files are partly copied (for device tree blob size optimization), and then completed with the DDR configuration copied from U-Boot, and with the security configuration (firewalling).


The figure below shows the device tree creation flow for Linux, U-Boot and TF-A:

Device tree for Linux U-Boot TF-A.png

Color legend:

  •  Linux  in dark blue
  •  U-Boot  in green
  •  TF-A  in pink
  •  STM32CubeMX generated parts  in light blue

The above color codes are used for all the figures included in this article.

2.2. Upstreamed device tree[edit source]

2.2.1. Overview[edit source]

As explained in the STM32 MPU Embedded Software Open Source Software (OSS) philosophy, STMicroelectronics maximizes the usage of open source software and the upstreaming to the communities.

As a result, the device tree files supporting the evaluation board and the Discovery kit are upstreamed to Linux , U-Boot and TF-A repositories.

2.2.2. Linux[edit source]

Device tree Linux upstreamed.png
Device tree legend.png


2.2.3. U-Boot[edit source]

Device tree U-Boot upstreamed.png
Device tree legend.png


2.2.4. TF-A[edit source]

Device tree TF-A upstreamed.png
Device tree legend.png


Note: The hashed areas on Linux device tree files represent the fact that these files are partly copied in TF-A.


2.3. Manual customization of STM32MP15 reference device tree[edit source]

As we can see on the above sections, current device tree structure is based on STM32MP157C configuration. So anyone could wonder how to proceed in case of other STM32MP15 part numbers (see STM32MP15 microprocessor diversity for reference).
Here is below how to proceed.

2.3.1. Generic setup[edit source]

This first step will allow you to boot with any STM32MP15 reference but you will get some warning or error message on the console (without consequence with the boot success).

2.3.1.1. Whatever your chip reference, include "stm32mp157c.dtsi":[edit source]

This is the super set of device tree declaration corresponding to the largest feature set of STM32MP15 microprocessor.

2.3.1.2. Include the pinctrl reference file corresponding to your package size (a, b, c or d)[edit source]
  • stm32mp157caa-pinctrl.dtsi for 18x18 package
  • stm32mp157cab-pinctrl.dtsi for 16x16 package
  • stm32mp157cac-pinctrl.dtsi for 14x14 package
  • stm32mp157cad-pinctrl.dtsi for 12x12 package

2.3.2. Clean up[edit source]

2.3.2.1. Customize your "stm32mp157c.dtsi" file to remove any configuration not relevant for your STM32MP15 reference[edit source]

For example:

  • remove cpu1 core if not relevant
  • All the possible peripherals are configured but not activated so should be ok.
2.3.2.2. Make sure your are activating in your board only the peripherals available on your STM32MP15 reference[edit source]

For example:

  • devices linked to security and cryptography for non secured microprocessors (157axxx)
  • devices removed like CAN, DSI, GPU from MP15x lines

2.4. STM32CubeMX generated device tree[edit source]

2.4.1. Overview[edit source]

STM32CubeMX can be used to generate the device tree files for a given project. The tool generates the files  highlighted in light blue  in the following diagrams, including the upstreamed files shown in the previous chapter.


The device tree files generated by STM32CubeMX can be built with the Developer Package or Distribution Package:

2.4.2. Linux[edit source]

Device tree Linux STM32CubeMX.png


2.4.3. U-Boot[edit source]

Device tree U-Boot STM32CubeMX.png


2.4.4. TF-A[edit source]

Device tree TF-A STM32CubeMX.png