Template:ArticleMainWriter Template:ArticleProposedVersion Template:ReviewersList
1. Purpose[edit source]
This article explains how to update boot chain (trusted mode) in case of use of a "customised" devicetree.
As exemple, CubeMX is able to generate "customised" devicetree.
This article describes how to update the DTB (devicetree compiled) part of the boot binaries.
2. Rationale[edit source]
The rationale to not use the devicetree provided by OpenSTLinux distribution and prefer a "customised" devicetree is various;
- You made your own board
- You need to swap some IPs from MCU side to MPU side (or reverse)
- For any other reason...
3. Pre-requisites[edit source]
This article only need to update three software of the complete boot chain (trusted mode); Trusted Firmware A (TF-A), u-boot and the Linux kernel.
Modifying those software need to handle :
- Starter package :
- need flashlayout and images to flash provided from file IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
- Developer package :
- Need components sources and patches which are provided by file SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
- Need SDK toolchain which is provided by file SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz
- (optionnal) STM32CubeProgrammer: the tool used to flash the images and binaries into target
- Custom devicetree sources:
- For the rest of document the custom devicetree are considered generated by STM32CubeMX and stored in a tarball MyDeviceTree_fromCubeMX.tar.xz with following file tree:
MyDeviceTree_fromCubeMX |-- kernel | |-- stm32mp157c-mydevicetree-mx.dts |-- tf-a | |-- stm32mp15-mx.h | |-- stm32mp157c-mydevicetree-mx.dts |-- u-boot | |-- stm32mp15-mx.h | |-- stm32mp157c-mydevicetree-mx-u-boot.dtsi | |-- stm32mp157c-mydevicetree-mx.dts
- Make sure PC_Prerequisite#Linux PC have been run (even with a WSL2 setup)
4. Prepare your environnement[edit source]
As seen in #Pre-requisites, there are numerus inputs so here a proposition to organize your environment.
Better is to create a dedicated WORKDIR somewhere in your HOME. Then copy all inputs quoted in #Pre-requisites in that just created WORKDIR:
- cd
- mkdir WORKDIR
- cd WORKDIR
- export WORKDIR="$PWD"
- tar --strip-components=1 -xf <IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
- tar --strip-components=1 -xf <SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
- tar --strip-components=1 -xf <SDK-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
- tar xf <MyDeviceTree_fromCubeMX.tar.xz> -C $WORKDIR/
Then proceed in the SDK installation.
Commands of the rest of the document should be run in a SDK environment context (Starting_up_the_SDK).
5. Kernel device tree update[edit source]
Updating the devicetree of kernel only needs to replace the 'dtb' file of '/boot' partition.
Indeed 'extlinux.conf' explicitly points on the dtb the kernel should use (something like '/boot/<devicetree>.dtb').
Below the procedure to generate and then copy new DTB in target:
5.1. Kernel : unpack and patch sources[edit source]
Run following command into a shell:
- pushd $WORKDIR
- mkdir -p kernel
- tar xf sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.*.tar.xz -C kernel
- mv kernel/linux-* kernel/kernel-sources/
- pushd kernel/kernel-sources/
- for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/*.patch); do patch -p1 < $p; done
- popd
- popd
5.2. Kernel : copy dts into source code[edit source]
- pushd $WORKDIR
- cp -r MyDeviceTree_fromCubeMX/kernel kernel/kernel-sources/arch/arm/boot/dts/
- popd
5.3. Kernel : regenerate kernel DTB[edit source]
- pushd $WORKDIR/kernel/kernel-sources
- make O="$PWD/../build" multi_v7_defconfig
- for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config $f; done
- make oldconfig O="$PWD/../build"
- make dtbs LOADADDR=0xC2000040 O="$PWD/../
- popd
- ls -l $WORKDIR/kernel/build/arch/arm/boot/dts/st*.dtb
5.4. Kernel : copy DTB into bootfs[edit source]
First of all update bootfs with the just new DTB to take it into account on next boot of the target.
Then if needed update extlinux of target according this new dtb filename. This is only needed if the filename of the dtb generated is diferent from the one used by extlinux to boot.
6. U-Boot device tree update[edit source]
Updating the devicetree of u-boot needs to replace the 'dtb' part of the u-boot binary.
By adding new devicetree to u-boot source code, the Makefile will regenerate a new u-boot.stm32 containing the new 'dts'
6.1. U-boot : unpack and patch sources[edit source]
- pushd $WORKDIR
- mkdir -p u-boot
- tar xf sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/v*.tar.gz -C u-boot
- mv u-boot/u-boot* u-boot/u-boot-sources/
- pushd u-boot/u-boot-sources
- for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/*.patch); do patch -p1 < $p; done
- popd
6.2. U-boot : copy DTS in u-boot source code[edit source]
- pushd $WORKDIR/u-boot/u-boot-sources
- cp ../../MyDeviceTree_fromCubeMX/u-boot/* arch/arm/dts/
- popd
6.3. U-boot : regenerate u-boot.stm32[edit source]
- pushd $WORKDIR/u-boot/u-boot-sources
- make stm32mp15_<config>_defconfig
- <config> : could be trusted or basic according the boot type
- make DEVICE_TREE=<device tree> all
- <device tree> : is the devicetree just copied, i.e.: stm32mp157c-mydevicetree-mx
- popd
- ls -l $WORKDIR/u-boot/u-boot-sources/u-boot.stm32
6.4. U-boot : copy u-boot on target[edit source]
- Because of 'extlinux' and before flashing the new u-boot.stm32, make sure #extlinux update is done according the 'compatible' value in DTS file.
- Then flash the u-boot.stm32 into 'ssbl' partition of the target with STM32CubeProgrammer else using 'dd' as following :
- dd if=u-boot.stm32 of=Template:Highlight3 conv=fdatasync
7. TF-A device tree update[edit source]
Updating the devicetree of TF-A needs to replace the 'dtb'part of the TF-A binary.
TF-A binary allocates just after the 'mkimage" headers a 'fixed' zone for DTB. DTB is smaller than the reserved zone, padding is done with zero.
Below the procedure to generate TF-A with a new DTB and then flash it on target:
7.1. TF-A : unpack and patch sources[edit source]
- pushd $WORKDIR
- mkdir -p tf-a
- tar xf sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/v*.tar.gz -C tf-a
- mv tf-a/arm-trusted-firmware-* tf-a/tf-a-sources
- pushd tf-a/tf-a-sources
- for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/*.patch); do patch -p1 < $p; done
- popd
- popd
7.2. TF-A : copy dts into source code[edit source]
- pushd $WORKDIR/tf-a
- cp -r ../MyDeviceTree_fromCubeMX/tf-a tf-a-sources/fdts/
- popd
7.3. TF-A : regenerate TF-A.stm32[edit source]
- pushd $WORKDIR/tf-a/tf-a-sources
- make -f $PWD/../Makefile.sdk TFA_DEVICETREE=<device tree> TF_A_CONFIG=<config> all
- <config> : could be trusted or basic according the boot type
- <device tree> : is the devicetree just copied, i.e.: stm32mp157c-mydevicetree-mx
- popd
- ls -l $WORKDIR/tf-a/build/<config>/tf-a-<device tree>-<config>.stm32
7.4. TF-A : copy DTB on target/bootfs[edit source]
Then flash the tf-a-*.stm32 into the 'fsbl1' and 'fsbl2' partitions of the target with STM32CubeProgrammer else use 'dd' as follow:
- dd if=tf-a.stm32 of=Template:Highlight3 conv=fdatasync
- dd if=tf-a.stm32 of=Template:Highlight3 conv=fdatasync
8. Update methods[edit source]
8.1. bootfs update[edit source]
- scp stm32mp157c-mydevicetree-mx.dtb root@<Target_IP>:/boot/
This method doesn't need to have a target up and running but only need the "st-image-bootfs-openstlinux-weston-stm32mp1.ext4" file. To modify a 'ext4' file, a loopback mount tool is need which is avaible in any Linux Distribution (even through Windows 10 via WSL2):
- mkdir -p $WORKING/bootfs
- mount -o loop Template:Highlight3 $WORKING/bootfs
- ##Then copy the new dtb file at the root of $WORKING/bootfs
- umount $WORKING/bootfs
- sync
- dd if=Template:Highlight3 of=Template:Highlight3 conv=fdatasync
8.2. extlinux update[edit source]
8.2.1. extlinux : basics[edit source]
'extlinux' is a collection of scripts/config files describing how u-boot should boots. Updating extlinux consists in updating the extlinux.conf.
- As exemple by using a DK-2 board and booting on sdcard, then the extlinux.conf file is located in "/boot/mmc0_stm32mp157c-dk2_extlinux/".
- If "mmc0_Template:Highlight3_extlinux" directory is not available, please use "/boot/extlinux/extlinux.conf" file instead.
'extlinux.conf' is the description of a boot menu with one or several entries, 'DEFAULT' selects the one to use by default .
Below an exemple of file:
menu title Select the boot mode MENU BACKGROUND ../splash.bmp TIMEOUT 5 DEFAULT stm32mp157c-mydevicetree-mx LABEL stm32mp157c-dk2-sdcard KERNEL /uImage FDT /stm32mp157c-dk2.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-dk2-a7-examples-sdcard KERNEL /uImage FDT /stm32mp157c-dk2-a7-examples.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-dk2-m4-examples-sdcard KERNEL /uImage FDT /stm32mp157c-dk2-m4-examples.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 LABEL stm32mp157c-mydevicetree-mx KERNEL /uImage FDT /stm32mp157c-mydevicetree-mx.dtb APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
In example above the highlighted lines may need to be updated/added by this wiki page:
- DEFAULT: This is the default 'LABEL' to boot
- LABEL : The entry 'LABEL' is the value of 'compatible' of the DTS file compiled with u-boot.
- The 'compatible' value is at head of the DTS file and looks like : "st,stm32mp157c-mydevicetree-mx"
- FDT : The path from /boot of the kernel DTB to use
8.2.2. extlinux : updating[edit source]
Updating 'extlinux' consists into modifying the extlinux.conf. There are 2 ways to proceed:
Open a ssh connection to the target or directly with tty terminal, and then use an editor as 'vi' to modify the extlinux.conf file.
- Do not forget to synchronize the file system before rebooting the target:
- sync
This method doesn't need to have a target up and running but only need the "st-image-bootfs-openstlinux-weston-stm32mp1.ext4" file. To modify a 'ext4' file, a loopback mount tool is need which is avaible in any Linux Distribution (even through Windows 10 via WSL2):
- mkdir -p $WORKING/bootfs
- mount -o loop Template:Highlight3 $WORKING/bootfs
- ##Then edit the extlinux.conf file (for WSL2 use a 'Linux' type editor; vi, ...)
- ##Once extlinux.conf up-to-date, umount loopback and flash the bootfs into sdcard with STM32CubeProgrammer or 'dd' :
- umount $WORKING/bootfs
- sync
- dd if=Template:Highlight3 of=Template:Highlight3 conv=fdatasync