This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Supported Flash memory technologies[edit source]
The STM32MP15 boards support different kind of Flash memories:
- SD card on SDMMC interface that is present on EVAL and DISCO boards.
- eMMC on SDMMC interface that is present on EVAL board only.
The next section lists all partitions used on STM32MP15 boards (size, name, content) and the following sections show how they are mapped on the different types of Flash memories.
2. Flash partitions[edit source]
The table below lists the partitions defined for STMP32MP15 boards.
![Flash partitions for Android.png](/stm32mpu-ecosystem-v1/nsfr_img_auth.php/thumb/b/b5/Flash_partitions_for_Android.png/750px-Flash_partitions_for_Android.png)
3. SD card memory mapping[edit source]
The SD card has to be partitioned with GPT format to be recognized by STM32MP15. The easiest way to achieve this is to use STM32CubeProgrammer.
The ROM code search the GPT entries which name begins with "fsbl": fsbl1 and fsbl2 for example.
![SD card mapping for Android.png](/stm32mpu-ecosystem-v1/nsfr_img_auth.php/thumb/0/0e/SD_card_mapping_for_Android.png/750px-SD_card_mapping_for_Android.png)
4. eMMC memory mapping[edit source]
The eMMC embeds four physical partitions:
- Boot area partition 1: used to store the first copy of the FSBL.
- Boot area partition 2: used to store the second copy of the FSBL.
- User data area: formatted with GPT partitioning and used to store all remaining partitions.
- Replay Protected Memory Block (RPMB): not shown in the figure below, since not involved in the current boot chain.
STM32CubeProgrammer has to be used to prepare the eMMC with the layout shown below and to populate each partition.
![EMMC mapping for Android.png](/stm32mpu-ecosystem-v1/nsfr_img_auth.php/thumb/c/c8/EMMC_mapping_for_Android.png/750px-EMMC_mapping_for_Android.png)