This page explains how to change the kernel configuration and device tree. It is intended for Distribution Package users.
1. Prerequisites[edit source]
The environment must be installed using the Distribution Package adapted to your selected microprocessor device. See the list of Android Distribution Package.
You must get kernel sources as explained in How to build kernel for Android.
To be able to execute following instructions you need to work from your distribution root directory and initialise your environment:
source build/envsetup.sh
bspsetup
lunch aosp-<BoardId>-userdebug
2. Updating the kernel configuration[edit source]
By using menuconfig
, you can update the configuration file for your needs. Some guidelines are given below.
2.1. Save the current configuration[edit source]
Before making any changes to the kernel configuration, it is advised to build the kernel with the current configuration:
build_kernel
A default config file named defconfig.default
is generated in out-bsp/<STM32Series>/KERNEL_OBJ/
directory which can the be copied to a safe location.
2.2. Create a new kernel configuration[edit source]
Start menuconfig
:
build_kernel menuconfig
You can load a .config
file and modify any entry using this interface. Please read on the top of the windows the instructions to navigate.
Do not forget to hit save. This will generate a .config
file located in out-bsp/<STM32Series>/KERNEL_OBJ/
.
2.3. Test new kernel configuration[edit source]
To test your configuration you need to rebuild the kernel, then update the prebuilts and flash, like explain in more details in How to build kernel for Android.
2.4. Applying the newly generated kernel configuration[edit source]
To make your change permanent you need to compare the new defconfig.default
file with the one previously stored in a safe location. You can you a graphical tool like meld
.
meld <path-to-safe-location>/defconfig.default out-bsp/<STM32Series>/KERNEL_OBJ/defconfig.default
Then report the changes to the android-soc.config
file located in device/stm/<STM32Series>-kernel/source/kconfig/<kernel version>/
.
And force the regeneration of the .config:
build_kernel defaultconfig
To test your configuration you need to rebuild the kernel, then update the prebuilts and flash, like explain in more details in How to build kernel for Android.
3. Changing the kernel command line[edit source]
You can customize the kernel command line call at boot time.
Arguments are defined in the BoardConfig.mk
file located in device/stm/<STM32Series>/<BoardId>/
.
Change the value of the BOARD_KERNEL_CMDLINE variable to your needs.
To Apply changes, you need to rebuild the bootimage:
make bootimage-nodeps
And then flash the boot partition.
4. Changing the Device Tree[edit source]
The kernel device tree used is set in the dt.mk
file available in the device/stm/<STM32Series>/build/tasks/
directory. For more information please refer to the Device tree and How to create your board device tree pages.
This device trees are located inside the Linux kernel source code previously loaded and can be modified directly in device/stm/<STM32Series>-kernel/linux-<STM32Series>/arch/arm/boot/dts
.
After modification you need to rebuild the device tree by:
build_kernel -i dtb
make -j
And then re-flash the DT partition.
This page is a candidate for renaming (move). The requested new name is: How to customize kernel for Android . The supplied reason is: request to have name coherent together (How to build / How to customize) . -- N. Louboutin. Wiki maintainers: remember to update the pages that link this page before renaming (moving) it. |