How to customize the STM32MPU distribution for Android

Revision as of 13:50, 21 August 2019 by Registered User (→‎Audio configuration)

This articles explain how you can customize the STM32MPU distribution for Android™. It's intent to be used by distribution package users.

1. Prerequisites[edit source]

The environment used must have been installed using the right Distribution Package for your selected microprocessor device. See Distribution_Package.

To be able to execute following instructions you need to work from your distribution root directory and initialise your environment:

 source build/envsetup.sh
 lunch aosp-<BoardId>-userdebug

2. Layout configuration[edit source]

It is possible to configuration the memory layout. The file android_layout.config located device/stm/<STM32Series>/layout contains all the necessary data.

When changes is done you need to reload the environment with:

 source build/envsetup.sh
 lunch aosp-<BoardId>-userdebug

2.1. Memory type[edit source]

To adapt your build to the memory you desire, you must change in the file android_layout.config the parameter PART_MEMORY_TYPE.

For example the possible values can be:

  • sd
  • emmc

2.2. Memory size[edit source]

To adapt your build to the size of your memory you can change in the file android_layout.config the parameter PART_MEMORY_SIZE.

For example the possible values can be:

  • 4GiB
  • 8GiB

This value must match the parameter at the end of the file that looks like PART_<Memory size>_MEMORY_MAX_SIZE

It may be necessary to change the value attach to this parameter. For example:

PART_8GiB_MEMORY_MAX_SIZE 7432M x1 sd

The 7536M must be adapt if your memory is less than its definition.

To find the correct value execute:

 sgdisk -p /dev/mmcblk<x>

It will output something looking like:

Disk /dev/mmcblk0: 15433728 sectors, 7.4 GiB
Logical sector size: 512 bytes
Disk identifier (GUID): XXXXXXXX-XXXX-XXXX-XXXX-XXXXXXXXXXX
Partition table holds up to 128 entries
First usable sector is 34, last usable sector is 15433694
Partitions will be aligned on 2-sector boundaries
Total free space is 0 sectors (0 bytes)

First line show the microSD card available size: here 15433728 sectors.

To calculate the size in MiB:

size = (NbSectors * SectorSize) / 1024 / 1024
In this example: (15433728 * 512) / 1024 / 1024 = 7536 MiB

Report this value for the parameter PART_8GiB_MEMORY_MAX_SIZE

PART_8GiB_MEMORY_MAX_SIZE 7536M x1 sd

You can refer to the README file in the same folder for more details.

2.3. Partition size[edit source]

If you decide to change the size of some partition you need to change in the file android_layout.config.

You need to adapt all parameter that looks like

PART_<NAME> <PART_SIZE> <PART_NB> <PART_LABEL> <PART_SUFFIX> <PART_ENABLE>
NAME: name of the local variable (last partition MUST start with PART_LAST_)
PART_SIZE: as xxxMB or xxxKB or xxxGB
PART_NB: number of instances of partition (x1 or x2)
PART_LABEL: name of the partition label
PART_SUFFIX (optional): name of the suffix in case PART_NB equal x2 (_a/_b by default)
PART_ENABLE (optional): device for which the partition is only applicable (sd)

When this is done you also need to adapt every FlashLayout_*.tsv under device/stm/<STM32Series>/layout/programmer to match your changes.

For that purpose, you can use the script build_tsv_.py.

3. Bluetooth configuration[edit source]

The configuration is stored in bdroid_buildcfg.h located in device/stm/<STM32Series>/<BoardId>/network/bt.

The Bluetooth is enabled in device/stm/<STM32Series>/<BoardId>/BoardConfig.mk

BOARD_HAVE_BLUETOOTH := true
BOARD_HAVE_BLUETOOTH_LINUX := true

The path of the configuration file overlay bdroid_buildcfg.h must be also added:

BOARD_BLUETOOTH_BDROID_BUILDCFG_INCLUDE_DIR ?= device/stm/<STM32Series>/<BoardId>/network/bt

The Android Bluetooth stack (located in system/bt) can be configured thanks to the file device/stm/<BoardId>/network/bt/bdroid_buildcfg.h.

It must at least contain the definition of the Class of Device (CoD) (see more information in the Bluetooth Specification[1])

#define BTA_DM_COD {0x5A, 0x01, 0x1C}

Additionally, it can contain the Bluetooth Stack profile configuration. If a variable is not set in this file, the default configuration is selected in the stack.

By default, all the profiles are selected (see system/bt/include/bt_target.h). Example for the PAN profile:

#ifndef BTA_PAN_INCLUDED
#define BTA_PAN_INCLUDED TRUE
#endif

If you want to disable it, add the following line in bdroid_buildcfg.h:

#define BTA_PAN_INCLUDED FALSE

More details in Android Bluetooth[2].

4. Audio configuration[edit source]

The configuration file audio.stm.xml is stored in device/stm/<STM32Series>/<BoardId>/media/audio

For more details please refer to How to change audio device for Android

5. Wi-Fi configuration[edit source]

The configuration is stored in device/stm/<STM32Series>/<BoardId>/network/wifi.

You can change various configuration:

  • p2p
  • wpa supplicant
  • dhcp

For more details please refer to How to change Wi-Fi device for Android

6. Patch Android distribution[edit source]

It may be necessary to patch some files from the Android distribution.

To do so make the changes you need in the Android distribution repository and create a patch file containing your changes.

Then copy this file to device/stm/<STM32Series>/patch/android/<repoName>.

You need to add you file name in the configuration file android_patch.config at the appropriate section.

For example if you need to change a file in the repository framework/base, do your changes, then:

 git commit -m "Some comment"
 git format-patch -1 #Where 1 is the number to commit to include.

The output result of a file name 0001-commitName.

Then copy it to device/stm/<STM32Series>/patch/android/framework_base.

In the configuration file it would result of:

PATCH_PATH frameworks/base
PATCH_X frameworks_base/0001-commitName #Where X is the patch order

To apply this change you need to execute:

 <STM32Series>clear -p
 <STM32Series>setup
 make -j