This article explain how to integrate the custom Android SDK for Android Studio.
1. Prerequisites[edit source]
You must have installed one of the following environment:
Android Studio must be installed.
Informations about Android API Levels are explain in the Android SDK page[1].
For Developer Package directly go to the section #Install SDK in Android Studio and ignore the rest.
2. Build SDK for distribution[edit source]
2.1. Set environment[edit source]
The Android SDK has to be generated in the eng build environment, so you must select the right case using the lunch command.
2.2. SDK for Linux[edit source]
Execute the following build command to generate the SDK
make update-api make sdk
The result is in path out/host/linux-x86/sdk/<BoardId>/android-sdk_eng.<login>_<linux-x86>/platforms/android-<Version>/android.jar
.
2.3. SDK for Windows[edit source]
A specific Ubuntu package needs to be installed for Windows Android SDK building, to add the unix2dos command:
sudo apt-get install tofrodos
Execute the following build command to generate the SDK:
make update-api make win_sdk
The result is in path out/host/windows/sdk/<BoardId>/android-sdk_eng.<login>_<windows>/platforms/android-<Version>/android.jar
.
3. Install SDK in Android Studio[edit source]
The information below applies to both Linux Ubuntu and Windows environments. (It is assumed that Android Studio is already installed.)
- Open Android Studio
- Open the Settings item in the File Menu
- In Appearance & Behavior --> System Settings --> Android SDK
- Check the path of the SDK as highlighted in Red in the picture below.
- Check for the current SDK API selected, as highlighted in Template:DarkBlue in the picture below.
- Copy the
android.jar
file provided with the developper package or the one you generate with the distribution to the Android Studio SDK path :<YourAndroidStudio_SDKPath>/platforms/android-<APILevel>/
- Restart Android Studio
- To check for new API availability in Android Studio, you can search for new Class/Symbol through the Navigate menu.