Template:ArticleMainWriter Template:ReviewersList
Template:ArticleProposedVersion
This article aims to describe the content of the release STM32MP15-Ecosystem-v1.0.0 for STM32MPU Embedded Software distribution and its associated ecosystem.
1. Delivery purpose and scope[edit source]
The purpose of this delivery is the first Mass Market release, aka STM32MP1-V1.0.0, provided to STMicroelectronics customers.
The scope of this ecosystem delivery, dedicated to STM32MP15 devices, is:
- The STM32MPU Embedded Software distribution:
- The OpenSTLinux distribution running on the Arm® Cortex®-A7 processor(s)
- The STM32Cube MPU Package running on the Arm® Cortex®-M4 processor
- The associated tools: : Referenced tools
- STM32-CoPro-MPU Eclipse plugin
- STM32CubeMX
- STM32CubeProgrammer
- Keygen
- Signing tool
- The documentation:
- This user guide (wiki format)
- Documentation package : Reference_documents
- The supported boards: Boards
- STM32MP15 Evaluation board
- STM32MP15 Discovery kit
Aim of this release:
- To provide a full ecosystem for STM32MP15x devices.
- To work efficiently with STM32MP15 boards, using one of the Packages developed by STMicroelectronics for STM32 MPU devices (Starter Package, Developer Package, Distribution Package). See Which Package better suits your needs for more information on these Packages.
2. Intended audience[edit source]
The targeted audience consists in STMicroelectronics customers.
3. Licensing[edit source]
This software package is licensed under LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION, the "LLA". Customer may not use this package except in compliance with the Limited License Agreement.
4. Main features / main highlights[edit source]
4.1. Boards[edit source]
Boards | PCBs list | Content | Availability | Distribution Package | Starter Package | Developper Package |
---|---|---|---|---|---|---|
EVAL Rev.C | MB1263C (Daughter) + MB1262C (Mother) + MB1230C (Display) + MB1379A (Camera) |
STM32MP1 STM32MP157AAA3 Rev.B PMIC STPMIC1APQR cut1.2 external oscillator |
Jan'19 | Machine stm32mp1-boards-revc for all flashs Machine stm32mp1-eval-revc for SDCard |
EVAL Rev.C Starter Package | EVAL Rev.C Developer Package |
DISCO Rev.C | MB1272C (Mother) + MB1407B (Display) |
STM32MP1 STM32MP157CAC3 Rev.B PMIC STPMIC1APQR cut1.2 external oscillator |
Jan'19 | Machine stm32mp1-boards-revc for all flashs Machine stm32mp1-disco-revc for SDCard |
DISCO Rev.C Starter Package | DISCO Rev.C Developer Package |
- Warning STLINK in EVAL and DISCO Rev.C boards integrates the latest firmware STLINK (V2J32M22) which requires upgraded USB PC drivers - new Windows USB driver
4.2. Embedded software[edit source]
4.2.1. Cortex-A7 Linux software[edit source]
- STM32MP15 microprocessor support with following components:
- Kernel version LTS v4.19.9
- TF-A version v2.0
- U-Boot version v2018.11
- OP-TEE version v3.3.0
- openOCD version v0.10.0
- Build process
- OpenEmbedded Thud (v2.6)
- GCC version v8.2
- Applicative components
- Weston version v5.0.0
- GStreamer version v1.14.2
- GCnano version v6.2.4
4.2.2. Boot configurations[edit source]
- At boot, you can select two kernel configurations:
- Configuration 1: All internal peripherals assigned to Cortex-A7 for Linux drivers, Cortex-M4 co-processing firmware TTY executed by default
- Configuration 2: Some internal peripherals assigned to Cortex-M4 to execute Cortex-M4 delivered examples on the board (EVAL or DISCO) see (How to run Cortex-M4 examples).
- Configuration 1 activated by default if you do not specify 2 in the console at boot.
4.2.3. Cortex-M4 Cube firmware[edit source]
- STM32MP15 microprocessor support with STM32CubeMP1 FW v1.0.0 package
- All HAL drivers for internal peripherals assignable to Cortex-M4 context released
- BSP EVAL and DISCO boards released
- Middlewares (OpenAMP, Resource Manager, FreeROTS) for Cortex-M4 context released
- Examples HAL with EVAL / DISCO boards with device tree per boards applied by U-Boot released
- Co-processing examples on EVAL / DISCO boards based on UART virtual channel released
- Product and Engineering modes detected automatically by boot pins configuration (same M4 firmware binary)
- Cortex-M4 Early boot released (start M4 firmware from u-boot, same M4 firmware binary than M4 firmware start from kernel)
- By default, the firmware Linux is booting with a Cortex-M4 TTY firmware example
- To enable Cortex-M4 Cube examples in EVAL or DISCO board, a specific device tree configuration must be enabled through U-Boot.
4.3. STM32CubeProgrammer, Signing tool, Key gen[edit source]
- Flashload SDCard, eMMC, NAND, NOR images through USB and UART for EV1, DK1, DK2 boards
- Private and public keys generation
- Images signature with hash public key
- Flashlayout file format change
- STM32MP1 fuses management (with console interface only)
- PMIC NVM management (with console interface only)
4.4. STM32CubeMX[edit source]
- Support STMP32MP1 series : STM32MP151xx, STM32MP153xx and STM32MP157xx
- Support STM32MP157 boards : STM32MP157A-EV1, STM32MP157C-EV1, STM32MP157C-DK2
- Support PCC feature for the STM32MP1 series, and Tj versus Ta calculation
- Support DDR Test suite Tool for the STM32MP1 series
4.5. SW4STM32 IDE[edit source]
STM32-CoPro-MPU plug-in integrated in SW4STM32 IDE covers the Arm Cortex-M4 development and debug with:
- SW4STM32 plug-in to support Cortex-M4 STM32CubeMP1 in Production mode and Engineering mode
- Cortex-M4 Firmware compilation, Load, Debug
- PC Linux with Ethernet (recommended) or serial link
- PC Windows with Ethernet or Ethernet over USB link
- Cortex-M4 Firmware installation directory configurable
This plug-in is delivered with SW4STM32 from version 2.8.0
Info: To use delivered Cortex-M4 examples per ST board, the user needs to enable Cortex-M4 examples device tree configuration using U-Boot
4.6. User guide[edit source]
This user guide version comprises about 450 articles:
- The "Release notes" category includes the release notes for the STM32MP1-V1.0.0 release
- The "Getting started with STM32MP1 boards" category describes the STM32MP157C-EV1 Evaluation board and STM32MP157X_DKX Discovery kit, with their associated software Packages (Starter, Developer, and Distribution)
- The "Hardware components" category describes some components available on the STM23MP15 boards
- The "STM32 MPU microprocessor devices" category describes more STM32MP15 internal peripherals with the way to configure them (Arm® Cortex® assignment and device tree)
- The "Embedded software components" category introduces more Linux® frameworks. This user guide version adds lot of articles about the Linux frameworks, including articles about the coprocessing management
- The "Tools" category has been restructured
- The "Trace and debug tools" category provides much more articles to help tracing, monitoring and debugging applications
- The "How To" category has been restructured into
- "How To - Android" focuses on Android tips (nothing new compared to previous user guide version)
- "How to build software" deals with the build operations
- "How to customize software" helps configuring your software
- "How to run use cases" proposes many use cases to go through the STM32MP15 features
- "How to trace and debug" gives tips and recommendations for tracing, monitoring and debugging
4.7. Miscellaneous[edit source]
- Detailed features are available in the release notes of the different items constituting this delivery.
- See sections STM32MPU Embedded Software distribution detailed release notes , Referenced tools release notes and Reference documents
5. Recommendations of use[edit source]
5.1. Safe[edit source]
- Develop board based on STM32MP1
- Flashload and boot from all flashes SDCard, eMMC, NAND ONFI, NOR
- Application can activate Low power modes (STOP and STANBY)
- Develop Linux application, libraries, kernel modules based on OpenSTLinux delivery
- Develop Cube application with co-processing link based on Cube delivery
- Prototype some applications based on ST boards
- Stress available features
5.2. Not recommended[edit source]
6. Main restriction list[edit source]
6.1. Boards[edit source]
- None
6.2. Embedded software[edit source]
- As mentionned on Boot chains overview article, the Basic boot chain has a limited features set versus Trusted boot chain (which is the default solution delivered by STMicroelectronics). See details in STM32MP15_OpenSTLinux_release_note_-_v1.0.0#Main_restrictions_list
- Some IPs modes not supported on Embedded SW. See details in STM32MP15_OpenSTLinux_release_note_-_v1.0.0#Main_restrictions_list
- Some modes proposed in CubeMX for Cortex-A7 non secure context not supported in Cortex-A7 secure context. See details in STM32MP15_OpenSTLinux_release_note_-_v1.0.0#Main_restrictions_list
6.3. STM32CubeProgrammer, signing tool, key generator[edit source]
- None
6.4. STM32CubeMX[edit source]
6.4.1. Restrictions[edit source]
6.5. SW4STM32 IDE[edit source]
- None
6.6. Miscelleanous[edit source]
- Exhaustive restriction lists are available in the release notes of each delivery.
- See sections STM32MPU Embedded Software distribution detailed release notes and Referenced tools release notes .
7. Reference documents[edit source]
All the resources for the STM32MP1 Series are in the Resources area of the STM32MP1 Series web page.
The resources below are referenced in some of the articles in this user guide for the STM32MP1 Series.
Reference | Name | Link | Version |
---|---|---|---|
Application notes | |||
AN5031 | Getting started with STM32MP15 Series hardware development | AN5031.pdf | v1.0 |
AN5109 | STM32MP1 Series using low-power modes | AN5109.pdf | v1.0 |
AN5253 | Migration of microcontroller applications from STM32F4x9 lines to STM32MP15x lines microprocessor | AN5253.pdf | v1.0 |
AN5122 | STM32MP1 Series DDR memory routing guidelines | AN5122.pdf | v1.0 |
AN5168 | STM32MP1 series DDR configuration | AN5168.pdf | v1.0 |
Datasheets[1] | |||
DS12505 | STM32MP157Cxx datasheet (secure) |
DS12505.pdf | v1.0 |
DS12504 | STM32MP157Axx datasheet (basic) |
DS12504.pdf | v1.0 |
DS12503 | STM32MP153Cxx datasheet (secure) |
DS12503.pdf | v1.0 |
DS12502 | STM32MP153Axx datasheet (basic) |
DS12502.pdf | v1.0 |
DS12501 | STM32MP151Cxx datasheet (secure) |
DS12501.pdf | v1.0 |
DS12500 | STM32MP151Axx datasheet (basic) |
DS12500.pdf | v1.0 |
Errata sheets | |||
ES0438 | STM32MP15xx device errata | ES0438.pdf | v1.0 |
Reference manuals[1] | |||
RM0436 | STM32MP157xxx reference manual (STM32MP157xxx advanced Arm®-based 32-bit MPUs) |
RM0436.pdf | v2.0 |
RM0442 | STM32MP153xxx reference manual (STM32MP153xxx advanced Arm®-based 32-bit MPUs) |
RM0442.pdf | v2.0 |
RM0441 | STM32MP151xxx reference manual (STM32MP151xxx advanced Arm®-based 32-bit MPUs) |
RM0441.pdf | v2.0 |
Boards schematics | |||
MB1262 schematics | STM32MP157C-EV1 motherboard schematics (Evaluation board) |
MB1262C-01.pdf | vC-0.1 |
MB1263 schematics | STM32MP157C-EV1 daughterboard schematics (Evaluation board) |
MB1263C-01.pdf | vC-0.1 |
MB1230 schematics | DSI 720p LCD display daughterboard schematics (Evaluation board) |
MB1230B-02.pdf | vB-0.2 |
MB1379 schematics | Camera daughterboard schematics (Evaluation board) |
MB1379A-01.pdf | vA-0.1 |
MB1272 schematics | STM32MP157x-DKx motherboard schematics (Discovery kit) |
MB1272C-01.pdf | vC-0.1 |
MB1407 schematics | STM32MP157x-DKx daughterboard schematics (Discovery kit) |
MB1407C-01.pdf | vB-0.1 |
Boards user manuals | |||
UM2535 | STM32MP157x-EV1 evaluation board user manual | UM2535.pdf | V1.0 |
UM2534 | STM32MP157x-DKx discovery board user manual | UM2534.pdf | V1.0 |
8. How to get the software and start with this release?[edit source]
The list of embedded software packages available for downloaded depends on the Package to be used.
More information can be found on STM32MPU Embedded Software distribution and the supported Packages, at:
The table below provides the available board part numbers and the source of information in order to:
- Get started with one of the three available Packages (Starter, Developer or Distribution Packages)
- Get started with the board
- Find the associated embedded software distributions
- Download source code
- Build an embedded software
Board part number | Jump to |
---|---|
STM32MP157C-EV1 Evaluation board |
STM32MP15 Evaluation boards - getting started, including software download |
STM32MP157X-DKX Discovery kit |
STM32MP15 Discovery kits - getting started, including software download |
9. STM32MPU Embedded Software distribution detailed release notes[edit source]
The table below lists the software packages available in the STM32MPU Embedded Software distribution, and provides the corresponding release notes.
The release notes provide more information and details about the features and content of each package.
The release notes does not explain how to get software. For that, refer chapter How to get the software and start with this release
Firmware | Release note | Version |
![]() |
STM32MP15 OpenSTLinux release note - v1.0.0 | openstlinux-4.19-thud-mp1-19-02-20 |
![]() |
STM32CubeMP1 Package release note - v1.0.0 | STM32CubeMP1-V1.0.0 |
10. Referenced tools release notes[edit source]
The table below lists the available tools, and provides links to the respective release notes.
Each release note provides information on how to install and use the corresponding tool.
The set of tools to be downloaded depends on the Package to be used (double check Which Package better suits your needs article to find more information on each Package).
Tools | Release notes | Host PC | Which Package may need the tool ? | |||
Linux version | Windows version | Starter Package | Developer Package | Distribution Package | ||
STM32CubeProgrammer | STM32CubeProgrammer release note | 2.0.0 | 2.0.0 | ☑ | ☐ | ☑ |
STM32-CoPro-MPU plug-in for SW4STM32 IDE | STM32-CoPro-MPU plugin release note | 1.0.0 | 1.0.0 | ☐ | ☑ | ☐ |
STM32CubeMX | STM32CubeMX release note | 5.1 | 5.1 | ☐ | ☑ | ☑ |
Keygen | KeyGen release note | 1.0.0 | 1.0.0 | ☑ | ☑ | ☑ |
Signing tool | Signing tool release note | 1.0.0 | 1.0.0 | ☑ | ☑ | ☑ |
11. Change log[edit source]
See detailed release notes for more information STM32MPU Embedded Software distribution detailed release notes and Referenced tools release notes .
12. References[edit source]
- ↑ 1.0 1.1 The part numbers are specified in STM32MP15 microprocessor part numbers