This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User mNo edit summary |
||
Line 40: | Line 40: | ||
| Off | | Off | ||
| The execution may have failed during Linux<sup>®</sup> kernel execution between two heartbeat pulses (blue LED): a fatal error leading to a kernel panic might have occurred... | | The execution may have failed during Linux<sup>®</sup> kernel execution between two heartbeat pulses (blue LED): a fatal error leading to a kernel panic might have occurred... | ||
| See [[ | | See [[Linux tracing, monitoring and debugging]] to investigate the failure | ||
|- | |- | ||
| Blinking | | Blinking |
Latest revision as of 09:21, 7 August 2020
1. Introduction[edit source]
The blue and red LEDs on STM32MP15 boards are used to notify the user in case of boot failure during the boot chain execution and at runtime.
2. Description and debug[edit source]
The statuses of blue and red LEDs allow to see at which stage the execution failed: the diagram below shows how each boot component uses these LEDs while the table gives more information on the way to interpret the LED statuses when the boot fails. Among the boot components, the FSBL can be TF-A or U-Boot SPL and the SSBL is U-Boot, as explained in the boot chains overview.
Blue LED | Red LED | System state | Action |
---|---|---|---|
Off | Blinking | The execution failed during ROM code execution | Check that:
|
On | Blinking | The execution failed during the second stage bootloader (SSBL) | See U-Boot - How to debug to investigate the failure |
Off | Off | The execution may have failed:
|
|
Off or on | Off | The execution may have failed during Linux® kernel execution between two heartbeat pulses (blue LED): a fatal error leading to a kernel panic might have occurred... | See Linux tracing, monitoring and debugging to investigate the failure |
Blinking | Off | Your platform is alive | Enjoy ! |