This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User mNo edit summary |
||
Line 7: | Line 7: | ||
* the [[Linux remoteproc framework overview|remoteproc driver]] to reserve the regions in [[RETRAM internal memory|RETRAM]] and [[MCU SRAM internal memory|MCU SRAM]] where the coprocessor firmware will be loaded. | * the [[Linux remoteproc framework overview|remoteproc driver]] to reserve the regions in [[RETRAM internal memory|RETRAM]] and [[MCU SRAM internal memory|MCU SRAM]] where the coprocessor firmware will be loaded. | ||
* the [[Linux_RPMsg_framework_overview|RPMsg driver]] to reserve the region where [[Linux RPMsg framework overview|RPMsg]] buffers used for interprocess communication with the coprocessor, are allocated, typically [[MCU SRAM internal memory|MCU SRAM]]. | * the [[Linux_RPMsg_framework_overview|RPMsg driver]] to reserve the region where [[Linux RPMsg framework overview|RPMsg]] buffers used for interprocess communication with the coprocessor, are allocated, typically [[MCU SRAM internal memory|MCU SRAM]]. | ||
* the | * the Vivante Gcnano driver to reserve the region where the GPU working memory is allocated, typically the [[DDRCTRL and DDRPHYC internal peripherals|DDR]]. | ||
== References == | == References == |
Latest revision as of 11:21, 31 July 2020
1. Article purpose[edit source]
The Reserved-memory mechanism[1] allows reserving memory regions in the kernel. This mechanism is used by drivers to allocate buffers in specific memory regions (such as MCU SRAM) or to get a dedicated memory pool that will not be managed by Linux® conventionnal memory allocator (in DDR).
2. Use cases[edit source]
In STM32 MPU Linux OS, the reserved-memory is used by:
- the dmaengine driver to reserve the region where DMA buffers are allocated, typically MCU SRAM.
- the remoteproc driver to reserve the regions in RETRAM and MCU SRAM where the coprocessor firmware will be loaded.
- the RPMsg driver to reserve the region where RPMsg buffers used for interprocess communication with the coprocessor, are allocated, typically MCU SRAM.
- the Vivante Gcnano driver to reserve the region where the GPU working memory is allocated, typically the DDR.
3. References[edit source]