Registered User No edit summary |
Registered User No edit summary |
||
Line 43: | Line 43: | ||
Please remove the capital letter in the word Weston. The correct command is | Please remove the capital letter in the word Weston. The correct command is | ||
{{Board$}} systemctl restart {{Highlight|'''w'''}}eston | {{Board$}} systemctl restart {{Highlight|'''w'''}}eston | ||
|- | |||
| | |||
{{Board$}} weston-image mypicture.bmp | |||
mypicture.bmp: unrecognized file header 0x42 0x4d 0x1e 0x51 | |||
|| | |||
"weston-image" small application supports only jpeg, png and webp image files. Please convert your ".bmp" image file into one of these supported image file formats. | |||
Note: The official source code of "weston-image" is in the file [https://cgit.freedesktop.org/wayland/weston/tree/clients/image.c image.c] and the related error message is in [https://cgit.freedesktop.org/wayland/weston/tree/shared/image-loader.c image-loader.c]. | |||
</onlyinclude> | </onlyinclude> | ||
|} | |} |
Latest revision as of 12:15, 29 November 2019
Some typical issues related to the Wayland / Weston framework are listed below. Solutions or debugging methods are proposed for these issues.
If your issue is not listed, try also looking in the articles in the Wayland/Weston or troubleshooting grids categories.
Symptom | Resolution |
---|---|
EGL state Error: main: Could not initialize canvasglmark2-es2-wayland [11380.091100] reserved_mem_unmap_user: vm_munmap failed eglCreateWindowSurface failed with error: 0x3003 Error: eglCreateWindowSurface failed with error: 0x3003 Error: CanvasGeneric: Invalid EGL_EXT_buffer_age and EGL_EXT_swap_buffers_with_damage weston-simple-egl: ../git/clients/simple-egl.c:440: create_surface: Assertion `ret == EGL_TRUE' failed. Aborted (core dumped)weston-simple-egl [11380.091100] reserved_mem_unmap_user: vm_munmap failed has EGL_EXT_buffer_age and EGL_EXT_swap_buffers_with_damage Segmentation fault (core dumped)weston-simple-egl has |
Weston is using pixman software composition instead of GPU hardware composition. This may be because you have not accepted the EULA at the beginning of the build...
cat /etc/default/weston
#Autogenerated
OPTARGS=--use-pixman
Please comment the content of the file /etc/default/weston or delete it. |
systemctl stop Weston
Failed to stop Weston.service: Unit Weston.service not loaded.
|
Please remove the capital letter in the word Weston. The correct command is westonsystemctl restart |
weston-image mypicture.bmp
mypicture.bmp: unrecognized file header 0x42 0x4d 0x1e 0x51
|
"weston-image" small application supports only jpeg, png and webp image files. Please convert your ".bmp" image file into one of these supported image file formats. Note: The official source code of "weston-image" is in the file image.c and the related error message is in image-loader.c. |