Registered User mNo edit summary |
Registered User |
||
(5 intermediate revisions by 2 users not shown) | |||
Line 1: | Line 1: | ||
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 17:40, 27 July 2020 (CEST)<br />I accept the MT review because publication is mandatory for this week but as soon as Ludovic is coming back, this article must be updated again}} {{ReviewsComments|-- OlivierG<br />Accept but a warning related to fact that directly using "import from ac6 ... " is also a working solution. To be clarified/enhanced later. | |||
LudovicR: Let's publish it like this and revisit proposal for CubeFW examples usage. }} | |||
==Import an SW4STM32 project with an ioc file== | ==Import an SW4STM32 project with an ioc file== | ||
If the project already contains an ioc file, the easiest way to import the project into a working STM32CubeIDE environment is to copy it and open the copy through STM32CubeMX stand alone, then, in the Project Manager, change the Toolchain / IDE to STM32CubeIDE and regenerate the project. | If the project already contains an ioc file, the easiest way to import the project into a working STM32CubeIDE environment is to copy it and open the copy through STM32CubeMX stand alone, then, in the Project Manager, change the Toolchain / IDE to STM32CubeIDE and regenerate the project. | ||
Line 9: | Line 12: | ||
==Import an SW4STM32 project without an ioc file== | ==Import an SW4STM32 project without an ioc file== | ||
To make sure the project gets a | To make sure the project gets a hierarchical structure, the recommended way to is to go to '''[File]>[New]>[STM32 Project]''' as shown below. | ||
[[File:IDE_Image13.png|700px|thumb|center|Menu option for a new STM32 project - Figure 1]] | [[File:IDE_Image13.png|700px|thumb|center|Menu option for a new STM32 project - Figure 1]] | ||
Latest revision as of 11:36, 27 October 2020
1. Import an SW4STM32 project with an ioc file[edit source]
If the project already contains an ioc file, the easiest way to import the project into a working STM32CubeIDE environment is to copy it and open the copy through STM32CubeMX stand alone, then, in the Project Manager, change the Toolchain / IDE to STM32CubeIDE and regenerate the project.
After the project is regenerated, go to [File]>[Import...] and choose to import it as an Existing projects into Workspace.
Then copy the code inside the different /* USER CODE BEGIN */
blocks that exists in the project into the new STM32CubeIDE environment.
2. Import an SW4STM32 project without an ioc file[edit source]
To make sure the project gets a hierarchical structure, the recommended way to is to go to [File]>[New]>[STM32 Project] as shown below.
Select the device for the project being imported and click on [Next >].
When setting up the project as shown below, make sure the Targeted Project Type is set to Empty and click on [Finish].
After the empty hierarchical project is generated:
- Go to [File]>[Import...].
- Import the SW4STM32 project as Import ac6 System Workbench for STM32 Project
- Copy and paste the project content into the sub-project of the empty project by means of STM32CubeIDE project explorer as shown below
![]() |
It is not recommended to import the .cproject, .project or .settings files. |
It is important to remember to also configure the same build settings that was used previously while the project was in the SW4STM32 environment. If the project contains linked resources those needs to be updates to point to the correct resource in the file system. This process is necessary because when importing a project from SW4STM32 without any special treatment and that does not have an ioc-file then it will be imported into STM32CubeIDE with a flat project structure.