This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(2 intermediate revisions by the same user not shown) | |||
Line 42: | Line 42: | ||
rect 353 216 428 303 [[Power overview]] | rect 353 216 428 303 [[Power overview]] | ||
rect 432 216 507 303 [[Regulator overview]] | rect 432 216 507 303 [[Regulator overview]] | ||
rect 353 307 428 359 [[Power overview]] | rect 353 307 428 359 [[Power overview]] | ||
rect 179 118 253 169 [[Reset overview]] | rect 179 118 253 169 [[Reset overview]] | ||
rect 177 216 253 269 [[Serial TTY overview]] | rect 177 216 253 269 [[Serial TTY overview]] | ||
rect 12 216 88 269 [[SPI overview]] | rect 12 216 88 269 [[SPI overview]] |
Latest revision as of 11:24, 16 October 2020
This section gives an overview of Linux® kernel drivers (UPPERCASE in the figure) implemented for the STM32MP15 support, with their respective software frameworks (lowercase in the figure).
The components are grouped per functional domains.
Each Linux framework is further described in Linux operating system category articles.
Each STM32 MPU peripheral is introduced in peripherals overview articles.
Both those sections are reusing the same functional domain split.
The color code, explained in the legend, allows to see the code origin for each component.

STM32MP15 Linux kernel overview