This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(4 intermediate revisions by the same user not shown) | |||
Line 10: | Line 10: | ||
[[File: OpenSTLinux architecture overview.png|link=OpenSTLinux architecture overview|thumb|Zoom out to OpenSTLinux distribution]] | [[File: OpenSTLinux architecture overview.png|link=OpenSTLinux architecture overview|thumb|Zoom out to OpenSTLinux distribution]] | ||
</noinclude> | </noinclude> | ||
{{ImageMap|Image: STM32MP15 Linux kernel.png {{!}} frame {{!}} center {{!}} STM32MP15 Linux kernel overview | {{ImageMap|Image: STM32MP15 Linux kernel.png {{!}} frame {{!}} center {{!}} STM32MP15 Linux kernel overview | ||
rect 525 26 678 113 [[ALSA overview]] | rect 525 26 678 113 [[ALSA overview]] | ||
rect 12 24 86 75 [[:Category:Arm architecture]] | rect 12 24 86 75 [[:Category:Arm architecture]] | ||
Line 28: | Line 28: | ||
rect 345 24 420 150 [[Dmaengine overview]] | rect 345 24 420 150 [[Dmaengine overview]] | ||
rect 693 190 768 280 [[DRM KMS overview]] | rect 693 190 768 280 [[DRM KMS overview]] | ||
rect 96 215 171 269 [[I2C overview]] | rect 96 215 171 269 [[I2C overview]] | ||
rect 693 306 767 496 [[IIO overview]] | rect 693 306 767 496 [[IIO overview]] | ||
Line 43: | Line 42: | ||
rect 353 216 428 303 [[Power overview]] | rect 353 216 428 303 [[Power overview]] | ||
rect 432 216 507 303 [[Regulator overview]] | rect 432 216 507 303 [[Regulator overview]] | ||
rect 353 307 428 359 [[Power overview]] | rect 353 307 428 359 [[Power overview]] | ||
rect 179 118 253 169 [[Reset overview]] | rect 179 118 253 169 [[Reset overview]] | ||
rect 177 216 253 269 [[Serial TTY overview]] | rect 177 216 253 269 [[Serial TTY overview]] | ||
rect 12 216 88 269 [[SPI overview]] | rect 12 216 88 269 [[SPI overview]] |
Latest revision as of 11:24, 16 October 2020
This section gives an overview of Linux® kernel drivers (UPPERCASE in the figure) implemented for the STM32MP15 support, with their respective software frameworks (lowercase in the figure).
The components are grouped per functional domains.
Each Linux framework is further described in Linux operating system category articles.
Each STM32 MPU peripheral is introduced in peripherals overview articles.
Both those sections are reusing the same functional domain split.
The color code, explained in the legend, allows to see the code origin for each component.


- ALSA overview
- Category:Arm architecture
- Bluetooth overview
- Clock overview
- CEC overview
- Resource manager for coprocessing
- remoteproc framework overview
- Mailbox framework overview
- RPMsg framework overview
- Hardware spinlock overview
- Coprocessor management overview
- Hardware random overview
- Crypto API overview
- OP-TEE overview
- Linux kernel device tree
- Dmaengine overview
- DRM KMS overview
- I2C overview
- IIO overview
- Interrupt overview
- Overview of GPIO pins
- MMC overview
- MTD overview
- NVMEM overview
- CAN overview
- Ethernet overview
- WLAN overview
- Power overview
- Regulator overview
- Reset overview
- Serial TTY overview
- SPI overview
- PWM overview
- USB overview
- V4L2 camera overview
- Watchdog overview
STM32MP15 Linux kernel overview