Registered User |
Registered User |
||
(30 intermediate revisions by 5 users not shown) | |||
Line 1: | Line 1: | ||
This article gives a short introduction to the official STM32CubeProgrammer tool: What are the flashing principles? Where to download the software? How to install it? How to use it? | This article gives a short introduction to the official STM32CubeProgrammer tool: What are the flashing principles? Where to download the software? How to install it? How to use it? | ||
Line 78: | Line 71: | ||
More examples as well as information on the description format are available in [[STM32CubeProgrammer flashlayout]]. | More examples as well as information on the description format are available in [[STM32CubeProgrammer flashlayout]]. | ||
See [[STM32MP15 resources#AN5275|AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders]] for protocol details. | |||
==How to flash with STM32CubeProgrammer== | ==How to flash with STM32CubeProgrammer== | ||
Line 95: | Line 90: | ||
{{PC$}} STM32_Programmer_CLI -c port=<DEVICE_PORT_LOCATION> -w [<file.tsv>] | {{PC$}} STM32_Programmer_CLI -c port=<DEVICE_PORT_LOCATION> -w [<file.tsv>] | ||
where | where | ||
w: | w: | ||
Write | Write | ||
Line 213: | Line 206: | ||
For partial Flash memory update, the flashlayout.tsv must be edited to select only the partition that needs to be updated (first column =1).<br> | For partial Flash memory update, the flashlayout.tsv must be edited to select only the partition that needs to be updated (first column =1).<br> | ||
See [[STM32CubeProgrammer_flashlayout# | See [[STM32CubeProgrammer_flashlayout#Updating partitions]] for details and example, the rest of the procedure is the same. | ||
On ST boards, if FSBL or SSBL partitions need to be updated, the Bin2boot fields must be configured with '''ST binaries''', as described in [[STM32CubeProgrammer_flashlayout# | On ST boards, if FSBL or SSBL partitions need to be updated, the Bin2boot fields must be configured with '''ST binaries''', as described in [[STM32CubeProgrammer_flashlayout#Updating partitions using official ST bootloaders]]. | ||
===How to populate a microSD card inserted in a '''Linux host PC'''=== | ===How to populate a microSD card inserted in a '''Linux host PC'''=== | ||
STMicroelectronics distribution is delivered with the ''[[How to populate the SD card with dd command| create_sdcard_from_flashlayout.sh]] '' script that allows to prepare and flash a microSD card image. | STMicroelectronics distribution is delivered with the ''[[How to populate the SD card with dd command| create_sdcard_from_flashlayout.sh]] '' script that allows to prepare and flash a microSD card image. | ||
===How to fuse STM32MP15x OTP === | |||
==== Connection ==== | |||
STM32CubeProgrammer requires to be connected to U-Boot in order to access [[STM32CubeProgrammer_OTP_management|OTP alternate]]. | |||
To do it, you have to initiate a flash process but selecting only the 2 first "boot" partitions TF-A( 0x1) and U-Boot( 0x03) of a .tsv. | |||
Using STM32CubeProgrammer GUI this can done without editing by using any available .tsv but selecting only the 2 first partitions thanks to "Select" column tick boxes on the left, as follow: | |||
[[File: Tsv to access OTP and NVM partition.png|800px|center|link]] | |||
Perform the "Download" till success popup then disconnect from the GUI and switch to CLI in a terminal without rebooting the board: | |||
{{PC$}} STM32_Programmer_CLI -c port=usb1 | |||
==== Display status ==== | |||
It will also displayed the status for each OTP words (Shadow lock read/write, program stick lock, permanent write lock): | |||
*All lower OTP | |||
*Only upper that are available for non secure (defined in TF-A [[BSEC_device_tree_configuration|device tree]]). | |||
To display the OTP: | |||
{{PC$}} STM32_Programmer_CLI -c port=usb1 {{HighlightParam|-otp}} {{HighlightParam|displ}} | |||
------------------------------------------------------------------- | |||
STM32CubeProgrammer v2.3.0 | |||
------------------------------------------------------------------- | |||
USB speed : High Speed (480MBit/s) | |||
Manuf. ID : STMicroelectronics | |||
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000 | |||
SN : 002500253338510534383330 | |||
FW version : 0x0110 | |||
Device ID : 0x0500 | |||
Device name : STM32MPxxx | |||
Device type : MPU | |||
Device CPU : Cortex-A7 | |||
UPLOADING OTP STRUCTURE ... | |||
Partition : 242 | |||
Size : 1024 Bytes | |||
Uploading OTP data: | |||
[==================================================] 100% | |||
OTP Partition read successfully | |||
OTP STRUCTURE VERSION :0x00000001 | |||
BSEC CONTROL REGISTERS: | |||
BSEC_OTP_CONFIG :0x0000000e | |||
|_[08] TR[1] : 0 | |||
|_[07] TR[0] : 0 | |||
|_[06] PRGWIDTH[3] : 0 | |||
|_[05] PRGWIDTH[2] : 0 | |||
|_[04] PRGWIDTH[1] : 0 | |||
|_[03] PRGWIDTH[0] : 1 | |||
|_[02] FRC[1] : 1 | |||
|_[01] FRC[0] : 1 | |||
|_[00] PWRUP : 0 | |||
BSEC_OTP_Status :0x00000041 | |||
|_[07] BIST2LOCK : 0 | |||
|_[06] BIST1LOCK : 1 | |||
|_[05] PWRON : 0 | |||
|_[04] PROGFAIL : 0 | |||
|_[03] BUSY : 0 | |||
|_[02] INVALID : 0 | |||
|_[01] FULLDBG : 0 | |||
|_[00] SECURE : 1 | |||
BSEC_OTP_LOCK :0x00000002 | |||
|_[04] GPLOCK : 0 | |||
|_[03] FENREG : 0 | |||
|_[02] DENREG : 0 | |||
|_[00] OTP : 0 | |||
BSEC_DENABLE :0x0000047f | |||
|_[10] DBGSWENABLE : 1 | |||
|_[09] CFGSDISABLE : 0 | |||
|_[08] CP15SDISABLE[1] : 0 | |||
|_[07] CP15SDISABLE[0] : 0 | |||
|_[06] SPNIDEN : 1 | |||
|_[05] SPIDEN : 1 | |||
|_[04] HDPEN : 1 | |||
|_[03] DEVICEEN : 1 | |||
|_[02] NIDEN : 1 | |||
|_[01] DBGEN : 1 | |||
|_[00] DFTEN : 1 | |||
BSEC_FENABLE :0x00000000 | |||
|_[03] CAN_disable : 0 | |||
|_[02] GPU_disable : 0 | |||
|_[01] Dual_A7_disable : 0 | |||
|_[00] Crypto_disable : 0 | |||
OTP LOWER SHADOW REGISTERS: | |||
ID value disturbed error R_SLock W_SLock Prog_SL Perm_L | |||
00 0x00000017 0 0 1 1 0 0 | |||
01 0x00008000 0 0 0 1 0 1 | |||
02 0x00000000 0 0 0 1 1 0 | |||
03 0x00000000 0 0 0 0 0 0 | |||
04 0x00000000 0 0 0 0 0 0 | |||
05 0x00000000 0 0 0 0 0 0 | |||
06 0x00000000 0 0 0 0 0 0 | |||
07 0x00000000 0 0 0 0 0 0 | |||
08 0x00000000 0 0 0 1 0 0 | |||
09 0x00000000 0 0 0 0 0 0 | |||
10 0x00000000 0 0 0 0 0 0 | |||
11 0x00000000 0 0 0 0 0 0 | |||
12 0x7ce7f0ee 0 0 0 0 0 1 | |||
13 0x00250025 0 0 0 0 0 1 | |||
14 0x33385105 0 0 0 0 0 1 | |||
15 0x34383330 0 0 0 0 0 1 | |||
16 0x125575aa 0 0 0 1 1 1 | |||
17 0x1f41185b 0 0 0 0 0 1 | |||
18 0x7a200140 0 0 1 1 0 0 | |||
19 0x0690147c 0 0 0 0 0 1 | |||
20 0x5de00048 0 0 0 0 0 1 | |||
21 0x00000000 0 0 0 0 0 1 | |||
22 0x00000000 0 0 0 0 0 1 | |||
23 0x3fec2fd7 0 0 0 0 0 1 | |||
24 0x00000000 0 0 0 1 0 0 | |||
25 0x00000000 0 0 0 1 0 0 | |||
26 0x00000000 0 0 0 1 0 0 | |||
27 0x00000000 0 0 0 1 0 0 | |||
28 0x00000000 0 0 0 1 0 0 | |||
29 0x00000000 0 0 0 1 0 0 | |||
30 0x00000000 0 0 0 1 0 0 | |||
31 0x00000000 0 0 0 1 0 0 | |||
OTP UPPER SHADOW REGISTERS: | |||
ID value disturbed error R_SLock W_SLock Prog_SL Perm_L | |||
32 0x00000000 0 0 1 1 1 1 | |||
33 0x00000000 0 0 1 1 1 1 | |||
34 0x00000000 0 0 1 1 1 1 | |||
35 0x00000000 0 0 1 1 1 1 | |||
36 0x00000000 0 0 1 1 1 1 | |||
37 0x00000000 0 0 1 1 1 1 | |||
38 0x00000000 0 0 1 1 1 1 | |||
39 0x00000000 0 0 1 1 1 1 | |||
40 0x00000000 0 0 0 1 1 1 | |||
41 0x00000000 0 0 0 1 1 1 | |||
42 0x00000000 0 0 0 1 1 1 | |||
43 0x00000000 0 0 0 1 1 1 | |||
44 0x00000000 0 0 0 1 1 1 | |||
45 0x00000000 0 0 0 1 1 1 | |||
46 0x00000000 0 0 0 1 1 1 | |||
47 0x00000000 0 0 0 1 1 1 | |||
48 0x00000000 0 0 0 1 1 1 | |||
49 0x00000000 0 0 0 1 1 1 | |||
50 0x00000000 0 0 0 1 1 1 | |||
51 0x00000000 0 0 0 1 1 1 | |||
52 0x00000000 0 0 0 1 1 1 | |||
53 0x00000000 0 0 0 1 1 1 | |||
54 0x00000000 0 0 0 1 1 1 | |||
55 0x00000000 0 0 0 1 1 1 | |||
56 0x00000000 0 0 1 1 0 0 | |||
57 0x42e18000 0 0 0 0 0 0 | |||
58 0x0000fd51 0 0 0 0 0 0 | |||
59 0x12722301 0 0 0 0 0 0 | |||
60 0x00000000 0 0 0 0 0 0 | |||
61 0x00000000 0 0 0 0 0 0 | |||
62 0x00000000 0 0 0 0 0 0 | |||
63 0x00000000 0 0 0 0 0 0 | |||
64 0x00000000 0 0 0 0 0 0 | |||
65 0x00000000 0 0 0 0 0 0 | |||
66 0x00000000 0 0 0 0 0 0 | |||
67 0x00000000 0 0 0 0 0 0 | |||
68 0x00000000 0 0 0 0 0 0 | |||
69 0x00000000 0 0 0 0 0 0 | |||
70 0x00000000 0 0 0 0 0 0 | |||
71 0x00000000 0 0 0 0 0 0 | |||
72 0x00000000 0 0 0 0 0 0 | |||
73 0x00000000 0 0 0 0 0 0 | |||
74 0x00000000 0 0 0 0 0 0 | |||
75 0x00000000 0 0 0 0 0 0 | |||
76 0x00000000 0 0 0 0 0 0 | |||
77 0x00000000 0 0 0 0 0 0 | |||
78 0x00000000 0 0 0 0 0 0 | |||
79 0x00000000 0 0 0 0 0 0 | |||
80 0x00000000 0 0 0 0 0 0 | |||
81 0x00000000 0 0 0 0 0 0 | |||
82 0x00000000 0 0 0 0 0 0 | |||
83 0x00000000 0 0 0 0 0 0 | |||
84 0x00000000 0 0 0 0 0 0 | |||
85 0x00000000 0 0 0 0 0 0 | |||
86 0x00000000 0 0 0 0 0 0 | |||
87 0x00000000 0 0 0 0 0 0 | |||
88 0x00000000 0 0 0 0 0 0 | |||
89 0x00000000 0 0 0 0 0 0 | |||
90 0x00000000 0 0 0 0 0 0 | |||
91 0x00000000 0 0 0 0 0 0 | |||
92 0x00000000 0 0 0 0 0 0 | |||
93 0x00000000 0 0 0 0 0 0 | |||
94 0x00000000 0 0 0 0 0 0 | |||
95 0x00000000 0 0 0 0 0 0 | |||
BSEC_HWCFGR :0x00000014 | |||
|_[07] ECC_USE[3] : 0 | |||
|_[06] ECC_USE[2] : 0 | |||
|_[05] ECC_USE[1] : 0 | |||
|_[04] ECC_USE[0] : 1 | |||
|_[03] SAFMEM_SIZE[3] : 0 | |||
|_[02] SAFMEM_SIZE[2] : 1 | |||
|_[01] SAFMEM_SIZE[1] : 0 | |||
|_[00] SAFMEM_SIZE[0] : 0 | |||
BSEC IP REV :1.1 | |||
BSEC IP ID :0x00100032 | |||
BSEC IP MAGIC ID :0xa3c5dd04 | |||
==== Update value ==== | |||
It is now possible to use programmer to manage new fuses values: | |||
bit to bit for Lower, only programmable once for Upper. | |||
For example: Set the value {{HighlightParam|0x21458000}} into the word {{HighlightParam|57 (0x39)}} | |||
{{PC$}} STM32_Programmer_CLI -c port=usb1 {{HighlightParam|-otp}} {{HighlightParam|program}} {{Highlight|wordID}}={{HighlightParam|0x39}} {{Highlight|value}}={{HighlightParam|0x21458000}} | |||
Words are written as a 32bit word. It is important to take care of the bit order once using the value in software. | |||
Example: Mac address 00:80:e1:42:45:e5 must be written as: | |||
*Word 57 : 0x42e18000 | |||
*Word 58 : 0x0000e545 | |||
{{Warning| MAC address / board Id OTP write should not be performed on ST boards ! They are written and protected by ECC during factory production. Any further write will break the board with no way to recover if these OTP are not locked}} | |||
==== Update lock ==== | |||
Lock (no other programmation could occured) could be added per word; the permanent lock access will only be refreshed after boot. | |||
For example: permanent lock ({{HighlightParam|pl}}={{HighlightParam|1}}) the word {{HighlightParam|57 (0x39)}} | |||
{{PC$}} STM32_Programmer_CLI -c port=usb1 {{HighlightParam|-otp}} {{HighlightParam|program}} {{HighlightParam|wordID}}={{HighlightParam|0x39}} value=0x21458000 {{Highlight|pl}}={{HighlightParam|1}} | |||
===How to program STPMIC NVM === | |||
STM32CubeProgrammer require to be connected to U-Boot in order to access [[STM32CubeProgrammer_STPMIC1_NVM_management|STPMIC NVM alternate]] (0xF4). | |||
Refer to previous Chapter 5.8.1 and follow same procedure to flash only the 2 first "boot" partition with GUI. | |||
Then disconnect from GUI and switch to CLI in a terminal. | |||
This is procedure to modify NVM values. | |||
*Read partition of pmic and load it into a .bin file | |||
{{PC$}} STM32_Programmer_CLI -c port=usb1 {{HighlightParam|-rp 0xf4 0x0 0x8 $MySelectedPATH\PMIC_NVM_read.bin}} | |||
*Backup it by creating a copy PMIC_NVM_write.bin | |||
*Use a binary editor in HEX format ( eg "vi -b file.bin" then :%!xxd ) to edit the copy PMIC_NVM_write.bin with new values.<br/> | |||
The binary format display the shadow register from 0xF8 to 0XFF. Refer to STPMIC1 DataSheet [[STM32MP15 resources#DS12792|DS12792]]. | |||
00000000: EE92 C002 F280 0233 .......3 | |||
respectively SHR address : F8F9 FAFB FCFD FEFF | |||
*Program back the STPMIC1 with modified NVM using following command: | |||
{{PC$}} STM32_Programmer_CLI -c port=usb1 {{HighlightParam|-pmic "PMIC_NVM_write.bin"}} | |||
<noinclude> | |||
{{PublicationRequestId | 9988 | 2018-12-10 | AnneJ}} | |||
[[Category:STM32CubeProgrammer|0]] | |||
</noinclude> |
Latest revision as of 15:57, 3 March 2020
This article gives a short introduction to the official STM32CubeProgrammer tool: What are the flashing principles? Where to download the software? How to install it? How to use it?

1. STM32CubeProgrammer overview[edit source]
STM32CubeProgrammer is the official STMicroelectronics tool for creating partitions into any Flash device available on STM32 platforms.
Once created, STM32CubeProgrammer allows populating and updating the partitions with the prebuilt binaries.
The connection between the host PC and the board can be done through UART or USB serial links.
Any Flash device supported on STM32MPU boards can be flashed using STM32CubeProgrammer. For example, for the STM32MP157 Evaluation board:
- microSDTM card
- eMMC
- NAND Flash memory
- NOR Flash memory
More details on supported Flash memory technologies and mapping can be found in Flash mapping articles, e.g. STM32MP15 Flash mapping.
2. STM32CubeProgrammer installation[edit source]
2.1. Installing the STM32CubeProgrammer tool[edit source]
STM32CubeProgrammer for Linux® host PC | STM32CubeProgrammer for Windows® host PC | |
---|---|---|
Download |
Version 2.4.0
| |
Installation |
./SetupSTM32CubeProgrammer-2.4.0.linux
export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
|
|
User manual |
| |
Detailed release note |
|
2.2. Preparing the USB serial link for flashing[edit source]
It is recommended to use the USB (in DFU mode) for flashing rather than the UART, which is too slow.
Below indications on how to install the USB in DFU mode under Linux and Windows OS, respectively.
- For Linux host PC or Windows host PC with VMWare:
The libusb1.0 package (including USB DFU mode) must be installed to be able to connect to the board via the USB port. This is achieved by typing the following command from the host PC terminal:
sudo apt-get install libusb-1.0-0
To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
cd <your STM32CubeProgrammer install directory>/Drivers/rules
sudo cp *.* /etc/udev/rules.d/
- For Windows host PC:
Run the “STM32 Bootloader.bat” file to install the STM32CubeProgrammer DFU driver and activate the STM32 microprocessor device in USB DFU mode. This driver (installed by STM32 Bootloader.bat) is provided within the STM32CubeProgrammer release package. It is located in the DFU driver folder, \Drivers\DFU_Driver.
In case of issue, refer to How to proceed when the DFU driver installation fails on Windows host PC.
To validate the installation, the DFU driver functionality can be verified by following the FAQ instructions provided in how to check if the DFU driver is functional.
STM32CubeProgrammer is now ready to use: to know more about this tool, please continue reading; otherwise, jump to the Starter or Distribution Package article corresponding to your board: Category:Starter Package or Category:Distribution Package.
3. Flash programming principles[edit source]
Flash programming consists in transferring the binaries stored on the host computer into the platform Flash memory(ies), via a serial interface.
This operation requires a communication interface between the STM32CubeProgrammer and an embedded programming service.
The selection of the binaries to download and the Flash memory destination is done through the flashlayout.tsv file.
The STM32Cubeprogrammer tool uses the Flashlayout.tsv file as an input.
The Flashlayout includes a formal description of the partitions (ID, naming, type, offset) as well as the identification of the Flash memory to be populated.
Some default "tsv" files aligned with the STM32 Flash memory mapping (e.g.STM32MP15_Flash_mapping) are provided in the STM32Cubeprogrammer tool. They can be used as a starting point and can be further adapted to specific application needs.
More examples as well as information on the description format are available in STM32CubeProgrammer flashlayout.
See AN5275: USB DFU/USART protocols used in STM32MP1 Series bootloaders for protocol details.
4. How to flash with STM32CubeProgrammer[edit source]
Once the STM32CubeProgrammer has been installed, complete flashing procedures for STM32 boards are available in Starter Package and Distribution Package articles. Select the article corresponding to your STMicroelectronics platform.
The generic syntax of the STM32CubeProgrammer command is explained below.
- With Linux host PC, the main command is:
./bin/STM32_Programmer_CLI + options given below
- With Windows host PC, the main command is:
./bin/STM32_Programmer_CLI.exe + options given below
The Linux related information provided below can be extrapolated for other host PC operating systems:
- Complete flashing command (for Linux host PC):
How to find the DEVICE_PORT_LOCATION parameter value for the USB link.STM32_Programmer_CLI -c port=<DEVICE_PORT_LOCATION> -w [<file.tsv>] where w: Write <file.tsv>:PathToFlashlayout/flashlayout.tsv file (see above) if Flashlayout and binaries are not in the same directory, then the path to the Flashlayout files must be precised. <DEVICE_PORT_LOCATION>: e.g. usb1 (case sensitive): for other options, please refer to
Populating all partitions can take a few minutes (depending mainly on the rootfs size).
5. FAQs[edit source]
5.1. Where to find the STM32CubeProgrammer user manual[edit source]
The user manual is available in ST deliveries under <STM32CubeProgrammer installation directory>/doc/UM2336.pdf (see Installing the STM32CubeProgrammer tool).
5.2. How to check if the DFU driver is functional[edit source]
Prerequisites: STM32CubeProgrammer installation completed and STM32 board connected to the host PC.
Execute the following command and check the result:
STM32_Programmer_CLI -l usb
- If the DFU is functional, the result is similar to the following
DFU mode: 1 Device Index : USB1 USB Bus Number : 002 USB Address Number : 008 Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000 Serial number : 0000000000 Firmware version : 0x0110 Device ID : 0x0500------------------------------------------------------------------- STM32CubeProgrammer <tool version> ------------------------------------------------------------------- Total number of available STM32 device in
- Otherwise, the DFU is not functional and the result is the following:
DFU mode connected------------------------------------------------------------------ STM32CubeProgrammer <tool version> ------------------------------------------------------------------ Warning: No STM32 device in
5.3. How to proceed when the DFU driver installation fails on Windows host PC[edit source]
Prerequisites: STM32CubeProgrammer installation completed.
The STM32 Bootloader.bat allows to install the DFU driver on a Windows PC (see Preparing the USB serial link for flashing).
In case of failure, here is a typical error log:
MPU\stm32_programmer_package_v1.0.3_MPU\Drivers\DFU_Driver>"STM32 Bootloader.bat" c:\demo\MPU\stm32_programmer_package_v1.0.3_MPU\Drivers\DFU_Driver>echo off Microsoft PnP Utility Processing inf : DFU_in_HS_Mode.inf Failed to install the driver on any of the devices on the system : No more data is available. Total attempted: 1 Number successfully imported: 0c:\demo\
This error occurs either because the STM32CubeProgrammer DFU driver is already installed or because the DFUSE driver is installed.
To verify if the STM32CubeProgrammer DFU driver is correctly installed on your Windows host PC, please proceed as follow:
- Connect the board to the Windows host PC.
- Launch the Device Manager utility and execute the below action depending on your use case:
- The STM32CubeProgrammer DFU driver is not installed:
- Execute the STM32 Bootloader.bat script to install it (see Preparing the USB serial link for flashing).
- The DfuSe driver is installed and you must uninstall it.
- Right click STM Device in DFU Mode and select Uninstall.
- The STM32CubeProgrammer DFU driver is installed and ready to be used.
5.4. How to find the DEVICE_PORT_LOCATION parameter value for the USB link[edit source]
Prerequisites: STM32CubeProgrammer installation completed and STM32 board connected to the host PC.
To find the value of the DEVICE_PORT_LOCATION corresponding to the USB link, use the following command:
DFU mode: 1 Device Index : USB1 USB Bus Number : 002 USB Address Number : 008 Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000 Serial number : 0000000000 Firmware version : 0x0110 Device ID : 0x0500STM32_Programmer_CLI -l usb ------------------------------------------------------------------- STM32CubeProgrammer <tool version> ------------------------------------------------------------------- Total number of available STM32 device in
You can then report the value returned by the command line as explained in the How to flash with STM32CubeProgrammer chapter. Pay attention that the value must be written in lower case.
5.5. How to explore all the partitions of a populated microSD card[edit source]
A populated microSD card can contain more than eight partitions, exceeding the number of partitions allowed by default in a Linux system.
At insertion step, you may get an 'Error mounting /dev/mmcblk0p9' or 'mount: cannot mount /dev/mmcblk0p9 read-only' error message.
By adding some options to modprobe, it is possible to allow more than eight partitions on a storage device:
echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf
sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf
5.6. How to update partitions[edit source]
For partial Flash memory update, the flashlayout.tsv must be edited to select only the partition that needs to be updated (first column =1).
See STM32CubeProgrammer_flashlayout#Updating partitions for details and example, the rest of the procedure is the same.
On ST boards, if FSBL or SSBL partitions need to be updated, the Bin2boot fields must be configured with ST binaries, as described in STM32CubeProgrammer_flashlayout#Updating partitions using official ST bootloaders.
5.7. How to populate a microSD card inserted in a Linux host PC[edit source]
STMicroelectronics distribution is delivered with the create_sdcard_from_flashlayout.sh script that allows to prepare and flash a microSD card image.
5.8. How to fuse STM32MP15x OTP[edit source]
5.8.1. Connection[edit source]
STM32CubeProgrammer requires to be connected to U-Boot in order to access OTP alternate.
To do it, you have to initiate a flash process but selecting only the 2 first "boot" partitions TF-A( 0x1) and U-Boot( 0x03) of a .tsv.
Using STM32CubeProgrammer GUI this can done without editing by using any available .tsv but selecting only the 2 first partitions thanks to "Select" column tick boxes on the left, as follow:
Perform the "Download" till success popup then disconnect from the GUI and switch to CLI in a terminal without rebooting the board:
STM32_Programmer_CLI -c port=usb1
5.8.2. Display status[edit source]
It will also displayed the status for each OTP words (Shadow lock read/write, program stick lock, permanent write lock):
- All lower OTP
- Only upper that are available for non secure (defined in TF-A device tree).
To display the OTP:
-otp displ ------------------------------------------------------------------- STM32CubeProgrammer v2.3.0 ------------------------------------------------------------------- USB speed : High Speed (480MBit/s) Manuf. ID : STMicroelectronics Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000 SN : 002500253338510534383330 FW version : 0x0110 Device ID : 0x0500 Device name : STM32MPxxx Device type : MPU Device CPU : Cortex-A7 UPLOADING OTP STRUCTURE ... Partition : 242 Size : 1024 Bytes Uploading OTP data: [==================================================] 100% OTP Partition read successfully OTP STRUCTURE VERSION :0x00000001 BSEC CONTROL REGISTERS: BSEC_OTP_CONFIG :0x0000000e |_[08] TR[1] : 0 |_[07] TR[0] : 0 |_[06] PRGWIDTH[3] : 0 |_[05] PRGWIDTH[2] : 0 |_[04] PRGWIDTH[1] : 0 |_[03] PRGWIDTH[0] : 1 |_[02] FRC[1] : 1 |_[01] FRC[0] : 1 |_[00] PWRUP : 0 BSEC_OTP_Status :0x00000041 |_[07] BIST2LOCK : 0 |_[06] BIST1LOCK : 1 |_[05] PWRON : 0 |_[04] PROGFAIL : 0 |_[03] BUSY : 0 |_[02] INVALID : 0 |_[01] FULLDBG : 0 |_[00] SECURE : 1 BSEC_OTP_LOCK :0x00000002 |_[04] GPLOCK : 0 |_[03] FENREG : 0 |_[02] DENREG : 0 |_[00] OTP : 0 BSEC_DENABLE :0x0000047f |_[10] DBGSWENABLE : 1 |_[09] CFGSDISABLE : 0 |_[08] CP15SDISABLE[1] : 0 |_[07] CP15SDISABLE[0] : 0 |_[06] SPNIDEN : 1 |_[05] SPIDEN : 1 |_[04] HDPEN : 1 |_[03] DEVICEEN : 1 |_[02] NIDEN : 1 |_[01] DBGEN : 1 |_[00] DFTEN : 1 BSEC_FENABLE :0x00000000 |_[03] CAN_disable : 0 |_[02] GPU_disable : 0 |_[01] Dual_A7_disable : 0 |_[00] Crypto_disable : 0 OTP LOWER SHADOW REGISTERS: ID value disturbed error R_SLock W_SLock Prog_SL Perm_L 00 0x00000017 0 0 1 1 0 0 01 0x00008000 0 0 0 1 0 1 02 0x00000000 0 0 0 1 1 0 03 0x00000000 0 0 0 0 0 0 04 0x00000000 0 0 0 0 0 0 05 0x00000000 0 0 0 0 0 0 06 0x00000000 0 0 0 0 0 0 07 0x00000000 0 0 0 0 0 0 08 0x00000000 0 0 0 1 0 0 09 0x00000000 0 0 0 0 0 0 10 0x00000000 0 0 0 0 0 0 11 0x00000000 0 0 0 0 0 0 12 0x7ce7f0ee 0 0 0 0 0 1 13 0x00250025 0 0 0 0 0 1 14 0x33385105 0 0 0 0 0 1 15 0x34383330 0 0 0 0 0 1 16 0x125575aa 0 0 0 1 1 1 17 0x1f41185b 0 0 0 0 0 1 18 0x7a200140 0 0 1 1 0 0 19 0x0690147c 0 0 0 0 0 1 20 0x5de00048 0 0 0 0 0 1 21 0x00000000 0 0 0 0 0 1 22 0x00000000 0 0 0 0 0 1 23 0x3fec2fd7 0 0 0 0 0 1 24 0x00000000 0 0 0 1 0 0 25 0x00000000 0 0 0 1 0 0 26 0x00000000 0 0 0 1 0 0 27 0x00000000 0 0 0 1 0 0 28 0x00000000 0 0 0 1 0 0 29 0x00000000 0 0 0 1 0 0 30 0x00000000 0 0 0 1 0 0 31 0x00000000 0 0 0 1 0 0 OTP UPPER SHADOW REGISTERS: ID value disturbed error R_SLock W_SLock Prog_SL Perm_L 32 0x00000000 0 0 1 1 1 1 33 0x00000000 0 0 1 1 1 1 34 0x00000000 0 0 1 1 1 1 35 0x00000000 0 0 1 1 1 1 36 0x00000000 0 0 1 1 1 1 37 0x00000000 0 0 1 1 1 1 38 0x00000000 0 0 1 1 1 1 39 0x00000000 0 0 1 1 1 1 40 0x00000000 0 0 0 1 1 1 41 0x00000000 0 0 0 1 1 1 42 0x00000000 0 0 0 1 1 1 43 0x00000000 0 0 0 1 1 1 44 0x00000000 0 0 0 1 1 1 45 0x00000000 0 0 0 1 1 1 46 0x00000000 0 0 0 1 1 1 47 0x00000000 0 0 0 1 1 1 48 0x00000000 0 0 0 1 1 1 49 0x00000000 0 0 0 1 1 1 50 0x00000000 0 0 0 1 1 1 51 0x00000000 0 0 0 1 1 1 52 0x00000000 0 0 0 1 1 1 53 0x00000000 0 0 0 1 1 1 54 0x00000000 0 0 0 1 1 1 55 0x00000000 0 0 0 1 1 1 56 0x00000000 0 0 1 1 0 0 57 0x42e18000 0 0 0 0 0 0 58 0x0000fd51 0 0 0 0 0 0 59 0x12722301 0 0 0 0 0 0 60 0x00000000 0 0 0 0 0 0 61 0x00000000 0 0 0 0 0 0 62 0x00000000 0 0 0 0 0 0 63 0x00000000 0 0 0 0 0 0 64 0x00000000 0 0 0 0 0 0 65 0x00000000 0 0 0 0 0 0 66 0x00000000 0 0 0 0 0 0 67 0x00000000 0 0 0 0 0 0 68 0x00000000 0 0 0 0 0 0 69 0x00000000 0 0 0 0 0 0 70 0x00000000 0 0 0 0 0 0 71 0x00000000 0 0 0 0 0 0 72 0x00000000 0 0 0 0 0 0 73 0x00000000 0 0 0 0 0 0 74 0x00000000 0 0 0 0 0 0 75 0x00000000 0 0 0 0 0 0 76 0x00000000 0 0 0 0 0 0 77 0x00000000 0 0 0 0 0 0 78 0x00000000 0 0 0 0 0 0 79 0x00000000 0 0 0 0 0 0 80 0x00000000 0 0 0 0 0 0 81 0x00000000 0 0 0 0 0 0 82 0x00000000 0 0 0 0 0 0 83 0x00000000 0 0 0 0 0 0 84 0x00000000 0 0 0 0 0 0 85 0x00000000 0 0 0 0 0 0 86 0x00000000 0 0 0 0 0 0 87 0x00000000 0 0 0 0 0 0 88 0x00000000 0 0 0 0 0 0 89 0x00000000 0 0 0 0 0 0 90 0x00000000 0 0 0 0 0 0 91 0x00000000 0 0 0 0 0 0 92 0x00000000 0 0 0 0 0 0 93 0x00000000 0 0 0 0 0 0 94 0x00000000 0 0 0 0 0 0 95 0x00000000 0 0 0 0 0 0 BSEC_HWCFGR :0x00000014 |_[07] ECC_USE[3] : 0 |_[06] ECC_USE[2] : 0 |_[05] ECC_USE[1] : 0 |_[04] ECC_USE[0] : 1 |_[03] SAFMEM_SIZE[3] : 0 |_[02] SAFMEM_SIZE[2] : 1 |_[01] SAFMEM_SIZE[1] : 0 |_[00] SAFMEM_SIZE[0] : 0 BSEC IP REV :1.1 BSEC IP ID :0x00100032 BSEC IP MAGIC ID :0xa3c5dd04STM32_Programmer_CLI -c port=usb1
5.8.3. Update value[edit source]
It is now possible to use programmer to manage new fuses values: bit to bit for Lower, only programmable once for Upper.
For example: Set the value 0x21458000 into the word 57 (0x39)
-otp program wordID=0x39 value=0x21458000STM32_Programmer_CLI -c port=usb1
Words are written as a 32bit word. It is important to take care of the bit order once using the value in software.
Example: Mac address 00:80:e1:42:45:e5 must be written as:
- Word 57 : 0x42e18000
- Word 58 : 0x0000e545
5.8.4. Update lock[edit source]
Lock (no other programmation could occured) could be added per word; the permanent lock access will only be refreshed after boot.
For example: permanent lock (pl=1) the word 57 (0x39)
-otp program wordID=0x39 value=0x21458000 pl=1STM32_Programmer_CLI -c port=usb1
5.9. How to program STPMIC NVM[edit source]
STM32CubeProgrammer require to be connected to U-Boot in order to access STPMIC NVM alternate (0xF4).
Refer to previous Chapter 5.8.1 and follow same procedure to flash only the 2 first "boot" partition with GUI. Then disconnect from GUI and switch to CLI in a terminal.
This is procedure to modify NVM values.
- Read partition of pmic and load it into a .bin file
-rp 0xf4 0x0 0x8 $MySelectedPATH\PMIC_NVM_read.binSTM32_Programmer_CLI -c port=usb1
- Backup it by creating a copy PMIC_NVM_write.bin
- Use a binary editor in HEX format ( eg "vi -b file.bin" then :%!xxd ) to edit the copy PMIC_NVM_write.bin with new values.
The binary format display the shadow register from 0xF8 to 0XFF. Refer to STPMIC1 DataSheet DS12792.
00000000: EE92 C002 F280 0233 .......3
respectively SHR address : F8F9 FAFB FCFD FEFF
- Program back the STPMIC1 with modified NVM using following command:
-pmic "PMIC_NVM_write.bin"STM32_Programmer_CLI -c port=usb1