Registered User mNo edit summary |
Registered User mNo edit summary |
||
(7 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
The '''STM32MP15x-EV1 Evaluation boards''' (STM32MP157A-EV1 and STM32MP157C-EV1) are high-end development platforms for STM32MP15 microprocessor devices. | The '''STM32MP15x-EV1 Evaluation boards''' (STM32MP157A-EV1 and STM32MP157C-EV1) are high-end development platforms for STM32MP15 microprocessor devices. | ||
Line 11: | Line 5: | ||
Two software distributions are supported in these boards: | Two software distributions are supported in these boards: | ||
* The '''STM32MPU Embedded Software distribution'''<ref name="Embedded Software distribution">[[STM32MPU Embedded Software distribution]]</ref>. You might also take a look at the latest [[STM32MP15 ecosystem release note]] | * The '''STM32MPU Embedded Software distribution'''<ref name="Embedded Software distribution">[[STM32MPU Embedded Software distribution]]</ref>. You might also take a look at the latest [[STM32MP15 ecosystem release note]] | ||
* The '''STM32MPU | * The '''STM32MPU Embedded Software distribution for Android'''<ref name="Android distribution">[[:Category:STM32MPU Embedded Software distribution for Android|STM32MPU Embedded Software distribution for Android]]</ref> | ||
For each distribution, three software Packages are delivered : the '''Starter Package''', the '''Developer Package''', the '''Distribution Package'''.<br> | For each distribution, three software Packages are delivered : the '''Starter Package''', the '''Developer Package''', the '''Distribution Package'''.<br> | ||
Line 18: | Line 12: | ||
These Packages provide you with the '''software packages''' (image, source code) and the '''tools''' that are needed to start using the STM32MP157x-EV1 Evaluation boards. | These Packages provide you with the '''software packages''' (image, source code) and the '''tools''' that are needed to start using the STM32MP157x-EV1 Evaluation boards. | ||
{|class=" | {|class="st-table" | ||
|- | |- | ||
| | | colspan="3" | [[File:ST_logo.png | 50px |link=]] '''STM32MPU Embedded Software distribution'''<ref name="Embedded Software distribution" /> | ||
|- | |- | ||
| style=" | | style="width:30%; text-align:center" | [[STM32MP15 Evaluation boards - Starter Package|'''Starter Package''']] | ||
| style=" | | style="width:30%; text-align:center" | [[STM32MP1 Developer Package|'''Developer Package''']] | ||
| style=" | | style="width:30%; text-align:center" | [[STM32MP1 Distribution Package|'''Distribution Package''']] | ||
|- | |- | ||
| | |||
* to evaluate the board capabilities | * to evaluate the board capabilities | ||
* to run examples | * to run examples | ||
| | |||
* to modify the pieces of software delivered as source code in this Package (for example the Linux kernel...) | * to modify the pieces of software delivered as source code in this Package (for example the Linux kernel...) | ||
* to add your own applications in the user space delivered as binary in this Package | * to add your own applications in the user space delivered as binary in this Package | ||
Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE | Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE | ||
| | |||
* to create your own distribution | * to create your own distribution | ||
|} | |} | ||
{|class=" | {|class="st-table" | ||
|- | |- | ||
| | | colspan="3" | [[File:Android_logo.png | 30px |link=]] '''STM32MPU Embedded Software distribution for Android'''<ref name="Android distribution" /> | ||
|- | |- | ||
| style=" | | style="width:30%; text-align:center" | [[STM32MP15 Evaluation boards - Starter Package for Android |'''Starter Package''']] | ||
| style=" | | style="width:30%; text-align:center" | [[STM32MP1 Developer Package for Android|'''Developer Package''']] | ||
| style=" | | style="width:30%; text-align:center" | [[STM32MP1 Distribution Package for Android|'''Distribution Package''']] | ||
|- | |||
| | |||
* to evaluate the board capabilities | |||
* to run examples | |||
| | |||
* to develop your own Android application, accessing, through proprietary coprocessor service (named Copro), the firmware started on Arm® Cortex®-M processor | |||
| | |||
* to create your own distribution | |||
|} | |} | ||
Line 54: | Line 56: | ||
It also contains a short introduction of the board hardware components and connectors. | It also contains a short introduction of the board hardware components and connectors. | ||
{|class=" | {|class="st-table" style="text-align: left;" width="50%" cellspacing="0" | ||
|- | |- | ||
! style=" | ! style=" text-align:left;" valign="top" | '''Board description''' | ||
|- | |- | ||
| | | align="center" | | ||
[[File:STM32MP157C-EV1.png | 400px | link=STM32MP157C-EV1 - hardware description|STM32MP157x-EV1 - hardware description]]<br>[[STM32MP157C-EV1 - hardware description|'''STM32MP157x-EV1 - hardware description''']] | [[File:STM32MP157C-EV1.png | 400px | link=STM32MP157C-EV1 - hardware description|STM32MP157x-EV1 - hardware description]]<br>[[STM32MP157C-EV1 - hardware description|'''STM32MP157x-EV1 - hardware description''']] | ||
|} | |} | ||
==References== | ==References== | ||
<references/> | <references/> | ||
<noinclude> | |||
{{ReviewsComments|File to be reviewed by the marketing communication team}} | |||
{{PublicationRequestId | 7654 | 2018-06-08 | PhilipS}} | |||
[[Category:STM32MP15 Evaluation boards |00]] | |||
</noinclude> |
Latest revision as of 18:05, 20 November 2019
The STM32MP15x-EV1 Evaluation boards (STM32MP157A-EV1 and STM32MP157C-EV1) are high-end development platforms for STM32MP15 microprocessor devices.
This article gives links to the main articles relevant to starting with these boards.
1. Supported software distributions[edit source]
Two software distributions are supported in these boards:
- The STM32MPU Embedded Software distribution[1]. You might also take a look at the latest STM32MP15 ecosystem release note
- The STM32MPU Embedded Software distribution for Android[2]
For each distribution, three software Packages are delivered : the Starter Package, the Developer Package, the Distribution Package.
Note that the Which Package better suits your needs article provides hints for choosing between these Packages.
These Packages provide you with the software packages (image, source code) and the tools that are needed to start using the STM32MP157x-EV1 Evaluation boards.
![]() | ||
Starter Package | Developer Package | Distribution Package |
|
Note: these developments require a host PC running the OpenSTLinux SDK, and optionally an IDE |
|
![]() | ||
Starter Package | Developer Package | Distribution Package |
|
|
|
2. Hardware description[edit source]
The article linked below briefly describes the board, and helps to understand how to:
- assemble the board
- configure hardware jumpers and switches
- connect the board to external material
It also contains a short introduction of the board hardware components and connectors.
Board description |
---|
3. References[edit source]