Registered User mNo edit summary |
Registered User mNo edit summary |
||
(One intermediate revision by the same user not shown) | |||
Line 1: | Line 1: | ||
== STM32MPU Embedded Software overview == | == STM32MPU Embedded Software overview == | ||
The diagram below shows [[STM32MPU Embedded Software distribution]] main components: | The diagram below shows [[STM32MPU Embedded Software distribution]] main components: | ||
Line 19: | Line 11: | ||
* The '''STM32Cube MPU Package''' is running on the Arm<sup>®</sup> Cortex<sup>®</sup>-M: it is based on HAL drivers and middlewares, like other STM32 microcontrollers, completed with [[Coprocessor_management_overview|coprocessor management]].<br /> | * The '''STM32Cube MPU Package''' is running on the Arm<sup>®</sup> Cortex<sup>®</sup>-M: it is based on HAL drivers and middlewares, like other STM32 microcontrollers, completed with [[Coprocessor_management_overview|coprocessor management]].<br /> | ||
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.<br /> | The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.<br /> | ||
{{ImageMap|Image: STM32MPU Embedded Software architecture overview.png{{!}} frame {{!}} center {{!}} STM32MPU Embedded Software architecture overview. | {{ImageMap|Image: STM32MPU Embedded Software architecture overview.png{{!}} frame {{!}} center {{!}} STM32MPU Embedded Software architecture overview. | ||
rect 621 104 715 408 [[STM32CubeMP1 architecture]] | rect 621 104 715 408 [[STM32CubeMP1 architecture]] | ||
rect 157 161 253 220 [[OP-TEE overview]] | rect 157 161 253 220 [[OP-TEE overview]] | ||
Line 43: | Line 35: | ||
== References == | == References == | ||
<references/> | <references/> | ||
<noinclude> | |||
{{ReviewsComments|File to be reviewed by the marketing communication team}} | |||
{{PublicationRequestId | 9172 | 2018-10-26 | AlainF}} | |||
[[Category:Architecture overview]] | |||
[[Category:Embedded software components|01]] | |||
</noinclude> |
Latest revision as of 13:55, 15 October 2019
1. STM32MPU Embedded Software overview[edit source]
The diagram below shows STM32MPU Embedded Software distribution main components:
- The OpenSTLinux distribution, running on the Arm® Cortex®-A, including:
- The OpenSTLinux BSP with:
- The boot chain based on TF-A and U-Boot.
- The OP-TEE secure OS running on the Arm® Cortex®-A in secure mode.
- The Linux® kernel running on the Arm® Cortex®-A in non-secure mode.
- The application frameworks are composed of middlewares relying on the BSP and providing API:
- on the OP-TEE side to run Trusted Applications (TA) that allow to manipulate secrets (not visible from the Linux and STM32Cube MPU Package)
- on the Linux side to run Applications that typically interact with the user via the display, the touchscreen, etc.
- The OpenSTLinux BSP with:
- The STM32Cube MPU Package is running on the Arm® Cortex®-M: it is based on HAL drivers and middlewares, like other STM32 microcontrollers, completed with coprocessor management.
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.


- STM32CubeMP1 architecture
- OP-TEE overview
- TF-A overview
- U-Boot overview
- STM32MP15 Linux kernel overview
- Boot chains overview
- Linux application frameworks overview
- OpenSTLinux BSP architecture overview
- OpenSTLinux architecture overview
- Category:Platform configuration
- Security overview
2. Open Source Software (OSS) philosophy[edit source]
The Open source software source code is released under a license in which the copyright holder grants users the rights to study, change and distribute the software to anyone and for any purpose[1].
STMicroelectronics maximizes the using of open source software and contributes to those communities. Notice that, due to the software review life cycle, it can take some time before getting all developments accepted in the communities, so STMicroelectronics can also temporarily provide some source code on github[2], until it is merged in the targeted repository.
3. References[edit source]